AM273x MCU+ SDK  08.05.00
CBUFF_SwSessionCfg Struct Reference

Detailed Description

CBUFF Software Triggered Session configuration.

The structure describes the configuration required to be specified if the session is created in software triggered mode.

Data Fields

CBUFF_BufferCfg userBufferInfo [CBUFF_MAX_USER_BUFFER]
 User supplied data buffers which can be transmitted over the interface. More...
 

Field Documentation

◆ userBufferInfo

CBUFF_BufferCfg CBUFF_SwSessionCfg::userBufferInfo[CBUFF_MAX_USER_BUFFER]

User supplied data buffers which can be transmitted over the interface.