Functions | |
int32_t | SDL_STC_getStatus (SDL_STC_Inst instance) |
This API is used to get status for STC result. More... | |
int32_t | SDL_STC_selfTest (SDL_STC_Inst instance, SDL_STC_TestType testType, SDL_STC_Config *pConfig) |
This API is used to run the STC module. More... | |
static int32_t | SDL_STC_configure (SDL_STC_Inst instance, SDL_STC_Config *pConfig, SDL_STC_TestType testType) |
This API is used to configure STC module. More... | |
static int32_t | SDL_STC_runTest (SDL_STC_Inst instance) |
This API is used to enable the STC module. More... | |
static void | SDL_STC_delay (int32_t count) |
This API is used to provide delay for processor core. More... | |
static void | SDL_STC_resetCauseClear (void) |
This API is used to clear the reset cause bits for processor core. More... | |
int32_t SDL_STC_getStatus | ( | SDL_STC_Inst | instance | ) |
This API is used to get status for STC result.
instance | Holds the instance for STC module. |
NOTE: This API informes only first that we should run STC test or not.if it will return that STC has been Done, then programe will be terminated simply from here.
int32_t SDL_STC_selfTest | ( | SDL_STC_Inst | instance, |
SDL_STC_TestType | testType, | ||
SDL_STC_Config * | pConfig | ||
) |
This API is used to run the STC module.
instance | Holds the instance for STC module. |
testType | testType that in wwhich mode test need to be run. |
pConfig | Configuration that need to be run. |
NOTE: This API informes only first that we should run STC test or not.if it will return that STC has been Done, then programe will be terminated simply from here. There nothing will be returned as core will be reset after run this API. testType that in wwhich mode test need to be run.
|
static |
This API is used to configure STC module.
instance | Holds the instance for STC module. |
pConfig | pointer to the STC config structure |
testType | Enum value for specifying testType |
NOTE: There are two types of testType
|
static |
This API is used to enable the STC module.
instance | Holds the instance for STC module. |
|
static |
This API is used to provide delay for processor core.
|
static |
This API is used to clear the reset cause bits for processor core.