AM273x MCU+ SDK  08.05.00

Introduction

The Ethernet PHY driver supports auto-negotiation and manual modes. The PHY driver uses an MDIO abstraction to perform register reads and writes. The MDIO abstraction can be implemented using Enet LLD's Enet Management Data I/O (MDIO) API or any other MDIO driver.

Sub Modules

 Generic PHY
 
 TI DP83822 PHY
 
 TI DP83867 PHY
 
 TI DP83869 PHY
 
 VSC8514 PHY
 

Data Structures

struct  EnetPhy_Version
 PHY version (ID). More...
 
struct  EnetPhy_LinkCfg
 Link speed and duplexity configuration. More...
 
struct  EnetPhy_FsmTimeoutCfg
 PHY State-Machine time-out values. More...
 
struct  EnetPhy_Cfg
 PHY configuration parameters. More...
 
struct  EnetPhy_Mdio
 MDIO driver. More...
 
struct  EnetPhy_State
 PHY driver FSM state. More...
 
struct  EnetPhy_Obj
 PHY driver object. More...
 

Functions

void EnetPhy_initCfg (EnetPhy_Cfg *phyCfg)
 Initialize PHY config params. More...
 
void EnetPhy_setExtendedCfg (EnetPhy_Cfg *phyCfg, const void *extendedCfg, uint32_t extendedCfgSize)
 Set PHY extended parameters. More...
 
EnetPhy_Handle EnetPhy_open (const EnetPhy_Cfg *phyCfg, EnetPhy_Mii mii, const EnetPhy_LinkCfg *linkCfg, uint32_t macPortCaps, EnetPhy_MdioHandle hMdio, void *mdioArgs)
 Open the PHY driver. More...
 
void EnetPhy_close (EnetPhy_Handle hPhy)
 Close the PHY driver. More...
 
EnetPhy_LinkStatus EnetPhy_tick (EnetPhy_Handle hPhy)
 Run PHY state machine. More...
 
int32_t EnetPhy_getId (EnetPhy_Handle hPhy, EnetPhy_Version *version)
 Get PHY id. More...
 
bool EnetPhy_isAlive (EnetPhy_Handle hPhy)
 Get PHY alive status. More...
 
bool EnetPhy_isLinked (EnetPhy_Handle hPhy)
 Get link status. More...
 
int32_t EnetPhy_getLinkCfg (EnetPhy_Handle hPhy, EnetPhy_LinkCfg *linkCfg)
 Get link configuration. More...
 
int32_t EnetPhy_readReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t *val)
 Read PHY register. More...
 
int32_t EnetPhy_writeReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t val)
 Write PHY register. More...
 
int32_t EnetPhy_rmwReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t mask, uint16_t val)
 Read-modify-write PHY register. More...
 
int32_t EnetPhy_readExtReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t *val)
 Read PHY extended register. More...
 
int32_t EnetPhy_writeExtReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t val)
 Write PHY extended register. More...
 
int32_t EnetPhy_rmwExtReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t mask, uint16_t val)
 Read-modify-write PHY extended register. More...
 
int32_t EnetPhy_readC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t *val)
 Read PHY register using Clause-45 frame. More...
 
int32_t EnetPhy_writeC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t val)
 Write PHY register using Clause-45 frame. More...
 
int32_t EnetPhy_rmwC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t mask, uint16_t val)
 Read-modify-write PHY register using Clause-45 frame. More...
 
void EnetPhy_printRegs (EnetPhy_Handle hPhy)
 Print all PHY registers. More...
 

Typedefs

typedef EnetPhy_MdioEnetPhy_MdioHandle
 MDIO driver handle. More...
 
typedef struct EnetPhy_Drv_s * EnetPhyDrv_Handle
 PHY specific driver handle. More...
 
typedef struct EnetPhy_Obj_s * EnetPhy_Handle
 PHY driver object handle. More...
 

Enumerations

enum  EnetPhy_Magic { ENETPHY_MAGIC = 0xCADACADAU, ENETPHY_NO_MAGIC = 0x0U }
 EnetPhy driver magic value, used to indicate if driver is open or not. More...
 
enum  EnetPhy_Mii {
  ENETPHY_MAC_MII_MII = 0U, ENETPHY_MAC_MII_RMII, ENETPHY_MAC_MII_GMII, ENETPHY_MAC_MII_RGMII,
  ENETPHY_MAC_MII_SGMII, ENETPHY_MAC_MII_QSGMII
}
 MAC Media-Independent Interface (MII). More...
 
enum  EnetPhy_Speed { ENETPHY_SPEED_10MBIT = 0U, ENETPHY_SPEED_100MBIT, ENETPHY_SPEED_1GBIT, ENETPHY_SPEED_AUTO }
 MAC interface speed. More...
 
enum  EnetPhy_Duplexity { ENETPHY_DUPLEX_HALF = 0U, ENETPHY_DUPLEX_FULL, ENETPHY_DUPLEX_AUTO }
 MAC interface duplexity. More...
 
enum  EnetPhy_LinkStatus { ENETPHY_GOT_LINK = 0U, ENETPHY_LINK_UP, ENETPHY_LOST_LINK, ENETPHY_LINK_DOWN }
 PHY link status. More...
 
enum  EnetPhy_FsmState {
  ENETPHY_FSM_STATE_INIT = 0U, ENETPHY_FSM_STATE_FINDING, ENETPHY_FSM_STATE_RESET_WAIT, ENETPHY_FSM_STATE_ENABLE,
  ENETPHY_FSM_STATE_FOUND, ENETPHY_FSM_STATE_NWAY_START, ENETPHY_FSM_STATE_NWAY_WAIT, ENETPHY_FSM_STATE_LINK_WAIT,
  ENETPHY_FSM_STATE_LINKED, ENETPHY_FSM_STATE_LOOPBACK
}
 PHY driver state-machine states. More...
 

Macros

#define ENETPHY_IS_ADDR_VALID(addr)   ((addr) <= 31U)
 Check if PHY address is valid (0 - 31). More...
 
#define ENETPHY_BIT(n)   (1U << (n))
 Macro to set bit at given bit position. More...
 
#define ENETPHY_IS_BIT_SET(val, n)   (((val) & ENETPHY_BIT(n)) != 0U)
 Macro to check if bit at given bit position is set. More...
 
#define ENETPHY_ARRAYSIZE(x)   (sizeof(x) / sizeof(x[0]))
 Macro to get the size of an array. More...
 
#define ENETPHY_EXTENDED_CFG_SIZE_MAX   (128U)
 Max extended configuration size, arbitrarily chosen. More...
 
#define ENETPHY_FSM_TICK_PERIOD_MS   (100U)
 Enet PHY State Machine tick period. More...
 
#define ENETPHY_INVALID_PHYADDR   (~0U)
 Invalid PHY address indicator. More...
 

Ethernet PHY driver error codes

Error codes returned by the Ethernet PHY driver APIs.

#define ENETPHY_SOK   (CSL_PASS)
 Success. More...
 
#define ENETPHY_EFAIL   (CSL_EFAIL)
 Generic failure error condition (typically caused by hardware). More...
 
#define ENETPHY_EBADARGS   (CSL_EBADARGS)
 Bad arguments (i.e. NULL pointer). More...
 
#define ENETPHY_EINVALIDPARAMS   (CSL_EINVALID_PARAMS)
 Invalid parameters (i.e. value out-of-range). More...
 
#define ENETPHY_ETIMEOUT   (CSL_ETIMEOUT)
 Time out while waiting for a given condition to happen. More...
 
#define ENETPHY_EALLOC   (CSL_EALLOC)
 Allocation failure. More...
 
#define ENETPHY_EPERM   (CSL_EALLOC - 4)
 Operation not permitted. More...
 
#define ENETPHY_ENOTSUPPORTED   (CSL_EALLOC - 5)
 Operation not supported. More...
 

Ethernet PHY link capability masks

Error codes returned by the Ethernet PHY driver APIs.

#define ENETPHY_LINK_CAP_HD10   ENETPHY_BIT(1)
 10-Mbps, half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_FD10   ENETPHY_BIT(2)
 10-Mbps, full-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_HD100   ENETPHY_BIT(3)
 100-Mbps, half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_FD100   ENETPHY_BIT(4)
 100-Mbps, full-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_HD1000   ENETPHY_BIT(5)
 1-Gbps, half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_FD1000   ENETPHY_BIT(6)
 1-Gbps, full-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_10
 10-Mbps, full and half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_100
 100-Mbps, full and half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_1000
 1-Gbps, full and half-duplex capability mask. More...
 
#define ENETPHY_LINK_CAP_ALL
 Auto-negotiation mask with all duplexity and speed values set. More...
 

Macro Definition Documentation

◆ ENETPHY_IS_ADDR_VALID

#define ENETPHY_IS_ADDR_VALID (   addr)    ((addr) <= 31U)

Check if PHY address is valid (0 - 31).

◆ ENETPHY_BIT

#define ENETPHY_BIT (   n)    (1U << (n))

Macro to set bit at given bit position.

◆ ENETPHY_IS_BIT_SET

#define ENETPHY_IS_BIT_SET (   val,
 
)    (((val) & ENETPHY_BIT(n)) != 0U)

Macro to check if bit at given bit position is set.

◆ ENETPHY_ARRAYSIZE

#define ENETPHY_ARRAYSIZE (   x)    (sizeof(x) / sizeof(x[0]))

Macro to get the size of an array.

◆ ENETPHY_SOK

#define ENETPHY_SOK   (CSL_PASS)

Success.

◆ ENETPHY_EFAIL

#define ENETPHY_EFAIL   (CSL_EFAIL)

Generic failure error condition (typically caused by hardware).

◆ ENETPHY_EBADARGS

#define ENETPHY_EBADARGS   (CSL_EBADARGS)

Bad arguments (i.e. NULL pointer).

◆ ENETPHY_EINVALIDPARAMS

#define ENETPHY_EINVALIDPARAMS   (CSL_EINVALID_PARAMS)

Invalid parameters (i.e. value out-of-range).

◆ ENETPHY_ETIMEOUT

#define ENETPHY_ETIMEOUT   (CSL_ETIMEOUT)

Time out while waiting for a given condition to happen.

◆ ENETPHY_EALLOC

#define ENETPHY_EALLOC   (CSL_EALLOC)

Allocation failure.

◆ ENETPHY_EPERM

#define ENETPHY_EPERM   (CSL_EALLOC - 4)

Operation not permitted.

◆ ENETPHY_ENOTSUPPORTED

#define ENETPHY_ENOTSUPPORTED   (CSL_EALLOC - 5)

Operation not supported.

◆ ENETPHY_LINK_CAP_HD10

#define ENETPHY_LINK_CAP_HD10   ENETPHY_BIT(1)

10-Mbps, half-duplex capability mask.

◆ ENETPHY_LINK_CAP_FD10

#define ENETPHY_LINK_CAP_FD10   ENETPHY_BIT(2)

10-Mbps, full-duplex capability mask.

◆ ENETPHY_LINK_CAP_HD100

#define ENETPHY_LINK_CAP_HD100   ENETPHY_BIT(3)

100-Mbps, half-duplex capability mask.

◆ ENETPHY_LINK_CAP_FD100

#define ENETPHY_LINK_CAP_FD100   ENETPHY_BIT(4)

100-Mbps, full-duplex capability mask.

◆ ENETPHY_LINK_CAP_HD1000

#define ENETPHY_LINK_CAP_HD1000   ENETPHY_BIT(5)

1-Gbps, half-duplex capability mask.

◆ ENETPHY_LINK_CAP_FD1000

#define ENETPHY_LINK_CAP_FD1000   ENETPHY_BIT(6)

1-Gbps, full-duplex capability mask.

◆ ENETPHY_LINK_CAP_10

#define ENETPHY_LINK_CAP_10
Value:
ENETPHY_LINK_CAP_FD10)

10-Mbps, full and half-duplex capability mask.

◆ ENETPHY_LINK_CAP_100

#define ENETPHY_LINK_CAP_100
Value:
ENETPHY_LINK_CAP_FD100)

100-Mbps, full and half-duplex capability mask.

◆ ENETPHY_LINK_CAP_1000

#define ENETPHY_LINK_CAP_1000
Value:
ENETPHY_LINK_CAP_FD1000)

1-Gbps, full and half-duplex capability mask.

◆ ENETPHY_LINK_CAP_ALL

#define ENETPHY_LINK_CAP_ALL
Value:
ENETPHY_LINK_CAP_FD10 | \
ENETPHY_LINK_CAP_HD100 | \
ENETPHY_LINK_CAP_FD100 | \
ENETPHY_LINK_CAP_HD1000 | \
ENETPHY_LINK_CAP_FD1000)

Auto-negotiation mask with all duplexity and speed values set.

◆ ENETPHY_EXTENDED_CFG_SIZE_MAX

#define ENETPHY_EXTENDED_CFG_SIZE_MAX   (128U)

Max extended configuration size, arbitrarily chosen.

◆ ENETPHY_FSM_TICK_PERIOD_MS

#define ENETPHY_FSM_TICK_PERIOD_MS   (100U)

Enet PHY State Machine tick period.

◆ ENETPHY_INVALID_PHYADDR

#define ENETPHY_INVALID_PHYADDR   (~0U)

Invalid PHY address indicator.

Typedef Documentation

◆ EnetPhy_MdioHandle

MDIO driver handle.

◆ EnetPhyDrv_Handle

typedef struct EnetPhy_Drv_s* EnetPhyDrv_Handle

PHY specific driver handle.

◆ EnetPhy_Handle

typedef struct EnetPhy_Obj_s* EnetPhy_Handle

PHY driver object handle.

PHY driver opaque handle used to call any PHY related APIs.

Enumeration Type Documentation

◆ EnetPhy_Magic

EnetPhy driver magic value, used to indicate if driver is open or not.

Enumerator
ENETPHY_MAGIC 

Magic number used to identify when driver has been opened.

ENETPHY_NO_MAGIC 

Magic number used to identify when driver is closed.

◆ EnetPhy_Mii

MAC Media-Independent Interface (MII).

Enumerator
ENETPHY_MAC_MII_MII 

MII interface.

ENETPHY_MAC_MII_RMII 

RMII interface.

ENETPHY_MAC_MII_GMII 

GMII interface.

ENETPHY_MAC_MII_RGMII 

RGMII interface.

ENETPHY_MAC_MII_SGMII 

SGMII interface.

ENETPHY_MAC_MII_QSGMII 

QSGMII interface.

◆ EnetPhy_Speed

MAC interface speed.

Enumerator
ENETPHY_SPEED_10MBIT 

10 Mbps

ENETPHY_SPEED_100MBIT 

100 Mbps

ENETPHY_SPEED_1GBIT 

1 Gbps

ENETPHY_SPEED_AUTO 

Speed determined automatically

◆ EnetPhy_Duplexity

MAC interface duplexity.

Enumerator
ENETPHY_DUPLEX_HALF 

Half duplex

ENETPHY_DUPLEX_FULL 

Full duplex

ENETPHY_DUPLEX_AUTO 

Duplexity determined automatically

◆ EnetPhy_LinkStatus

PHY link status.

Enumerator
ENETPHY_GOT_LINK 

PHY got link up

ENETPHY_LINK_UP 

PHY link is still up

ENETPHY_LOST_LINK 

PHY lost link

ENETPHY_LINK_DOWN 

PHY link is still down

◆ EnetPhy_FsmState

PHY driver state-machine states.

Enumerator
ENETPHY_FSM_STATE_INIT 

INIT state.

ENETPHY_FSM_STATE_FINDING 

FINDING state.

ENETPHY_FSM_STATE_RESET_WAIT 

RESET_WAIT state.

ENETPHY_FSM_STATE_ENABLE 

ENABLE state.

ENETPHY_FSM_STATE_FOUND 

FOUND state.

ENETPHY_FSM_STATE_NWAY_START 

NWAY_START state (auto-negotiation path)

ENETPHY_FSM_STATE_NWAY_WAIT 

NWAY_WAIT state (auto-negotiation path)

ENETPHY_FSM_STATE_LINK_WAIT 

LINK_WAIT state.

ENETPHY_FSM_STATE_LINKED 

LINKED state.

ENETPHY_FSM_STATE_LOOPBACK 

LOOPBACK state.

Function Documentation

◆ EnetPhy_initCfg()

void EnetPhy_initCfg ( EnetPhy_Cfg phyCfg)

Initialize PHY config params.

Initializes PHY driver configuration parameters.

Parameters
phyCfgPHY configuration params

◆ EnetPhy_setExtendedCfg()

void EnetPhy_setExtendedCfg ( EnetPhy_Cfg phyCfg,
const void *  extendedCfg,
uint32_t  extendedCfgSize 
)

Set PHY extended parameters.

Sets the PHY-specific extended parameters to the PHY config structure.

Parameters
phyCfgPointer to the PHY config
extendedCfgPointer to the PHY extended config
extendedCfgSizeSize of the PHY extended config

◆ EnetPhy_open()

EnetPhy_Handle EnetPhy_open ( const EnetPhy_Cfg phyCfg,
EnetPhy_Mii  mii,
const EnetPhy_LinkCfg linkCfg,
uint32_t  macPortCaps,
EnetPhy_MdioHandle  hMdio,
void *  mdioArgs 
)

Open the PHY driver.

Open the Ethernet PHY driver for the given MAC port number. The PHY driver takes PHY specific configuration parameters, the MAC port type connection and the desired link configuration (auto or manual).

Parameters
phyCfgPHY configuration params
miiPHY MII interface type
linkCfgLink configuration (speed and duplexity)
macPortCapsMAC port speed/duplex capabilities. It's a bit mask of EnetPhy_LinkCaps
hMdioMDIO driver to be used for PHY register read/write
mdioArgsPrivate data passed to the MDIO driver functions
Returns
PHY device handle if successful, NULL otherwise.

◆ EnetPhy_close()

void EnetPhy_close ( EnetPhy_Handle  hPhy)

Close the PHY driver.

Closes the Ethernet PHY driver.

Parameters
hPhyPHY device handle

◆ EnetPhy_tick()

EnetPhy_LinkStatus EnetPhy_tick ( EnetPhy_Handle  hPhy)

Run PHY state machine.

Runs the PHY FSM.

Parameters
hPhyPHY device handle
Returns
Whether PHY got or lost link, or no change.

◆ EnetPhy_getId()

int32_t EnetPhy_getId ( EnetPhy_Handle  hPhy,
EnetPhy_Version version 
)

Get PHY id.

Gets the device ID of a PHY, read from IDR1 and IDR2 registers.

Parameters
hPhyPHY device handle
versionPointer to PHY version.
Returns
EnetPhy_ErrorCodes

◆ EnetPhy_isAlive()

bool EnetPhy_isAlive ( EnetPhy_Handle  hPhy)

Get PHY alive status.

Gets the PHY alive status. Whether PHY is responding to read accesses.

Parameters
hPhyPHY device handle
Returns
true if PHY is alive, false otherwise

◆ EnetPhy_isLinked()

bool EnetPhy_isLinked ( EnetPhy_Handle  hPhy)

Get link status.

Gets the link status: linked or not, based on driver's state machine. The PHY driver state machine can take a little longer to detect link up because it runs on tick period intervals and need to traverse few states to reach link up FSM state.

Parameters
hPhyPHY device handle
Returns
true if PHY is linked, false otherwise

◆ EnetPhy_getLinkCfg()

int32_t EnetPhy_getLinkCfg ( EnetPhy_Handle  hPhy,
EnetPhy_LinkCfg linkCfg 
)

Get link configuration.

Gets the link configuration, that is, the configuration that the PHY has negotiated with the link partner or the manual link configuration it was set to.

Parameters
hPhyPHY device handle
linkCfgLink configuration
Returns
EnetPhy_ErrorCodes

◆ EnetPhy_readReg()

int32_t EnetPhy_readReg ( EnetPhy_Handle  hPhy,
uint32_t  reg,
uint16_t *  val 
)

Read PHY register.

Reads a PHY register. It's not meant for extended registers.

Parameters
hPhyPHY device handle
regRegister number
valPointer to the read value
Returns
EnetPhy_ErrorCodes

◆ EnetPhy_writeReg()

int32_t EnetPhy_writeReg ( EnetPhy_Handle  hPhy,
uint32_t  reg,
uint16_t  val 
)

Write PHY register.

Writes a PHY register. It's not meant for extended registers.

Parameters
hPhyPHY device handle
regRegister number
valValue to be written
Returns
EnetPhy_ErrorCodes

◆ EnetPhy_rmwReg()

int32_t EnetPhy_rmwReg ( EnetPhy_Handle  hPhy,
uint32_t  reg,
uint16_t  mask,
uint16_t  val 
)

Read-modify-write PHY register.

Read-modify-write a PHY register. It's not meant for extended registers.

Parameters
hPhyPHY device handle
regRegister number
maskBitmask to be applied on read value and value to be written
valValue to be written
Returns
EnetPhy_ErrorCodes

◆ EnetPhy_readExtReg()

int32_t EnetPhy_readExtReg ( EnetPhy_Handle  hPhy,
uint32_t  reg,
uint16_t *  val 
)

Read PHY extended register.

Reads a PHY extended register.

Parameters
hPhyPHY device handle
regRegister number
valPointer to the read value
Returns
EnetPhy_ErrorCodes

◆ EnetPhy_writeExtReg()

int32_t EnetPhy_writeExtReg ( EnetPhy_Handle  hPhy,
uint32_t  reg,
uint16_t  val 
)

Write PHY extended register.

Writes a PHY extended register.

Parameters
hPhyPHY device handle
regRegister number
valValue to be written
Returns
EnetPhy_ErrorCodes

◆ EnetPhy_rmwExtReg()

int32_t EnetPhy_rmwExtReg ( EnetPhy_Handle  hPhy,
uint32_t  reg,
uint16_t  mask,
uint16_t  val 
)

Read-modify-write PHY extended register.

Read-modify-write a PHY extended register.

Parameters
hPhyPHY device handle
regRegister number
maskBitmask to be applied on read value and value to be written
valValue to be written
Returns
EnetPhy_ErrorCodes

◆ EnetPhy_readC45Reg()

int32_t EnetPhy_readC45Reg ( EnetPhy_Handle  hPhy,
uint8_t  mmd,
uint32_t  reg,
uint16_t *  val 
)

Read PHY register using Clause-45 frame.

Reads a PHY register using Clause-45 frame.

Parameters
hPhyPHY device handle
mmdMMD
regRegister number
valPointer to the read value
Returns
EnetPhy_ErrorCodes

◆ EnetPhy_writeC45Reg()

int32_t EnetPhy_writeC45Reg ( EnetPhy_Handle  hPhy,
uint8_t  mmd,
uint32_t  reg,
uint16_t  val 
)

Write PHY register using Clause-45 frame.

Writes a PHY register using Clause-45 frame.

Parameters
hPhyPHY device handle
mmdMMD
regRegister number
valValue to be written
Returns
EnetPhy_ErrorCodes

◆ EnetPhy_rmwC45Reg()

int32_t EnetPhy_rmwC45Reg ( EnetPhy_Handle  hPhy,
uint8_t  mmd,
uint32_t  reg,
uint16_t  mask,
uint16_t  val 
)

Read-modify-write PHY register using Clause-45 frame.

Read-modify-write a PHY register using Clause-45 frame.

Parameters
hPhyPHY device handle
mmdMMD
regRegister number
maskBitmask to be applied on read value and value to be written
valValue to be written
Returns
EnetPhy_ErrorCodes

◆ EnetPhy_printRegs()

void EnetPhy_printRegs ( EnetPhy_Handle  hPhy)

Print all PHY registers.

Prints all registers of a PHY.

Parameters
hPhyPHY device handle
ENETPHY_LINK_CAP_HD100
#define ENETPHY_LINK_CAP_HD100
100-Mbps, half-duplex capability mask.
Definition: enetphy.h:144
ENETPHY_LINK_CAP_HD1000
#define ENETPHY_LINK_CAP_HD1000
1-Gbps, half-duplex capability mask.
Definition: enetphy.h:150
ENETPHY_LINK_CAP_HD10
#define ENETPHY_LINK_CAP_HD10
10-Mbps, half-duplex capability mask.
Definition: enetphy.h:138