This example demonstrates the usage of the SDL DSS_L3 module. The example shows how to setup and use the ECC BUS Safety Diagnostic operation. Shows the generation of SEC, DED and RED error on DSS L3 BANK A, BANK B, BANK C and BANK D.
Note : SEC - Single Error Correction, DED - Double Error Correction, RED - Redundancy Error Correction
| Use Case | Description |
|---|---|
| UC-1 | SEC Error insertion on DSS L3 BANK A. |
| UC-2 | DED Error insertion on DSS L3 BANK A. |
| UC-3 | RED Error insertion on DSS L3 BANK A. |
| UC-4 | SEC Error insertion on DSS L3 BANK B. |
| UC-5 | DED Error insertion on DSS L3 BANK B. |
| UC-6 | RED Error insertion on DSS L3 BANK B. |
| UC-7 | SEC Error insertion on DSS L3 BANK C. |
| UC-8 | DED Error insertion on DSS L3 BANK C. |
| UC-9 | RED Error insertion on DSS L3 BANK C. |
| UC-10 | SEC Error insertion on DSS L3 BANK D. |
| UC-11 | DED Error insertion on DSS L3 BANK D. |
| UC-12 | RED Error insertion on DSS L3 BANK D. |
Shown below is a sample output when the application is run,