![Logo](ti_logo.svg) |
AM273x MCU+ SDK
08.05.00
|
|
Features Supported
DSS L3 module consists ECC Bus Safety Diagnostics.
BUS Safety Errors : This includes SEC , DED and RED error injection on DSS L3 BANK A, BANK B, BANK C and BANK D
Note : SEC - Single Error Correction, DED - Double Error Correction, RED - Redundancy Error Correction
The module supports below API's for the application
- API to support and induce error on DSS L3 BUS.
- API to support interrupt configuration
SysConfig Features
Features NOT Supported
Important Usage Guidelines
Example Usage
The following shows an example of SDL DSS L3 API usage by the application for Error Injection Tests.
Include the below file to access the APIs
#include <sdl/sdl_adcbuf.h>
Induce the error SEC in DSS L3 Bank A
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
Induce the error DED in DSS L3 Bank A
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
Induce the error RED in DSS L3 Bank A
if(ret_val == SDL_PASS )
{
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
}
else
{
ret_val = SDL_EFAIL;
}
Induce the error SEC in DSS L3 Bank B
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
Induce the error DED in DSS L3 Bank B
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
Induce the error RED in DSS L3 Bank B
if(ret_val == SDL_PASS )
{
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
}
else
{
ret_val = SDL_EFAIL;
}
Induce the error SEC in DSS L3 Bank C
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
Induce the error DED in DSS L3 Bank C
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
Induce the error RED in DSS L3 Bank C
if(ret_val == SDL_PASS )
{
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
}
else
{
ret_val = SDL_EFAIL;
}
Induce the error SEC in DSS L3 Bank D
uint32_t timeout = SDL_DSS_L3_ECC_TIMEOUT;
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
Induce the error DED in DSS L3 Bank D
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
Induce the error RED in DSS L3 Bank D
if(ret_val == SDL_PASS )
{
{
ret_val = SDL_PASS;
}
else
{
ret_val = SDL_EFAIL;
}
}
else
{
ret_val = SDL_EFAIL;
}
API
APIs for SDL DSS_L3
uint32_t SDL_DSS_L3_BankA_dedErrorStatus(void)
This API is used to get DED error status from Bank A.
void SDL_DSS_L3_BANKC_secExecute(void)
This API is used for SEC test on DSS L3 Bank C.
void SDL_DSS_L3_BankA_dedErrorClear(void)
This API is used to clear DED error from Bank A.
void SDL_DSS_L3_BANKA_secExecute(void)
This API is used for SEC test on DSS L3 Bank A.
void SDL_DSS_L3_BankC_dedErrorClear(void)
This API is used to clear DED error from Bank C.
void SDL_DSS_L3_BankB_redErrorClear(void)
This API is used to clear RED error from Bank B.
uint32_t SDL_DSS_L3_BankC_secErrorStatus(void)
This API is used to get SEC error status from Bank C.
uint32_t SDL_DSS_L3_BankD_dedErrorStatus(void)
This API is used to get DED error status from Bank D.
@ SDL_DSS_L3_FI_GLOBAL_SAFE
Definition: dss_l3/v0/sdl_dss_l3.h:85
int32_t SDL_DSS_L3_BANKA_redExecute(SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType)
This API is used for RED test on DSS L3 Bank A.
void SDL_DSS_L3_BankD_redErrorClear(void)
This API is used to clear RED error from Bank D.
uint32_t SDL_DSS_L3_BankB_dedErrorStatus(void)
This API is used to get DED error status from Bank B.
uint32_t SDL_DSS_L3_BankB_redErrorStatus(void)
This API is used to get RED error status from Bank B.
void SDL_DSS_L3_BankC_redErrorClear(void)
This API is used to clear RED error from Bank C.
void SDL_DSS_L3_BankD_dedErrorClear(void)
This API is used to clear DED error from Bank D.
void SDL_DSS_L3_BankB_secErrorClear(void)
void SDL_DSS_L3_BANKC_dedExecute(void)
This API is used for DED test on DSS L3 Bank C.
int32_t SDL_DSS_L3_BANKC_redExecute(SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType)
This API is used for RED test on DSS L3 Bank C.
void SDL_DSS_L3_BANKB_dedExecute(void)
This API is used for DED test on DSS L3 Bank B.
void SDL_DSS_L3_BANKD_dedExecute(void)
This API is used for DED test on DSS L3 Bank D.
uint32_t SDL_DSS_L3_BankC_dedErrorStatus(void)
This API is used to get DED error status from Bank C.
void SDL_DSS_L3_BankD_secErrorClear(void)
This API is used to clear SEC error from DSS L3 Bank D.
void SDL_DSS_L3_BANKB_secExecute(void)
This API is used for SEC test on DSS L3 Bank B.
uint32_t SDL_DSS_L3_BankA_secErrorStatus(void)
This API is used to get SEC error status from Bank A.
void SDL_DSS_L3_BankA_redErrorClear(void)
This API is used to clear RED error from Bank A.
void SDL_DSS_L3_BANKA_dedExecute(void)
This API is used for DED test on DSS L3 Bank A.
uint32_t SDL_DSS_L3_BankA_redErrorStatus(void)
This API is used to get RED error status from Bank A.
uint32_t SDL_DSS_L3_BankC_redErrorStatus(void)
This API is used to get RED error status from Bank C.
void SDL_DSS_L3_BankA_secErrorClear(void)
This API is used to clear SEC error from DSS_L3 Bank A.
void SDL_DSS_L3_BankC_secErrorClear(void)
This API is used to clear SEC error from DSS L3 Bank C.
void SDL_DSS_L3_BankB_dedErrorClear(void)
This API is used to clear DED error from Bank B.
void SDL_DSS_L3_BANKD_secExecute(void)
This API is used for SEC test on DSS L3 Bank D.
uint32_t SDL_DSS_L3_BankD_secErrorStatus(void)
This API is used to get SEC error status from Bank D.
int32_t SDL_DSS_L3_BANKD_redExecute(SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType)
This API is used for RED test on DSS L3 Bank D.
@ SDL_DSS_L3_MAIN_CMD_INTERFACE
Definition: dss_l3/v0/sdl_dss_l3.h:91
uint32_t SDL_DSS_L3_BankB_secErrorStatus(void)
This API is used to get SEC error status from Bank B.
int32_t SDL_DSS_L3_BANKB_redExecute(SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType)
This API is used for RED test on DSS L3 Bank B.
uint32_t SDL_DSS_L3_BankD_redErrorStatus(void)
This API is used to get RED error status from Bank D.