AM273x MCU+ SDK  08.05.00
MIBSPI

The Multi Buffered Serial Peripheral Interface (MibSPI/MibSPIP) driver is a generic, full-duplex driver that transmits and receives data on the SPI bus. The SPI protocol defines the format of a data transfer over the SPI bus, but it leaves flow control, data formatting, and handshaking mechanisms to higher-level software layers.

Features Supported

  • Controller and Peripheral mode of operation
  • Per transfer selection of different channels/chip select
  • Blocking and non-blocking (callback) transfers
  • icount enable/disable
  • EDMA

SysConfig Features

Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
  • MIBSPI instances and pin configurations
  • Init/Deinit API integration with SYSCFG
  • MIBSPI module configuration parameters like MOSI, MISO pin selection and others.
  • MIBSPI channel configurations.
  • In the advanced configurations option you can configure MIBSPI advanced features such as number of parallel mode pin, feature bit map, transmit dummy value, ecc enable, cs hold and compatibility mode.
  • Based on above parameters, the SysConfig generated code does MIBSPI instance parameter configuration as part of Drivers_open and Drivers_close functions.

Features NOT Supported

  • EDMA support in compatibility mode

Usage Overview

API Sequence

To use the MIBSPI driver to send data over the SPI bus, the application calls the following APIs:

Initializing the MIBSPI Driver

MIBSPI_init() must be called before any other MIBSPI APIs. This function Create driver lock Construct thread safe handles for SPI driver level Semaphore to provide exclusive access to the SPI APIs

Opening the MIBSPI Driver

After initializing the MIBSPI driver by calling MIBSPI_init(), the application can open a MIBSPI instance by calling MIBSPI_open(). Please note that opening MIBSPI driver is taken care by the SysConfig generated code. This function iterates through the elements of the MIBSPI_config[] array, calling the element's device implementation MIBSPI initialization function. Please note that initializing MIBSPI driver is taken care by the SysConfig generated code.

If no MIBSPI_OpenParams structure is passed to MIBSPI_open(), default values are used. If the open call is successful, it returns a non-NULL value.

MIBSPI Transfer Mode

The MIBSPI driver supports two transfer modes of operation: blocking and callback. The transfer mode is determined by the MIBSPI_OpenParams.transferMode parameter. The MIBSPI driver defaults to blocking mode, if the application does not set it. Once a MIBSPI driver is opened, the only way to change the operation mode is to close and re-open the MIBSPI instance with the new transfer mode.

In blocking mode, a task's code execution is blocked until a MIBSPI transaction has completed or a timeout has occurred. This ensures that only one MIBSPI transfer operates at a given time. Other tasks requesting MIBSPI transfers while a transfer is currently taking place will receive a error return value. If a timeout occurs the transfer is cancelled, the task is unblocked & will receive a error return value. The transaction count field will have the amount of frames which were transferred successfully before the timeout. In blocking mode, transfers cannot be performed in software or hardware ISR context.

In callback mode, a MIBSPI transaction functions asynchronously, which means that it does not block code execution. After a MIBSPI transaction has been completed, the MIBSPI driver calls a user-provided hook function. Callback mode is supported in the execution context of tasks and hardware interrupt routines.

MIBSPI Frame Formats and Data Size

The MIBSPI driver can configure the device's MIBSPI peripheral to transfer data in several MIBSPI format options: MIBSPI (with various polarity and phase settings). The frame format is set with MIBSPI_OpenParams.frameFormat.

The smallest single unit of data transmitted onto the MIBSPI bus is called a MIBSPI frame and is of size MIBSPI_OpenParams.dataSize. A series of MIBSPI frames transmitted/received on a MIBSPI bus is referred to as a MIBSPI transaction.

MIBSPI Transactions

A MIBSPI transaction consists of a series of MIBSPI frames transmitted/received on a MIBSPI bus. A MIBSPI transaction is performed using MIBSPI_transfer(). MIBSPI_transfer() accepts a pointer to a MIBSPI_Transaction structure that dictates the quantity of data to be sent and received. The MIBSPI_Transaction.txBuf and MIBSPI_Transaction.rxBuf are both pointers to data buffers. The optional MIBSPI_Transaction.arg variable can only be used when the MIBSPI driver has been opened in callback mode. This variable is used to pass a user-defined value into the user-defined callback function.

MIBSPI_transfer() always performs full-duplex MIBSPI transactions. This means the MIBSPI simultaneously receives data as it transmits data. The application is responsible for formatting the data to be transmitted as well as determining whether the data received is meaningful. Specifics about MIBSPI frame formatting and data sizes are provided in device-specific data sheets and technical reference manuals.

Important Usage Guidelines

  • The MIBSPI protocol does not account for a built-in handshaking mechanism and neither does this driver. Therefore, when operating in PERIPHERAL mode, the application must provide such a mechanism to ensure that the MIBSPI peripheral is ready for the MIBSPI controller. The MIBSPI peripheral must call MIBSPI_transfer() before the controller starts transmitting. Some example application mechanisms could include:
    • Timed delays on the MIBSPI controller to guarantee the MIBSPI peripheral is ready for a MIBSPI transaction.
    • A form of GPIO flow control from the peripheral to the MIBSPI controller to notify the controller when ready.

Example Usage

Include the below file to access the APIs

#include <drivers/mibspi.h>

Instance Open Example

MIBSPI_OpenParams spiParams;
MIBSPI_Params_init(&spiParams); /* Initialize SPI parameters */
gMibspiHandle = MIBSPI_open(CONFIG_MIBSPI0, &spiParams);
DebugP_assert(gMibspiHandle != NULL);

Instance Close Example

MIBSPI_close(gMibspiHandle);

Blocking Transfer Example

int32_t transferOK;
MIBSPI_Transaction spiTransaction;
uint8_t transmitBuffer[APP_MIBSPI_MSGSIZE];
uint8_t receiveBuffer[APP_MIBSPI_MSGSIZE];
/* Fill in transmitBuffer */
spiTransaction.count = APP_MIBSPI_MSGSIZE;
spiTransaction.txBuf = (void *)transmitBuffer;
spiTransaction.rxBuf = (void *)receiveBuffer;
spiTransaction.slaveIndex = 0U;
spiTransaction.arg = NULL;
/* Initiate transfer */
transferOK = MIBSPI_transfer(gMibspiHandle, &spiTransaction);
if((SystemP_SUCCESS != transferOK) ||
(MIBSPI_TRANSFER_COMPLETED != spiTransaction.status))
{
/* MIBSPI transfer failed!! */
DebugP_assert(FALSE);
}

Non-Blocking Transfer Example

void App_callbackFxn(MIBSPI_Handle handle,
MIBSPI_Transaction *transaction)
{
if((NULL != transaction) &&
(MIBSPI_TRANSFER_COMPLETED == transaction->status))
{
semObj = (SemaphoreP_Object *) transaction->arg;
if(NULL != semObj)
{
SemaphoreP_post(semObj);
}
}
}
void transfer_nonblocking(void)
{
int32_t status;
int32_t transferOK;
MIBSPI_OpenParams spiParams;
MIBSPI_Transaction spiTransaction;
uint8_t transmitBuffer[APP_MIBSPI_MSGSIZE];
uint8_t receiveBuffer[APP_MIBSPI_MSGSIZE];
MIBSPI_Params_init(&spiParams); /* Initialize SPI parameters */
spiParams.transferCallbackFxn = &App_callbackFxn;
gMibspiHandle = MIBSPI_open(CONFIG_MIBSPI0, &spiParams);
DebugP_assert(gMibspiHandle != NULL);
/* Fill in transmitBuffer */
spiTransaction.count = APP_MIBSPI_MSGSIZE;
spiTransaction.txBuf = (void *)transmitBuffer;
spiTransaction.rxBuf = (void *)receiveBuffer;
spiTransaction.slaveIndex = 0U;
spiTransaction.arg = &gMibspiISRDoneSem;;
/* Initiate transfer */
transferOK = MIBSPI_transfer(gMibspiHandle, &spiTransaction);
/* Wait for callback */
status = SemaphoreP_pend(&gMibspiISRDoneSem, SystemP_WAIT_FOREVER);
}

API

APIs for MIBSPI

MIBSPI_Params_init
static void MIBSPI_Params_init(MIBSPI_OpenParams *openPrms)
Function to initialize the MIBSPI_OpenParams struct to its defaults.
Definition: mibspi/v0/mibspi.h:808
MIBSPI_Transaction
MIBSPI_Transaction data structure is used with MIBSPI_transfer(). It indicates how many MIBSPI_FrameF...
Definition: mibspi/v0/mibspi.h:381
MIBSPI_Transaction::rxBuf
void * rxBuf
Definition: mibspi/v0/mibspi.h:385
MIBSPI_transfer
int32_t MIBSPI_transfer(MIBSPI_Handle handle, MIBSPI_Transaction *transaction)
Function to perform MIBSPI transactions on a instance of a MIBSPI peripheral specified by the MIBSPI ...
mibspi.h
SystemP_WAIT_FOREVER
#define SystemP_WAIT_FOREVER
Value to use when needing a timeout of infinity or wait forver until resource is available.
Definition: SystemP.h:83
MIBSPI_Handle
void * MIBSPI_Handle
A handle that is returned from a MIBSPI_open() call.
Definition: mibspi/v0/mibspi.h:77
MIBSPI_TRANSFER_COMPLETED
@ MIBSPI_TRANSFER_COMPLETED
Definition: mibspi/v0/mibspi.h:159
MIBSPI_open
MIBSPI_Handle MIBSPI_open(uint32_t index, MIBSPI_OpenParams *params)
This function opens a given instance of the MIBSPI peripheral.
MIBSPI_Transaction::txBuf
void * txBuf
Definition: mibspi/v0/mibspi.h:384
MIBSPI_MODE_BLOCKING
@ MIBSPI_MODE_BLOCKING
Definition: mibspi/v0/mibspi.h:215
MIBSPI_close
void MIBSPI_close(MIBSPI_Handle handle)
Function to close a instance of a MIBSPI peripheral specified by the MIBSPI handle.
SystemP_SUCCESS
#define SystemP_SUCCESS
Return status when the API execution was successful.
Definition: SystemP.h:56
MIBSPI_Transaction::slaveIndex
uint8_t slaveIndex
Definition: mibspi/v0/mibspi.h:389
MIBSPI_OpenParams::transferMode
MIBSPI_TransferMode transferMode
Definition: mibspi/v0/mibspi.h:470
SemaphoreP_post
void SemaphoreP_post(SemaphoreP_Object *obj)
Post a semaphore object or unlock a mutex.
MIBSPI_OpenParams
MIBSPI Parameters.
Definition: mibspi/v0/mibspi.h:468
MIBSPI_Transaction::arg
void * arg
Definition: mibspi/v0/mibspi.h:386
SemaphoreP_Object
Opaque semaphore object used with the semaphore APIs.
Definition: SemaphoreP.h:59
MIBSPI_OpenParams::transferCallbackFxn
MIBSPI_CallbackFxn transferCallbackFxn
Definition: mibspi/v0/mibspi.h:474
MIBSPI_Transaction::status
MIBSPI_Status status
Definition: mibspi/v0/mibspi.h:388
DebugP_assert
#define DebugP_assert(expression)
Function to call for assert check.
Definition: DebugP.h:159
MIBSPI_Transaction::count
uint32_t count
Definition: mibspi/v0/mibspi.h:383
MIBSPI_MODE_CALLBACK
@ MIBSPI_MODE_CALLBACK
Definition: mibspi/v0/mibspi.h:220
SemaphoreP_pend
int32_t SemaphoreP_pend(SemaphoreP_Object *obj, uint32_t timeToWaitInTicks)
Pend on a semaphore object or lock a mutex.