In the following document and in TIFS-MCU document the term used to refer to the Firmware which runs on HSM core is TIFS-MCU Firmware. Please note that the terms 1.**HSMRt Firmware** and 2.**HSMRt** are synonymous to TIFS-MCU Firmware.
Introduction
The objective of HSM client is to provide APIs for accessing HSM services. Below given model explains the use of HSM client graphically. It uses SIPC Notify driver as a low level message passing mechanism to talk to HSM M4 core. HSM client APIs can be used with either FreeRTOS or noRTOS application.
The HSM Server provides APIs that will read the incoming request in the form of SIPC message and provide appropriate service based on it. The application which uses HSM server is also known as TIFS-MCU (HSM runtime firmware).
HSM CLIENT communication model
Along side providing services at runtime TIFS-MCU also enables secure boot flow. It is responsible for decrypting and authenticating R5Fs application images and sends a notification to SBL if it is a valid app image , later SBL will boot the R5 applications to respective cores.
The trusted R5Fs cores which can communicate with HSM are known as Secure hosts.
Following services are supported in MCU+SDK v8.4.0
BootNotify -: A special message sent by TIFS-MCU Firmware to indicate SBL that TIFS-MCU boot was successful.
GetVersion -: Get The current version of TIFS-MCU Firmware.
Debug Services -: For (HS-SE) device only. By default debug port for all R5F and HSM is closed. Secure R5Fs can request debug port access via runtime Debug services.
HSM Client message format.
Which R5 cores are going to be secure hosts will be decided by sysconfig configurations of TIFS-MCU at compile time and user has to make sure that similar configurations is done on the R5F side as well.
Below mentioned is the Message structure defined by SIPC Notify driver. HSM client populates a SIPC message with relevant parameters and sends this message to HSM Server.
SIPC message structure
Message structure description.
DestClientID -: Client Id to which a message is going to be sent. In case of R5F -> HSM ( R5 send message to HSM ) this field will always be equal to 1 because TIFS-MCU is a NORTOS application and only one client is required.
SrcClientID -: Client Id from which a message is going to be sent. In case of HSM -> R5F( HSM send message to R5 ) this field will always be equal to 1.
flags -: Used for ACK and NACK response signals based on weather a request has been processed correctly or not.
Client side signals 1. AOP -> ACK on process 2. NOP -> No ACK on process
Server side signals 1. ACK -> request processed successfully 2. NACK -> request process failure.
Service_type -: Type of a requested service.
Pointer_to_args -: Pointer to the arguments required by a particular service.
CRC16(args) -: CRC16 to check the integrity of arguments.
CRC16(msg) -: CRC16 to check the integrity of message.
The argument will reside in OCRAM and only its pointer is going to be passed in the message itself. When HSM receive the message it reads the argument content from OCRAM and process it. Thus other information needed by HSM server can be passed along with the message through HSM MBOX.
Note
It is strongly suggested that user application must cleary define a boundary between secure R5FSS and non secure R5FSS core's OCRAM memory so that non secure core cannot access the parameters of HSM message. One way to define such boundary is to protect some predefined memory region in OCRAM with firewalls so that only secure cores can access this particular memory region.
HSM client Initialization.
User needs to add an instance of HSM client in Secure R5F's sysconfig configuration.
Select the Secure_host_id for the current secure R5F core.
Note
Make sure that SIPC Message Queue Depth, Number of secure Hosts fields are configured same as in HSM Server's sysconfig.
populate ReqMsg field of HsmClient_t with appropriate paramters.
ReqMsg → destClientId = 0
ReqMsg → srcClientId = current client ID.
ReqMsg → serType = supported service MACRO.
ReqMsg → flags = AOP if ack is expected otherwise NAOP
ReqMsg → args = pointer to message structure based on service type.
ReqMsg → crcArgs = crc of args which is in OCRAM
ReqMsg → crcMsg = crc of the ReqMsg without crcMsg field.
Use SIPC_sendMsg() Api to send the 13 byte message to HSM.
If HSM_FLAG_AOP flag is selected then pend on HsmClient_t::Semaphore till timeout exception occurs or a Response message is received. If HSM_FLAG_NAOP flag is passed then server will not respond with message.
HsmClient_isr() will receive the response message and copy the same in to HsmClient_t::RespMsg and post the semaphore. As this ISR is blocking we want to quickly read the message and exit it.
check RespMsg integrity i.e CRC16 for HSM message and CRC16 for args. if integrity check fails then return SystemP_FAILURE.
If HSM_FLAG_ACK is received then returns SystemP_SUCCESS else SystemP_FAILURE.
HSM Client Load TIFS-MCU API and BootNotify message.
HSM client Module is used by SBL to load TIFS-MCU Fiwmware on HSM core.
SBL includes hsmRtImg.h file which contains TIFS-MCU Firmware in byte format, next the TIFS-MCU will be built along with SBL application.
SBL instantiates HSM client Module via sysconfig and calls HsmClient_loadHSMRtFirmware() which will load the TIFS-MCU Firmware.
After loading TIFS-MCU Firmware SBL application will wait for a HSM_MSG_BOOT_NOTIFY message from HSM server. This messages indicates that TIFS-MCU load is successfull and HSM Server is now ready to take requests from Secure R5F cores.
Similarly on the HSM side once the TIFS-MCU initialization sequence completes it calls HsmServer_sendBootNotify() API to send a BootNotify message.
Boot Notify sequence Flow chart.
Boot Notify sequence Flow chart
HsmClient_waitForBootNotify() API takes two parameters one of them is timeToWaitInTicks, This parameter defines how long SBL will wait for HSM_MSG_BOOT_NOTIFY message .User can change this parameter in SBL source code as per need.
Note
Currently the HsmClient_waitForBootNotify()'s timeToWaitInTicks paramter is set to SystemP_WAIT_FOREVER i.e SBL will keep waiting for HSM_MSG_BOOT_NOTIFY message indefinitely.
This service is used to get the current version of TIFS-MCUFirmware running on HSM core.
User needs to instantiate HsmVer_t object and call HsmClient_getVersion() API to get the current TIFS-MCU's version.
Refer to HsmVer_t_ for the description of different fields that defines a unique TIFS-MCU Firmware version. If User needs to know just the unique 64 bit version ID then, user should read HsmVer_t_::HsmrtVer a 64 bit field which combines all the different fields of HsmVer_t_.
HsmClient_getVersion() API takes timeToWaitInTicks parameter as input which dictates how long application will wait for the response from HSM core. If the timeout exception occurs HsmClient_getVersion() API return SystemP_TIMEOUT.
Example Usage
Demo code for HsmClient_init(). This will be autogenerated by sysconfig.
/*
* HSM Client
*/
/* memory assigned for each R5x <-> HSM channel */
As debug is closed for both HSM (M4) core and R5F cores in HS-SE device, this service is used to open debug firewall on device running TIFS-MCU Firmware.
User needs to create a signed certificate with correct cert type as a part of boot extensions, correct sw revision and correct UID in debug extensions.
User needs to instantiate a uint8_t * pointing to the certificate with certificate length and call HsmClient_openDbgFirewall() API to send the certificate to TIFS-MCU Firmware.
Example Usage
Registering HsmClient_t with client ID and requesting TIFS-MCU Firmware to open Debug Firewalls.