AM273x MCU+ SDK  08.03.00
MIBSPI_DMAXferSizeInfo Struct Reference

Detailed Description

MIBSPI Driver DMA module Transfer size definition.

Data structure used to exchange size of transaction between the MIBSPI driver and the SoC specific DMA engine implementation

Data Fields

uint16_t elemSize
 
uint16_t elemCnt
 
uint16_t frameCnt
 

Field Documentation

◆ elemSize

uint16_t MIBSPI_DMAXferSizeInfo::elemSize

Element Size of transfer in bytes

◆ elemCnt

uint16_t MIBSPI_DMAXferSizeInfo::elemCnt

Number of elements

◆ frameCnt

uint16_t MIBSPI_DMAXferSizeInfo::frameCnt

Number of frames of elemCnt