GPADC Driver Channel configuration.
The structure holds the channel confiiguration values
Data Fields | |
Bool | isChannelBufferedMode |
true if Channel is Buffer mode More... | |
uint32_t | channelConfigValue |
Channel Config value More... | |
GPADC_ParamInfoType | channelParamValue |
Channel Param type. More... | |
Bool | isChannelConfigured |
true if channel is configured More... | |
Bool GPADC_DriverChannelConfigType::isChannelBufferedMode |
true if Channel is Buffer mode
uint32_t GPADC_DriverChannelConfigType::channelConfigValue |
Channel Config value
GPADC_ParamInfoType GPADC_DriverChannelConfigType::channelParamValue |
Channel Param type.
Bool GPADC_DriverChannelConfigType::isChannelConfigured |
true if channel is configured