AM273x MCU+ SDK  08.03.00

Detailed Description

Transmit Packet scatter gather list entry.

This structure contains info on scatter-gather fragments used for trasmitting packets when packets are split into list of discontinuous fragments called scatter-gather list. Each sg list has a fragment of the packet

Data Fields

uint8_t * bufPtr
 
uint32_t filledLen
 
bool disableCacheOps
 

Field Documentation

◆ bufPtr

uint8_t* EnetCpdma_SGListEntry::bufPtr

Pointer to scatter fragment

◆ filledLen

uint32_t EnetCpdma_SGListEntry::filledLen

Length of valid data in the scatter fragment

◆ disableCacheOps

bool EnetCpdma_SGListEntry::disableCacheOps