AM273x MCU+ SDK  08.03.00
ESM_NotifyParams Struct Reference

Detailed Description

Parameters used to register the ESM notify function to handle Group1 and Group2 errors. The notify function will be invoked post the ESM FIQ interrupt handler processing.

Data Fields

uint32_t groupNumber
 
uint32_t errorNumber
 
uint32_t setIntrPriorityLvl
 
Bool enableInfluenceOnErrPin
 
void * arg
 
ESM_CallBack notify
 

Field Documentation

◆ groupNumber

uint32_t ESM_NotifyParams::groupNumber

Group number to which the following error number belongs.

◆ errorNumber

uint32_t ESM_NotifyParams::errorNumber

Error number for which the notify function is registered.

◆ setIntrPriorityLvl

uint32_t ESM_NotifyParams::setIntrPriorityLvl

Set the interrupt priority level to high or low. Applicable to Group 1 errors only.

◆ enableInfluenceOnErrPin

Bool ESM_NotifyParams::enableInfluenceOnErrPin

Enable failure influence on ERROR pin. Applicable to Group 1 errors only.

◆ arg

void* ESM_NotifyParams::arg

Argument passed back when the Notify function is invoked.

◆ notify

ESM_CallBack ESM_NotifyParams::notify

Notify function called by the ESM driver.