AM273x MCU+ SDK  08.03.00

Introduction

Macros that define values for the trigger mode of HWA paramsets.

Macros

#define HWA_THREAD_BACKGROUNDCONTEXT   ((uint8_t)0U)
 
#define HWA_THREAD_ALTCONTEXT   ((uint8_t)1U)
 

Macro Definition Documentation

◆ HWA_THREAD_BACKGROUNDCONTEXT

#define HWA_THREAD_BACKGROUNDCONTEXT   ((uint8_t)0U)

HWA background (low-priority thread)

◆ HWA_THREAD_ALTCONTEXT

#define HWA_THREAD_ALTCONTEXT   ((uint8_t)1U)

HWA context switch, ALT (high-priority) thread