AM273x MCU+ SDK  08.03.00

Introduction

@ brief Macros that define values for the various modes of the interference threshold mode in pre-processing block

Macros

#define HWA_INTERFTHRESH_MODE_MAG_OR_MAGDIF   ((uint8_t)0U) /** interference threshold magnitude or Magnitude difference */
 
#define HWA_INTERFTHRESH_MODE_MAGDIFF   ((uint8_t)1U) /** interference threshold only magnitude difference */
 
#define HWA_INTERFTHRESH_MODE_MAG   ((uint8_t)2U) /** interference threshold only magnitude */
 
#define HWA_INTERFTHRESH_MODE_MAG_AND_MAGDIFF   ((uint8_t)3U) /** interference threshold magnitude AND magnitude difference */
 

Macro Definition Documentation

◆ HWA_INTERFTHRESH_MODE_MAG_OR_MAGDIF

#define HWA_INTERFTHRESH_MODE_MAG_OR_MAGDIF   ((uint8_t)0U) /** interference threshold magnitude or Magnitude difference */

◆ HWA_INTERFTHRESH_MODE_MAGDIFF

#define HWA_INTERFTHRESH_MODE_MAGDIFF   ((uint8_t)1U) /** interference threshold only magnitude difference */

◆ HWA_INTERFTHRESH_MODE_MAG

#define HWA_INTERFTHRESH_MODE_MAG   ((uint8_t)2U) /** interference threshold only magnitude */

◆ HWA_INTERFTHRESH_MODE_MAG_AND_MAGDIFF

#define HWA_INTERFTHRESH_MODE_MAG_AND_MAGDIFF   ((uint8_t)3U) /** interference threshold magnitude AND magnitude difference */