This file contains the type definitions and function prototypes of the Enet Utils functionality.
Go to the source code of this file.
Data Structures | |
struct | EnetUtils_Cfg |
Enet utils parameters. More... | |
Macros | |
#define | container_of(ptr, type, member) |
Macro to get container structure from one of its members' addresses. More... | |
#define | ENET_UNUSED(x) (x = x) |
Unused variable. More... | |
#define | ENET_MK_ONES(c_ebit, c_sbit) (((1U << (((c_ebit) - (c_sbit)) + 1U)) - 1U) << (c_sbit)) |
Macro to create a bit mask. More... | |
#define | ENET_UTILS_ALIGN(x, y) ((((x) + ((y) - 1)) / (y)) * (y)) |
Align a value by performing a round-up operation. More... | |
#define | ENET_UTILS_IS_ALIGNED(addr, alignSz) (((uintptr_t)addr & ((alignSz) - 1U)) == 0U) |
Macro to determine if an address is aligned to a given size. More... | |
#define | ENET_UTILS_ARRAY_COPY(dst, src) |
Macro to copy arrays. They must be of the same size. More... | |
#define | Enet_assert(cond, ...) (void)(cond) |
Assertion. More... | |
#define | Enet_devAssert(cond, ...) (void)(cond) |
Development-time assertion. More... | |
#define | ENET_UTILS_COMPILETIME_ASSERT(cond) |
Compile-time assertion. More... | |
Typedefs | |
typedef void(* | Enet_Print) (const char *fmt,...) |
Info/debug print function prototype. More... | |
typedef uint64_t(* | Enet_VirtToPhys) (const void *virtAddr, void *appData) |
Virtual-to-physical address translation callback function. More... | |
typedef void *(* | Enet_PhysToVirt) (uint64_t phyAddr, void *appData) |
Physical-to-virtual address translation callback function. More... | |
Functions | |
void | EnetUtils_init (const EnetUtils_Cfg *cfg) |
Initialize utils module. More... | |
void | EnetUtils_deinit (void) |
De-initialize utils module. More... | |
void | EnetUtils_printf (const char *fmt,...) |
Print function. More... | |
void | EnetUtils_vprintf (const char *fmt, va_list args) |
Print function for va_list. More... | |
uint32_t | EnetUtils_min (uint32_t num1, uint32_t num2) |
Returns minimum of two numbers. More... | |
uint32_t | EnetUtils_max (uint32_t num1, uint32_t num2) |
Returns minimum of two numbers. More... | |
void | EnetUtils_delay (uint32_t delayVal) |
Busy loop for a given amount of cycles. More... | |
uint64_t | EnetUtils_virtToPhys (const void *virtAddr, void *appData) |
Convert a virtual address to physical address. More... | |
void * | EnetUtils_physToVirt (uint64_t physAddr, void *appData) |
Convert a physical address to virtual address. More... | |
EnetPhy_Mii | EnetUtils_macToPhyMii (const EnetMacPort_Interface *macMii) |
Convert MAC port MII to PHY MII types. More... | |
static void | EnetUtils_copyMacAddr (uint8_t *dst, const uint8_t *src) |
Copy MAC address. More... | |
static bool | EnetUtils_cmpMacAddr (const uint8_t *addr1, const uint8_t *addr2) |
Compare two MAC address. More... | |
static void | EnetUtils_clearMacAddr (uint8_t *addr) |
Clear MAC address. More... | |
static bool | EnetUtils_isMcastAddr (const uint8_t *addr) |
Check if address is multicast. More... | |
#define container_of | ( | ptr, | |
type, | |||
member | |||
) |
Macro to get container structure from one of its members' addresses.
#define ENET_UNUSED | ( | x | ) | (x = x) |
Unused variable.
#define ENET_MK_ONES | ( | c_ebit, | |
c_sbit | |||
) | (((1U << (((c_ebit) - (c_sbit)) + 1U)) - 1U) << (c_sbit)) |
Macro to create a bit mask.
#define ENET_UTILS_ALIGN | ( | x, | |
y | |||
) | ((((x) + ((y) - 1)) / (y)) * (y)) |
Align a value by performing a round-up operation.
#define ENET_UTILS_IS_ALIGNED | ( | addr, | |
alignSz | |||
) | (((uintptr_t)addr & ((alignSz) - 1U)) == 0U) |
Macro to determine if an address is aligned to a given size.
#define ENET_UTILS_ARRAY_COPY | ( | dst, | |
src | |||
) |
Macro to copy arrays. They must be of the same size.
#define Enet_assert | ( | cond, | |
... | |||
) | (void)(cond) |
Assertion.
#define Enet_devAssert | ( | cond, | |
... | |||
) | (void)(cond) |
Development-time assertion.
#define ENET_UTILS_COMPILETIME_ASSERT | ( | cond | ) |
Compile-time assertion.
typedef void(* Enet_Print) (const char *fmt,...) |
Info/debug print function prototype.
This function is used by the driver to print info/debug messages.
fmt | Formatted string followed by variable arguments |
typedef uint64_t(* Enet_VirtToPhys) (const void *virtAddr, void *appData) |
Virtual-to-physical address translation callback function.
This function is used by the driver to convert virtual address to physical address.
virtAddr | Virtual address |
appData | Callback pointer passed during translation |
typedef void*(* Enet_PhysToVirt) (uint64_t phyAddr, void *appData) |
Physical-to-virtual address translation callback function.
This function is used by the driver to convert physical address to virtual address.
phyAddr | Physical address |
appData | Callback pointer passed during translation |
void EnetUtils_init | ( | const EnetUtils_Cfg * | cfg | ) |
Initialize utils module.
Utils module initialization function. Should be only called from the Enet top-level module.
cfg | Pointer to the initialization parameters |
void EnetUtils_deinit | ( | void | ) |
De-initialize utils module.
void EnetUtils_printf | ( | const char * | fmt, |
... | |||
) |
Print function.
Prints the provided formatted string.
fmt | Formatted string followed by variable arguments |
void EnetUtils_vprintf | ( | const char * | fmt, |
va_list | args | ||
) |
Print function for va_list.
Prints the provided formatted string.
fmt | Formatted string |
args | Arg list pointing to the arguments in the format string |
uint32_t EnetUtils_min | ( | uint32_t | num1, |
uint32_t | num2 | ||
) |
Returns minimum of two numbers.
num1 | First number |
num2 | Second number |
uint32_t EnetUtils_max | ( | uint32_t | num1, |
uint32_t | num2 | ||
) |
Returns minimum of two numbers.
num1 | First number |
num2 | Second number |
void EnetUtils_delay | ( | uint32_t | delayVal | ) |
Busy loop for a given amount of cycles.
delayVal | Delay time |
uint64_t EnetUtils_virtToPhys | ( | const void * | virtAddr, |
void * | appData | ||
) |
Convert a virtual address to physical address.
virtAddr | Virtual address |
appData | Auxiliary data |
void* EnetUtils_physToVirt | ( | uint64_t | physAddr, |
void * | appData | ||
) |
Convert a physical address to virtual address.
physAddr | Physical address |
appData | Auxiliary data |
EnetPhy_Mii EnetUtils_macToPhyMii | ( | const EnetMacPort_Interface * | macMii | ) |
Convert MAC port MII to PHY MII types.
Converts MII type definition from EnetMacPort_Interface to EnetPhy_Mii.
macMii | MAC port MII interface type |
|
inlinestatic |
Copy MAC address.
Copies 6-byte MAC address.
dst | Pointer to MAC address memory being copied into |
src | Pointer to MAC address memory to be copied from |
|
inlinestatic |
Compare two MAC address.
Compares two MAC address to determine if they are equal.
addr1 | MAC address being compared |
addr2 | MAC address being compared |
|
inlinestatic |
Clear MAC address.
Clear 6-byte MAC address memory.
addr | Pointer to MAC address memory to be cleared |
|
inlinestatic |
Check if address is multicast.
Checks if MAC address is multicast.
addr | MAC address |