AM273x MCU+ SDK  08.03.00
enet_trace.h File Reference

Introduction

This file contains the type definitions and helper macros for the Enet Trace interface.

Go to the source code of this file.

Macros

#define ENET_CFG_TRACE_LEVEL_NONE   (0U)
 All traces disabled at build-time. More...
 
#define ENET_CFG_TRACE_LEVEL_ERROR   (1U)
 Build-time error level. More...
 
#define ENET_CFG_TRACE_LEVEL_WARN   (2U)
 Build-time warning level. More...
 
#define ENET_CFG_TRACE_LEVEL_INFO   (3U)
 Build-time information level. More...
 
#define ENET_CFG_TRACE_LEVEL_DEBUG   (4U)
 Build-time debug level. More...
 
#define ENET_CFG_TRACE_LEVEL_VERBOSE   (5U)
 Build-time verbose level. More...
 
#define ENET_CFG_TRACE_LEVEL   (ENET_CFG_TRACE_LEVEL_INFO)
 Default trace level if none is set. More...
 
#define ENET_CFG_TRACE_FORMAT_FUNC   (0U)
 Trace prefix: "<func>: string". More...
 
#define ENET_CFG_TRACE_FORMAT_FILE   (1U)
 Trace prefix: "<func>: <line>: string". More...
 
#define ENET_CFG_TRACE_FORMAT_FULL   (2U)
 Trace prefix: "<file>: <line>: <func>: <line>: string". More...
 
#define ENET_CFG_TRACE_TRACE_FORMAT   (ENET_CFG_TRACE_FORMAT_FUNC)
 Default trace format if none is specified. More...
 

Enumerations

enum  EnetTrace_TraceLevel {
  ENET_TRACE_NONE = 0U, ENET_TRACE_ERROR = 1U, ENET_TRACE_WARN = 2U, ENET_TRACE_INFO = 3U,
  ENET_TRACE_DEBUG = 4U, ENET_TRACE_VERBOSE = 5U
}
 Enumerates the types of trace level. More...