Available <0-8> external sources/channels could be selected by using bitmap of 9 bits in LSB. Ex: 0x01F is the bitmap for conversion of <0-4> external sources.
NOTE: All channels selected in the group bitmap must have channel configuration available during GPADC initialization for successful conversion without errors.
Data Fields | |
struct { | |
uint16_t b9_ChannelSelectionBitMap: 9 | |
Channel selection bitmap for triggering group GPADC conversion and getting results for the specified channels of the group. More... | |
uint16_t b7_Reserved: 7 | |
Reserved. More... | |
} | bits |
Channel selection bitmap bits. More... | |
uint16_t | b16_Val |
bits 16: 0 More... | |
uint16_t GPADC_channelsGroupSelectType::b9_ChannelSelectionBitMap |
Channel selection bitmap for triggering group GPADC conversion and getting results for the specified channels of the group.
uint16_t GPADC_channelsGroupSelectType::b7_Reserved |
Reserved.
struct { ... } GPADC_channelsGroupSelectType::bits |
Channel selection bitmap bits.
uint16_t GPADC_channelsGroupSelectType::b16_Val |
bits 16: 0