AM273x MCU+ SDK  08.02.00
MIBSPI_SlaveProfile Struct Reference

Detailed Description

MIBSPI slave profile Parameters.

When MIBSPI is configured as master mode, it may connect to multiple slaves. This data structure captures the the configurations for remote slaves.

Data Fields

uint8_t chipSelect
 
uint8_t ramBufLen
 
uint32_t dmaReqLine
 

Field Documentation

◆ chipSelect

uint8_t MIBSPI_SlaveProfile::chipSelect

CS0-CS7 signal number from 0 -7

◆ ramBufLen

uint8_t MIBSPI_SlaveProfile::ramBufLen

RAM Length in bytes that used by the slave

◆ dmaReqLine

uint32_t MIBSPI_SlaveProfile::dmaReqLine

DMA request line to be used for slave