AM273x MCU+ SDK  08.02.00

Detailed Description

Init time VLAN configuration.

Data Fields

bool aleVlanAwareMode
 
bool cpswVlanAwareMode
 
bool autoLearnWithVlan
 
bool unknownVlanNoLearn
 
uint32_t unknownForceUntaggedEgressMask
 
uint32_t unknownRegMcastFloodMask
 
uint32_t unknownUnregMcastFloodMask
 
uint32_t unknownVlanMemberListMask
 

Field Documentation

◆ aleVlanAwareMode

bool CpswAle_InitVlanCfg::aleVlanAwareMode

Configure ALE to operate in VLAN aware mode

◆ cpswVlanAwareMode

bool CpswAle_InitVlanCfg::cpswVlanAwareMode

Flag indicating if CPSW is in VLAN aware mode

◆ autoLearnWithVlan

bool CpswAle_InitVlanCfg::autoLearnWithVlan

Learn VLAN with address when autolearning addresses

◆ unknownVlanNoLearn

bool CpswAle_InitVlanCfg::unknownVlanNoLearn

Do not learn addresses with unknown VLAN

◆ unknownForceUntaggedEgressMask

uint32_t CpswAle_InitVlanCfg::unknownForceUntaggedEgressMask

Unknown VLAN Force Untagged Egress

◆ unknownRegMcastFloodMask

uint32_t CpswAle_InitVlanCfg::unknownRegMcastFloodMask

Unknown VLAN Registered Multicast Flood Mask

◆ unknownUnregMcastFloodMask

uint32_t CpswAle_InitVlanCfg::unknownUnregMcastFloodMask

Unknown VLAN Multicast Flood Mask

◆ unknownVlanMemberListMask

uint32_t CpswAle_InitVlanCfg::unknownVlanMemberListMask

Unknown VLAN Member List