AM273x MCU+ SDK  08.02.00

Detailed Description

CBUFF Statistics.

The structure describes the CBUFF statistics which can be used to determine the behavior of the CBUFF module.

Data Fields

uint32_t numFrameDone
 Number of frame done interrupts received: This is available only in the following cases: (a) Enable debug mode (b) Sessions with the Frame done callback If either of the above cases is not met the value of this is always 0. More...
 
uint32_t numChirpDone
 Number of chirp done interrupts received: This is available only in the following cases: (a) Enable debug mode (b) Sessions with the Frame done callback If either of the above cases is not met the value of this is always 0. More...
 
uint32_t numErrorInterrupts
 Number of error interrupts received. This is always available. More...
 
uint8_t frameStartError
 Flag which indicated if a frame start error was detected. This is always available. More...
 
uint8_t chirpError
 Flag which indicated if a chirp error was detected. This is always available. More...
 

Field Documentation

◆ numFrameDone

uint32_t CBUFF_Stats::numFrameDone

Number of frame done interrupts received: This is available only in the following cases: (a) Enable debug mode (b) Sessions with the Frame done callback If either of the above cases is not met the value of this is always 0.

See also
CBUFF_InitCfg_t::enableDebugMode
CBUFF_SessionCfg_t::frameDoneCallbackFxn

◆ numChirpDone

uint32_t CBUFF_Stats::numChirpDone

Number of chirp done interrupts received: This is available only in the following cases: (a) Enable debug mode (b) Sessions with the Frame done callback If either of the above cases is not met the value of this is always 0.

See also
CBUFF_InitCfg_t::enableDebugMode
CBUFF_SessionCfg_t::frameDoneCallbackFxn

◆ numErrorInterrupts

uint32_t CBUFF_Stats::numErrorInterrupts

Number of error interrupts received. This is always available.

◆ frameStartError

uint8_t CBUFF_Stats::frameStartError

Flag which indicated if a frame start error was detected. This is always available.

◆ chirpError

uint8_t CBUFF_Stats::chirpError

Flag which indicated if a chirp error was detected. This is always available.