AM273x MCU+ SDK  08.02.00
APIs for Debug log's and assert's

Introduction

For more details and example usage, see Debug

Data Structures

struct  DebugP_ShmLog
 Data structure describing log in shared memory. More...
 

Functions

void _DebugP_assert (int expression, const char *file, const char *function, int line, const char *expressionString)
 Actual function that is called for assert's by DebugP_assert. More...
 
void _DebugP_assertNoLog (int expression)
 Actual function that is called for assert's by DebugP_assertNoLog. More...
 
void _DebugP_logZone (uint32_t logZone, char *format,...)
 Function to log a string to the enabled console for a given zone. More...
 
uint32_t DebugP_logZoneEnable (uint32_t logZoneMask)
 Enable log zones. More...
 
uint32_t DebugP_logZoneDisable (uint32_t logZoneMask)
 Disable log zones. More...
 
void DebugP_logZoneRestore (uint32_t logZoneMask)
 Restire zone mask returned from DebugP_logZoneDisable or DebugP_logZoneEnable. More...
 
void DebugP_shmLogWriterInit (DebugP_ShmLog *shmLog, uint16_t selfCoreId)
 Initialize shared memory log writer for this core. More...
 
void DebugP_shmLogWriterPutChar (char character)
 Write a character to shared memory log. More...
 
void DebugP_uartLogWriterPutChar (char character)
 Write a character to UART terminal. More...
 
void DebugP_shmLogReaderInit (DebugP_ShmLog *shmLog, uint16_t numCores)
 Initialize log reader to read from shared memory and log to console via DebugP_log. More...
 
void DebugP_memLogWriterInit (uint16_t selfCoreId)
 Initialize log write to write to memory trace buffer. More...
 
void DebugP_memLogWriterPutChar (char character)
 Write a character to trace buffer. More...
 
void DebugP_uartSetDrvIndex (uint32_t uartDrvIndex)
 Set UART driver index to use for character read and write form UART. More...
 
int32_t DebugP_scanf (char *format,...)
 Read a formatted string from the selected UART driver. More...
 
int32_t DebugP_readLine (char *lineBuf, uint32_t bufSize)
 Read a string from the selected UART driver. More...
 

Macros

#define DebugP_SHM_LOG_SIZE   ( (2*1024U) - 16U)
 size of shared memory log for a CPU More...
 
#define DebugP_MEM_LOG_SIZE   ( 4*1024U )
 size of memory log for a CPU More...
 
#define DebugP_SHM_LOG_IS_VALID   (0x12345678U)
 Flag to indicate shared memory buffer is valid. More...
 

Debug log zones

#define DebugP_LOG_ZONE_ALWAYS_ON   (0x0001U)
 Flag for always on zone, enabled by default and recommend to not switch off. More...
 
#define DebugP_LOG_ZONE_ERROR   (0x0002U)
 Flag for error zone. More...
 
#define DebugP_LOG_ZONE_WARN   (0x0004U)
 Flag for warning zone. More...
 
#define DebugP_LOG_ZONE_INFO   (0x0008U)
 Flag for info zone. More...
 

Compile time log and assert enable, disable

#define DebugP_ASSERT_ENABLED   1
 Pre-processor define to enable or disable DebugP assert's. More...
 
#define DebugP_LOG_ENABLED   1
 Pre-processor define to enable or disable DebugP log's. More...
 

Debug assert APIs

#define DebugP_assert(expression)
 Function to call for assert check. More...
 
#define DebugP_assertNoLog(expression)   (_DebugP_assertNoLog(expression))
 Function to call for assert check, no logs are printed. More...
 

Debug log APIs

#define DebugP_log(format, ...)
 Function to log a string to the enabled console. More...
 
#define DebugP_logError(format, ...)
 Function to log a string to the enabled console, for error zone. More...
 
#define DebugP_logWarn(format, ...)
 Function to log a string to the enabled console, for warning zone. More...
 
#define DebugP_logInfo(format, ...)
 Function to log a string to the enabled console, for info zone. More...
 

Macro Definition Documentation

◆ DebugP_LOG_ZONE_ALWAYS_ON

#define DebugP_LOG_ZONE_ALWAYS_ON   (0x0001U)

Flag for always on zone, enabled by default and recommend to not switch off.

◆ DebugP_LOG_ZONE_ERROR

#define DebugP_LOG_ZONE_ERROR   (0x0002U)

Flag for error zone.

◆ DebugP_LOG_ZONE_WARN

#define DebugP_LOG_ZONE_WARN   (0x0004U)

Flag for warning zone.

◆ DebugP_LOG_ZONE_INFO

#define DebugP_LOG_ZONE_INFO   (0x0008U)

Flag for info zone.

◆ DebugP_SHM_LOG_SIZE

#define DebugP_SHM_LOG_SIZE   ( (2*1024U) - 16U)

size of shared memory log for a CPU

◆ DebugP_MEM_LOG_SIZE

#define DebugP_MEM_LOG_SIZE   ( 4*1024U )

size of memory log for a CPU

◆ DebugP_SHM_LOG_IS_VALID

#define DebugP_SHM_LOG_IS_VALID   (0x12345678U)

Flag to indicate shared memory buffer is valid.

Written by the writer after it has initialized and cleared by the reader after reader has initialized

◆ DebugP_ASSERT_ENABLED

#define DebugP_ASSERT_ENABLED   1

Pre-processor define to enable or disable DebugP assert's.

Set to 0 to disable assert checks and recompile all code where this file is included.

◆ DebugP_LOG_ENABLED

#define DebugP_LOG_ENABLED   1

Pre-processor define to enable or disable DebugP log's.

Set to 0 to disable logging and recompile all code where this file is included.

◆ DebugP_assert

#define DebugP_assert (   expression)
Value:
do { \
_DebugP_assert(expression, \
__FILE__, __FUNCTION__, __LINE__, #expression); \
} while(0)

Function to call for assert check.

If expresion evaluates to 0 then the function disable's interrupt and loops forever. It logs the file name and line number before looping forever. User should fix their code and run again.

This API should not be called within ISR context.

Parameters
expression[in] expression to check for.

◆ DebugP_assertNoLog

#define DebugP_assertNoLog (   expression)    (_DebugP_assertNoLog(expression))

Function to call for assert check, no logs are printed.

Same as DebugP_assert except no logs are printed. This can be used in very early initialization code and in ISRs.

During very early initialization and inside ISRs asserts with log will not work.

Parameters
expression[in] expression to check for.

◆ DebugP_log

#define DebugP_log (   format,
  ... 
)
Value:
do { \
_DebugP_logZone(DebugP_LOG_ZONE_ALWAYS_ON, format, ##__VA_ARGS__); \
} while(0)

Function to log a string to the enabled console.

This API should not be called within ISR context.

Parameters
format[in] String to log

◆ DebugP_logError

#define DebugP_logError (   format,
  ... 
)
Value:
do { \
_DebugP_logZone(DebugP_LOG_ZONE_ERROR, "ERROR: %s:%d: " format, __FUNCTION__, __LINE__, ##__VA_ARGS__); \
} while(0)

Function to log a string to the enabled console, for error zone.

This API should not be called within ISR context.

Parameters
format[in] String to log

◆ DebugP_logWarn

#define DebugP_logWarn (   format,
  ... 
)
Value:
do { \
_DebugP_logZone(DebugP_LOG_ZONE_WARN, "WARNING: %s:%d: " format, __FUNCTION__, __LINE__, ##__VA_ARGS__); \
} while(0)

Function to log a string to the enabled console, for warning zone.

This API should not be called within ISR context.

Parameters
format[in] String to log

◆ DebugP_logInfo

#define DebugP_logInfo (   format,
  ... 
)
Value:
do { \
_DebugP_logZone(DebugP_LOG_ZONE_INFO, "INFO: %s:%d: " format, __FUNCTION__, __LINE__, ##__VA_ARGS__); \
} while(0)

Function to log a string to the enabled console, for info zone.

This API should not be called within ISR context.

Parameters
format[in] String to log

Function Documentation

◆ _DebugP_assert()

void _DebugP_assert ( int  expression,
const char *  file,
const char *  function,
int  line,
const char *  expressionString 
)

Actual function that is called for assert's by DebugP_assert.

◆ _DebugP_assertNoLog()

void _DebugP_assertNoLog ( int  expression)

Actual function that is called for assert's by DebugP_assertNoLog.

◆ _DebugP_logZone()

void _DebugP_logZone ( uint32_t  logZone,
char *  format,
  ... 
)

Function to log a string to the enabled console for a given zone.

This API should not be used directly, instead DebugP_log, DebugP_logError, DebugP_logWarn, DebugP_logInfo should be used.

Parameters
logZone[in] Value from DebugP_LOG_ZONE
format[in] String ot log

◆ DebugP_logZoneEnable()

uint32_t DebugP_logZoneEnable ( uint32_t  logZoneMask)

Enable log zones.

Parameters
logZoneMask[in] Mask of values from DebugP_LOG_ZONE
Returns
old value of zone mask, can be used to restore original state using DebugP_logZoneRestore

◆ DebugP_logZoneDisable()

uint32_t DebugP_logZoneDisable ( uint32_t  logZoneMask)

Disable log zones.

Parameters
logZoneMask[in] Mask of values from DebugP_LOG_ZONE
Returns
old value of zone mask, can be used to restore original state using DebugP_logZoneRestore

◆ DebugP_logZoneRestore()

void DebugP_logZoneRestore ( uint32_t  logZoneMask)

Restire zone mask returned from DebugP_logZoneDisable or DebugP_logZoneEnable.

Parameters
logZoneMask[in] Mask of values from DebugP_LOG_ZONE

◆ DebugP_shmLogWriterInit()

void DebugP_shmLogWriterInit ( DebugP_ShmLog shmLog,
uint16_t  selfCoreId 
)

Initialize shared memory log writer for this core.

Parameters
shmLog[in] Address of shared memory where the writer should write logs to
selfCoreId[in] ID of core on which this API is called, this is used to add a core name prefix string to each log line, see CSL_CoreID

◆ DebugP_shmLogWriterPutChar()

void DebugP_shmLogWriterPutChar ( char  character)

Write a character to shared memory log.

If shared memory log buffer is full, nothing is written and character gets "dropped"

Internally, the charaxter is stored in a local line buffer and line buffer is flushed to shared memory only when a '\n' character is put.

Parameters
character[in] character to write

◆ DebugP_uartLogWriterPutChar()

void DebugP_uartLogWriterPutChar ( char  character)

Write a character to UART terminal.

   Make sure the UART to use is set via DebugP_uartSetDrvIndex().
   When using SysConfig this is done when UART debug log is enabled.
Parameters
character[in] character to write

◆ DebugP_shmLogReaderInit()

void DebugP_shmLogReaderInit ( DebugP_ShmLog shmLog,
uint16_t  numCores 
)

Initialize log reader to read from shared memory and log to console via DebugP_log.

The parameter shmLog is a array and is indexed using core ID as defined by CSL_CoreID

Parameters
shmLog[in] Array of addresses of shared memory where the reader should read from.
numCores[in] Number of entries in the shmLog array. Typically CSL_CORE_ID_MAX

◆ DebugP_memLogWriterInit()

void DebugP_memLogWriterInit ( uint16_t  selfCoreId)

Initialize log write to write to memory trace buffer.

Used when IPC with Linux is enabled OR ROV based logging is enabled

Parameters
selfCoreId[in] ID of core on which this API is called, this is used to add a core name prefix string to each log line, see CSL_CoreID

◆ DebugP_memLogWriterPutChar()

void DebugP_memLogWriterPutChar ( char  character)

Write a character to trace buffer.

Used when IPC with Linux is enabled OR ROV based logging is enabled

Internally, the charaxter is stored in a local line buffer and line buffer is flushed to UART only when a '\n' character is put.

Parameters
character[in] character to write

◆ DebugP_uartSetDrvIndex()

void DebugP_uartSetDrvIndex ( uint32_t  uartDrvIndex)

Set UART driver index to use for character read and write form UART.

   Make sure the UART to use is set via DebugP_uartSetDrvIndex().
   When using SysConfig this is done when UART debug log is enabled.
Parameters
uartDrvIndex[in] UART driver instance index to use

◆ DebugP_scanf()

int32_t DebugP_scanf ( char *  format,
  ... 
)

Read a formatted string from the selected UART driver.

   This function returns when a "new line" or "enter" is input on the console.

   Make sure the UART to use is set via DebugP_uartSetDrvIndex().
   When using SysConfig this is done when UART debug log is enabled.
Returns
SystemP_SUCCESS on sucessful read
SystemP_FAILURE on failure

◆ DebugP_readLine()

int32_t DebugP_readLine ( char *  lineBuf,
uint32_t  bufSize 
)

Read a string from the selected UART driver.

   This function returns when a "new line" or "enter" is input on the console.

   Make sure the UART to use for reading is set via DebugP_uartSetDrvIndex.
   When using SysConfig this is done when UART debug log is enabled.

   A '\0' is always put at the end.
Parameters
lineBuf[in] Buffer into which the string is read
bufSize[in] Size of the buffer in which to read, if buffer is not enough, input is truncated.
Returns
SystemP_SUCCESS on sucessful read
SystemP_FAILURE on failure
DebugP_LOG_ZONE_ERROR
#define DebugP_LOG_ZONE_ERROR
Flag for error zone.
Definition: DebugP.h:63
DebugP_LOG_ZONE_WARN
#define DebugP_LOG_ZONE_WARN
Flag for warning zone.
Definition: DebugP.h:67
DebugP_LOG_ZONE_INFO
#define DebugP_LOG_ZONE_INFO
Flag for info zone.
Definition: DebugP.h:71
DebugP_LOG_ZONE_ALWAYS_ON
#define DebugP_LOG_ZONE_ALWAYS_ON
Flag for always on zone, enabled by default and recommend to not switch off.
Definition: DebugP.h:59