AM273x MCU+ SDK  08.02.00

Introduction

Sub Modules

 CPDMA Configuration
 
 CPDMA Packet Definitions
 

Functions

int32_t EnetCpdma_rxThreshIsr (EnetDma_Handle hEnetDma)
 ENET CPDMA Rx Threshold interrupt service routine. More...
 
int32_t EnetCpdma_rxIsr (EnetDma_Handle hEnetDma)
 ENET CPDMA Rx interrupt service routine. More...
 
int32_t EnetCpdma_txIsr (EnetDma_Handle hEnetDma)
 ENET CPDMA Tx interrupt service routine. More...
 
int32_t EnetCpdma_miscIsr (EnetDma_Handle hEnetDma, uint32_t *pStatusMask)
 ENET CPDMA Miscellaneous interrupt service routine. More...
 
void EnetCpdma_initParams (Enet_Type enetType, EnetDma_Cfg *pDmaConfig)
 Initialize CPDMA config params. More...
 

Macros

#define ENET_CPDMA_CPSW_MAX_SG_LIST   (4U)
 

Enet CPDMA instance configuration

Configuration macros for Enet CPDMA module.

#define ENET_CPDMA_CPSW_MAX_TX_CH   (8U)
 Maximum number of CPSW TX DMA channels. More...
 
#define ENET_CPDMA_CPSW_MAX_RX_CH   (8U)
 Maximum number of CPSW RX DMA channels. More...
 

Enet DMA driver opaque handles

Enet DMA configuration structure.

Opaque handle typedefs for Enet DMA driver objects.

typedef struct EnetCpdma_Cfg_s EnetDma_Cfg
 Opaque handle that holds config Info for Enet DMA channel. More...
 
typedef void(* EnetDma_PktNotifyCb) (void *cbArg)
 Function pointer type for packet notify call back. More...
 

Macro Definition Documentation

◆ ENET_CPDMA_CPSW_MAX_TX_CH

#define ENET_CPDMA_CPSW_MAX_TX_CH   (8U)

Maximum number of CPSW TX DMA channels.

◆ ENET_CPDMA_CPSW_MAX_RX_CH

#define ENET_CPDMA_CPSW_MAX_RX_CH   (8U)

Maximum number of CPSW RX DMA channels.

◆ ENET_CPDMA_CPSW_MAX_SG_LIST

#define ENET_CPDMA_CPSW_MAX_SG_LIST   (4U)

Maximum number of scatter gather segements supported in a packet

Typedef Documentation

◆ EnetDma_Cfg

typedef struct EnetCpdma_Cfg_s EnetDma_Cfg

Opaque handle that holds config Info for Enet DMA channel.

◆ EnetDma_PktNotifyCb

typedef void(* EnetDma_PktNotifyCb) (void *cbArg)

Function pointer type for packet notify call back.

This is called by driver when packet is received on the RX channel or transmission completed from TX channel.

Function Documentation

◆ EnetCpdma_rxThreshIsr()

int32_t EnetCpdma_rxThreshIsr ( EnetDma_Handle  hEnetDma)

ENET CPDMA Rx Threshold interrupt service routine.

Processes Rx Threshold interrupt. This function retrieves the received packets from the linked CPPI descriptors and passes them to the receive queue when the number of received descriptors exceed the threshold

Requirement:

Parameters
hEnetDma[IN] Enet DMA Handle
Returns
Enet_ErrorCodes

◆ EnetCpdma_rxIsr()

int32_t EnetCpdma_rxIsr ( EnetDma_Handle  hEnetDma)

ENET CPDMA Rx interrupt service routine.

Processes Rx interrupt. This function retrieves the received packets from the linked CPPI descriptors and passes them to the receive queue when one or more packets has been received

Requirement:

Parameters
hEnetDma[IN] Enet DMA Handle
Returns
Enet_ErrorCodes

◆ EnetCpdma_txIsr()

int32_t EnetCpdma_txIsr ( EnetDma_Handle  hEnetDma)

ENET CPDMA Tx interrupt service routine.

Processes Tx interrupt. This function retrieves the completed Tx packets from the linked CPPI descriptors and passes them to the free queue when one or more packets have been transmitted.

Requirement:

Parameters
hEnetDma[IN] Enet DMA Handle
Returns
Enet_ErrorCodes

◆ EnetCpdma_miscIsr()

int32_t EnetCpdma_miscIsr ( EnetDma_Handle  hEnetDma,
uint32_t *  pStatusMask 
)

ENET CPDMA Miscellaneous interrupt service routine.

Processes Miscellaneous interrupt. This function extracts the intrrupt status bit masks from MMR and pass it to the caller to process all masked interrupts.

Requirement:

Parameters
hEnetDma[IN] Enet DMA Handle
pStatusMask[IN] pointer to the interrupt status bit mask
Returns
Enet_ErrorCodes

◆ EnetCpdma_initParams()

void EnetCpdma_initParams ( Enet_Type  enetType,
EnetDma_Cfg pDmaConfig 
)

Initialize CPDMA config params.

Initialize CPDMA config params to default values

Requirement:

Parameters
enetType[IN] Enet Type
pDmaConfig[IN] pointer to the config structure