AM273x MCU+ SDK  08.02.00
enet_mod_stats.h File Reference

Introduction

This file contains the type definitions and helper macros for the Enet Statistics module interface.

Go to the source code of this file.

Macros

#define ENET_STATS_PUBLIC_IOCTL(x)
 Helper macro to create IOCTL commands for STATS module. More...
 

Enumerations

enum  EnetStats_Ioctl {
  ENET_STATS_IOCTL_GET_VERSION = ENET_STATS_PUBLIC_IOCTL(0U), ENET_STATS_IOCTL_PRINT_REGS = ENET_STATS_PUBLIC_IOCTL(1U), ENET_STATS_IOCTL_GET_HOSTPORT_STATS = ENET_STATS_PUBLIC_IOCTL(2U), ENET_STATS_IOCTL_GET_MACPORT_STATS = ENET_STATS_PUBLIC_IOCTL(3U),
  ENET_STATS_IOCTL_RESET_HOSTPORT_STATS = ENET_STATS_PUBLIC_IOCTL(4U), ENET_STATS_IOCTL_RESET_MACPORT_STATS = ENET_STATS_PUBLIC_IOCTL(5U)
}
 Statistics IOCTL commands. More...