AM263x MCU+ SDK  26.00.00
OTFA_readRegion_t Struct Reference

Detailed Description

This is the OTFA Region structure which holds individual region specific information to be read from OTFA registers.

Data Fields

uint8_t regionNumber
 
uint8_t authMode
 
uint8_t encMode
 
uint8_t authKeyHash [64]
 
uint8_t encKeyHash [64]
 
uint32_t regionStAddr
 
uint32_t regionSize
 
uint16_t regionIV [16]
 

Field Documentation

◆ regionNumber

uint8_t OTFA_readRegion_t::regionNumber

◆ authMode

uint8_t OTFA_readRegion_t::authMode

◆ encMode

uint8_t OTFA_readRegion_t::encMode

◆ authKeyHash

uint8_t OTFA_readRegion_t::authKeyHash[64]

◆ encKeyHash

uint8_t OTFA_readRegion_t::encKeyHash[64]

◆ regionStAddr

uint32_t OTFA_readRegion_t::regionStAddr

◆ regionSize

uint32_t OTFA_readRegion_t::regionSize

◆ regionIV

uint16_t OTFA_readRegion_t::regionIV[16]