Structure holding the hs mmcsd controller system configurations.
Data Fields | |
uint32_t | clockActivity |
uint32_t | standbyMode |
uint32_t | idleMode |
uint32_t | enableWakeup |
uint32_t | enableAutoIdle |
uint32_t MMCSD_sysCfg::clockActivity |
Configuration of clock activity during wake up period. This can take values from the following enum MMCSD_clkAct.
uint32_t MMCSD_sysCfg::standbyMode |
standby mode configuration. This can take values from the following enum MMCSD_standbyMode.
uint32_t MMCSD_sysCfg::idleMode |
Idle mode configuration. This can take values from the following enum MMCSD_idleMode.
uint32_t MMCSD_sysCfg::enableWakeup |
Wake up enable/disable control. This can take following two values
uint32_t MMCSD_sysCfg::enableAutoIdle |
Auto idle enable/disable control. This can take following two values