AM263x MCU+ SDK  26.00.00
MMCSDLLD_Object Struct Reference

Detailed Description

MMCSD Driver Object.

Data Fields

uint32_t cmdErrorStat
 
uint32_t xferErrorStat
 
uint8_t * dataBufIdx
 
uint32_t dataBlockCount
 
uint32_t dataBlockSize
 
uint32_t remainingBlockCount
 
MMCSDLLD_Transaction * currentTxn
 
MMCSDLLD_Transaction mmcsdTxn
 
uint32_t setBusSpeed
 
uint32_t setBusWidth
 
uint8_t xferState
 
uint8_t state
 
MMCSDLLD_InitHandle initHandle
 
void * args
 
MMCSD_lld_transferCompleteCallback transferCompleteCallback
 

Field Documentation

◆ cmdErrorStat

uint32_t MMCSDLLD_Object::cmdErrorStat

Command Error Status

◆ xferErrorStat

uint32_t MMCSDLLD_Object::xferErrorStat

Transfer Error Status

◆ dataBufIdx

uint8_t* MMCSDLLD_Object::dataBufIdx

Data buffer index

◆ dataBlockCount

uint32_t MMCSDLLD_Object::dataBlockCount

Data Block count used for Transfer

◆ dataBlockSize

uint32_t MMCSDLLD_Object::dataBlockSize

Data Block size used for Transfer

◆ remainingBlockCount

uint32_t MMCSDLLD_Object::remainingBlockCount

Remaining Block Count

◆ currentTxn

MMCSDLLD_Transaction* MMCSDLLD_Object::currentTxn

Pointer to the current Transaction

◆ mmcsdTxn

MMCSDLLD_Transaction MMCSDLLD_Object::mmcsdTxn

MMCSDLLD_Transaction object used by driver

◆ setBusSpeed

uint32_t MMCSDLLD_Object::setBusSpeed

Set transfer Speed for the Device MMCSDSpeedModesSD

◆ setBusWidth

uint32_t MMCSDLLD_Object::setBusWidth

Set bus width MMCSDLLD_BusWidth

◆ xferState

uint8_t MMCSDLLD_Object::xferState

Stores the MMCSD Transaction state MMCSD_XferStates

◆ state

uint8_t MMCSDLLD_Object::state

Stores the MMCSD state MMCSD_DriverStates

◆ initHandle

MMCSDLLD_InitHandle MMCSDLLD_Object::initHandle

Initialization parameters of MMCSD instance

◆ args

void* MMCSDLLD_Object::args

Pointer to be used by application to store miscellaneous data

◆ transferCompleteCallback

MMCSD_lld_transferCompleteCallback MMCSDLLD_Object::transferCompleteCallback

Callback Function Pointer