AM263x MCU+ SDK  26.00.00
MCSPILLD_Object Struct Reference

Detailed Description

MCSPI driver object.

Data Fields

uint32_t baseAddr
 
uint32_t state
 
void * transferMutex
 
MCSPILLD_InitHandle hMcspiInit
 
uint32_t errorFlag
 
uint32_t transferChannel
 
uint32_t transferCsDisable
 
uint32_t transferDataSize
 
MCSPI_Transaction transaction
 
void * args
 

Field Documentation

◆ baseAddr

uint32_t MCSPILLD_Object::baseAddr

Peripheral base address

◆ state

uint32_t MCSPILLD_Object::state

Driver state variable

◆ transferMutex

void* MCSPILLD_Object::transferMutex

Transfer Sync Sempahore - to signal transfer completion

◆ hMcspiInit

MCSPILLD_InitHandle MCSPILLD_Object::hMcspiInit

[IN] Initialization parameters of McSPI instance

◆ errorFlag

uint32_t MCSPILLD_Object::errorFlag

Variable to store different McSPI errors

◆ transferChannel

uint32_t MCSPILLD_Object::transferChannel

[IN] Channel number (chip select) to use for transfers

◆ transferCsDisable

uint32_t MCSPILLD_Object::transferCsDisable

[IN] TRUE/FALSE to disable CS(chip select) for transfers

◆ transferDataSize

uint32_t MCSPILLD_Object::transferDataSize

[IN] MCSPI data frame size in bits - valid values: 4 bits to 32 bits

◆ transaction

MCSPI_Transaction MCSPILLD_Object::transaction

Pointer to current transaction

◆ args

void* MCSPILLD_Object::args

Pointer to be used by application to store miscellaneous data.