AM263x MCU+ SDK  26.00.00

Detailed Description

This is a HSMClient type which holds the information needed by hsm client to communicate with HSM .

Data Fields

SemaphoreP_Object Semaphore
 
HsmMsg_t ReqMsg
 
HsmMsg_t RespMsg
 
uint8_t RespFlag
 
uint8_t ClientId
 

Field Documentation

◆ Semaphore

SemaphoreP_Object HsmClient_t::Semaphore

◆ ReqMsg

HsmMsg_t HsmClient_t::ReqMsg

Registered client will pend of this semaphore till it receives a response from HSM server.

◆ RespMsg

HsmMsg_t HsmClient_t::RespMsg

message frame that is to be passed to HSM server.

◆ RespFlag

uint8_t HsmClient_t::RespFlag

Stores a message frame received from HSM server.

◆ ClientId

uint8_t HsmClient_t::ClientId

Indicates weather a request has been Acked or Nacked by HSM server.