AM263x MCU+ SDK  09.02.00

Detailed Description

Transmit Packet scatter gather list entry.

This structure contains info on scatter-gather fragments used for trasmitting packets when packets are split into list of discontinuous fragments called scatter-gather list. Each sg list has a fragment of the packet

Data Fields

uint8_t * bufPtr
 
uint32_t segmentFilledLen
 
uint32_t segmentAllocLen
 
bool disableCacheOps
 

Field Documentation

◆ bufPtr

uint8_t* EnetCpdma_SGListEntry::bufPtr

Pointer to scatter fragment

◆ segmentFilledLen

uint32_t EnetCpdma_SGListEntry::segmentFilledLen

Length of valid data in the scatter fragment

◆ segmentAllocLen

uint32_t EnetCpdma_SGListEntry::segmentAllocLen

Length of allocated buffer for scatter fragment

◆ disableCacheOps

bool EnetCpdma_SGListEntry::disableCacheOps