AM263x MCU+ SDK  26.00.00
DeviceConfigRead_t Struct Reference

Detailed Description

This is device configuration read request structure passed to HSM core via SIPC as argument, these parameters are required by the service handler.

Parameters
configType[IN] Type of configuration to read (safety/security/debug/all)
configData[OUT] Pointer to buffer where device configuration will be stored
configSize[IN/OUT] Size of the configuration buffer in bytes (input), actual size returned (output)
configDataCRC[OUT] CRC of the configuration data returned by HSM

Data Fields

uint32_t configType
 
uint32_t * configData
 
uint32_t configSize
 
uint16_t configDataCRC
 

Field Documentation

◆ configType

uint32_t DeviceConfigRead_t::configType

◆ configData

uint32_t* DeviceConfigRead_t::configData

Type of configuration to read

◆ configSize

uint32_t DeviceConfigRead_t::configSize

Pointer to buffer for device configuration data

◆ configDataCRC

uint16_t DeviceConfigRead_t::configDataCRC

Size of configuration buffer (input), actual size (output)