AM263x MCU+ SDK  26.00.00

Detailed Description

Multicast entry type info apart from MAC address.

Data Fields

bool super
 
CpswAle_FwdStateLevel fwdState
 
uint32_t portMask
 
uint32_t numIgnBits
 

Field Documentation

◆ super

bool CpswAle_McastEntryInfo::super

Supervisory flag which indicates that this address can be received in port state other than Forwarding state

◆ fwdState

CpswAle_FwdStateLevel CpswAle_McastEntryInfo::fwdState

Forward state level

◆ portMask

uint32_t CpswAle_McastEntryInfo::portMask

Port bit mask that is returned with a found multicast destination address

◆ numIgnBits

uint32_t CpswAle_McastEntryInfo::numIgnBits

Number of bits in the address to ignore. Up to 10 least significant bits can be ignored to form a multicast address range