AM263x MCU+ SDK  26.00.00

Detailed Description

This is bank swap request structure passed to HSM core via SIPC as argument, these parameters are required by the service handler. Valid only for F29x family of devices.

Parameters
c29CpuIdC29 CPU for which flash banks are to be swapped
syncFlagSynchronisation flag, HSM waits for this flag to be set to a specific value within a given time period, post which HSM swaps the flash banks
timeoutTimeout period for which HSM is supposed to wait
c29CpuBankSwapValC29 CPU bankswap register value read before making swap request to HSM, used by C29 CPU only

Data Fields

uint8_t c29CpuId
 
uint8_t syncFlag
 
uint32_t timeout
 
uint32_t c29CpuBankSwapVal
 

Field Documentation

◆ c29CpuId

uint8_t BankSwapReq_t::c29CpuId

◆ syncFlag

uint8_t BankSwapReq_t::syncFlag

C29 CPU for which flash banks are to be swapped

◆ timeout

uint32_t BankSwapReq_t::timeout

Synchronisation flag used by HSM to initiate bank swap

◆ c29CpuBankSwapVal

uint32_t BankSwapReq_t::c29CpuBankSwapVal

Timeout period for which HSM is supposed to wait before exiting server function