AM263x MCU+ SDK  26.00.00

Introduction

Files

file  gptpbasetypes.h
 File contains base datatypes used, as per IEEE 802.1AS Standard Documentation.
 
file  gptpmasterclock.h
 file contains gptp master clock related functions.
 

Data Structures

struct  PortIdentity
 The portIdentity identifies a port of a time-aware system. More...
 
struct  ClockQuality
 The clock quality represents quality of clock. More...
 
struct  UInteger48
 48bit variable, lsb is 32 bits More...
 
struct  UInteger48m32
 48bit variable, msb is 32 bits More...
 
struct  UInteger112
 UInteger112 (802.1AS, 10.3.2 systemIdentity) More...
 
struct  UInteger224
 UInteger224 (802.1AS, 10.3.4 time-synchronization spanning tree priority vectors ) More...
 
struct  ScaledNs
 The ScaledNs type represents signed values of time and time interval in units of 2e-16 ns. More...
 
struct  UScaledNs
 The ScaledNs type represents unsigned values of time and time interval in units of 2^-16 ns. More...
 
struct  TimeInterval
 
struct  Timestamp
 The Timestamp type represents a positive time with respect to the epoch. More...
 
struct  ExtendedTimestamp
 802.1AS-rev ExtendedTimestamp More...
 

Functions

int gptpmasterclock_init (const char *shmem_name)
 initialize to get gptp clock from tsn_gptp daemon. if previously initialized, it will simply return 0. More...
 
int gptpmasterclock_close (void)
 close gptpmasterclcock More...
 
int gptpmasterclock_gm_domainIndex (void)
 return the domainIndex which is currently used as systeme wide gptp clock. More...
 
int64_t gptpmasterclock_getts64 (void)
 get 64-bit nsec unit ts of system wide gptp clock More...
 
int gptpmasterclock_wait_until_ts64 (int64_t tts, int64_t vclose, int64_t toofar)
 Wait until tts comes. More...
 
uint64_t gptpmasterclock_expand_timestamp (uint32_t timestamp)
 expand 32-bit nsec time to 64 bit with aligning to gptp clock. More...
 
uint64_t gptpmasterclock_expand_timestamp_ts64 (uint32_t timestamp, int64_t ts64)
 expand 32-bit nsec time to 64 bit with aligning to gptp clock at the time ts64. More...
 
int gptpmasterclock_gmchange_ind (void)
 get GM change indicator, the number is incremented whenever GM is changed More...
 
int gptpmasterclock_get_max_domains (void)
 get maximum number of domains More...
 
int gptpmasterclock_get_domain_ts64 (int64_t *ts64, int domainIndex)
 get a synchronized clock value on specific domain More...
 
void gptpmasterclock_dump_offset (void)
 print phase offset for all domains More...
 

Typedefs

typedef uint8_t ClockIdentity[CLOCK_IDENTITY_LENGTH]
 
typedef uint8_t Nibble
 Primitive data types specifications for IEEE 802.1AS. All non-primitive data types are derived from the primitive types, signed integers are represented as two's complement form. More...
 
typedef uint8_t Octet
 
typedef uint8_t Octet2[2]
 
typedef uint8_t Octet3[3]
 
typedef uint8_t Octet4[4]
 
typedef uint8_t Enumeration2
 
typedef uint8_t Enumeration4
 
typedef uint8_t Enumeration8
 
typedef uint16_t Enumeration16
 
typedef uint32_t Enumeration24
 
typedef uint8_t UInteger4
 

Enumerations

enum  TimeSource {
  ATOMIC_CLOCK = 0x10, GPS = 0x20, TERRESTRIAL_RADIO = 0x30, PTP = 0x40,
  NTP = 0x50, HAND_SET = 0x60, OTHER = 0x90, INTERNAL_OSCILLATOR = 0xA0
}
 the type of source of time used by a ClockMaster(802.1AS, 8.6.2.7 timeSource) More...
 
enum  PTPPortState { DisabledPort = 3, MasterPort = 6, PassivePort = 7, SlavePort = 9 }
 value of the port state (802.1AS 14.8.3 portState) More...
 
enum  gmsync_status_t { GMSYNC_UNSYNC =0, GMSYNC_SYNC, GMSYNC_SYNC_STABLE }
 

Macros

#define MAX_PATH_TRACE_N   179
 Macro to define maximum path trace. More...
 
#define CLOCK_IDENTITY_LENGTH   8
 Macro which defines Clock Identity Length. More...
 
#define SCALEDNS_FACTOR   0x10000
 
#define VALUE_DISABLED   0u
 
#define VALUE_ENABLED   1u
 

Macro Definition Documentation

◆ MAX_PATH_TRACE_N

#define MAX_PATH_TRACE_N   179

Macro to define maximum path trace.

Note
The maximum possible number is 179 based on specification we can set the maximum here and restrict the frame using MAX_PTP_PACKET instead
#define MAX_PATH_TRACE_N 179
See also
10.3.8.23 pathTrace

◆ CLOCK_IDENTITY_LENGTH

#define CLOCK_IDENTITY_LENGTH   8

Macro which defines Clock Identity Length.

◆ SCALEDNS_FACTOR

#define SCALEDNS_FACTOR   0x10000

◆ VALUE_DISABLED

#define VALUE_DISABLED   0u

◆ VALUE_ENABLED

#define VALUE_ENABLED   1u

Typedef Documentation

◆ ClockIdentity

typedef uint8_t ClockIdentity[CLOCK_IDENTITY_LENGTH]

◆ Nibble

typedef uint8_t Nibble

Primitive data types specifications for IEEE 802.1AS. All non-primitive data types are derived from the primitive types, signed integers are represented as two's complement form.

See the following Table
Data Types Definition
EnumerationN N-bit enumerated value
UIntegerN N-bit unsigned integer
Nibble 4-bit field not interpreted as a number
Octet 8-bit field not interpreted as a number
OctetN N-octet fiels not interpreted as a number
Double Double precision (64-bit) floating-point vlaue

◆ Octet

typedef uint8_t Octet

◆ Octet2

typedef uint8_t Octet2[2]

◆ Octet3

typedef uint8_t Octet3[3]

◆ Octet4

typedef uint8_t Octet4[4]

◆ Enumeration2

typedef uint8_t Enumeration2

◆ Enumeration4

typedef uint8_t Enumeration4

◆ Enumeration8

typedef uint8_t Enumeration8

◆ Enumeration16

typedef uint16_t Enumeration16

◆ Enumeration24

typedef uint32_t Enumeration24

◆ UInteger4

typedef uint8_t UInteger4

Enumeration Type Documentation

◆ TimeSource

enum TimeSource

the type of source of time used by a ClockMaster(802.1AS, 8.6.2.7 timeSource)

Enumerator
ATOMIC_CLOCK 
GPS 
TERRESTRIAL_RADIO 
PTP 
NTP 
HAND_SET 
OTHER 
INTERNAL_OSCILLATOR 

◆ PTPPortState

value of the port state (802.1AS 14.8.3 portState)

Note
IEEE1588-2019, initializing=1, faulty=2, disabled=3, listening=4, pre-master=5, master=6, passive=7, uncalibrated=8, slave=9
Enumerator
DisabledPort 
MasterPort 
PassivePort 
SlavePort 

◆ gmsync_status_t

Enumerator
GMSYNC_UNSYNC 
GMSYNC_SYNC 
GMSYNC_SYNC_STABLE 

Function Documentation

◆ gptpmasterclock_init()

int gptpmasterclock_init ( const char *  shmem_name)

initialize to get gptp clock from tsn_gptp daemon. if previously initialized, it will simply return 0.

Parameters
shmem_nameshared memory node name. set NULL to use the default
Returns
-1 on error, 0 on Successful initialization.
Note
argument 'shmem_name' will not be used in platforms that recommends against using shared memory (e.g GHS INTEGRITY). Pass NULL is such case.

◆ gptpmasterclock_close()

int gptpmasterclock_close ( void  )

close gptpmasterclcock

Returns
-1: on error, 0:on successfull

◆ gptpmasterclock_gm_domainIndex()

int gptpmasterclock_gm_domainIndex ( void  )

return the domainIndex which is currently used as systeme wide gptp clock.

Returns
domainIndex, -1: error

◆ gptpmasterclock_getts64()

int64_t gptpmasterclock_getts64 ( void  )

get 64-bit nsec unit ts of system wide gptp clock

Returns
>=0 on success, -1 on error

◆ gptpmasterclock_wait_until_ts64()

int gptpmasterclock_wait_until_ts64 ( int64_t  tts,
int64_t  vclose,
int64_t  toofar 
)

Wait until tts comes.

Returns
-1: error, 1:already passed, 2:in vclose, 3:farther than toofar seconds, 0:returns from nanosleep(has been waited to very close timing)
Parameters
ttstarget time in nano second unit
vclosenano second unit; treated as very close, and stop waiting even ttv is still in future
toofarnano second unit; treated as too far, and stop waiting

◆ gptpmasterclock_expand_timestamp()

uint64_t gptpmasterclock_expand_timestamp ( uint32_t  timestamp)

expand 32-bit nsec time to 64 bit with aligning to gptp clock.

Parameters
timestamptimestamp which we are going to convert into 32bit to 64 bit.
Returns
expanded time
Note
a range of -2.147 to 2.147 secconds can be correctly aligned

◆ gptpmasterclock_expand_timestamp_ts64()

uint64_t gptpmasterclock_expand_timestamp_ts64 ( uint32_t  timestamp,
int64_t  ts64 
)

expand 32-bit nsec time to 64 bit with aligning to gptp clock at the time ts64.

Parameters
timestamptimestamp which we are going to convert into 32bit to 64 bit.
ts64the gptp clock time that the timestamp will be aligned to.
Returns
expanded time
Note
a range of -2.147 to 2.147 secconds can be correctly aligned

◆ gptpmasterclock_gmchange_ind()

int gptpmasterclock_gmchange_ind ( void  )

get GM change indicator, the number is incremented whenever GM is changed

Returns
GM change indicator value, -1: on error

◆ gptpmasterclock_get_max_domains()

int gptpmasterclock_get_max_domains ( void  )

get maximum number of domains

Returns
returns available number of domains.

◆ gptpmasterclock_get_domain_ts64()

int gptpmasterclock_get_domain_ts64 ( int64_t *  ts64,
int  domainIndex 
)

get a synchronized clock value on specific domain

Parameters
ts64pointer to return clock value
domainIndexdomain index number
Returns
0 on success, -1 on error.

◆ gptpmasterclock_dump_offset()

void gptpmasterclock_dump_offset ( void  )

print phase offset for all domains