AM263x MCU+ SDK  26.00.00

Introduction

This module contains APIs to program and use DMA drivers available in the SoC with MCSPI.

Functions

int32_t MCSPI_lld_dmaInit (MCSPI_DmaHandle mcspiDmaHandle)
 API to open an MCSPI DMA channel. More...
 
int32_t MCSPI_lld_dmaDeInit (MCSPILLD_Handle hMcspi, const MCSPI_ChConfig *chCfg, uint32_t chCnt)
 API to close an MCSPI DMA channel. More...
 
int32_t MCSPI_lld_dmaChInit (MCSPILLD_Handle hMcspi, uint32_t chCnt)
 API to init a DMA Channel opened. More...
 
int32_t MCSPI_lld_dmaTransfer (MCSPILLD_Handle hMcspi, MCSPI_ChObject *chObj, const MCSPI_Transaction *transaction)
 API to do a DMA transfer using a specific DMA driver - UDMA, EDMA etc. More...
 
void MCSPI_lld_dmaStop (MCSPILLD_Handle hMcspi, MCSPI_ChObject *chObj, uint32_t chNum)
 API to Stop DMA using a specific DMA driver - UDMA, EDMA etc. More...
 

Function Documentation

◆ MCSPI_lld_dmaInit()

int32_t MCSPI_lld_dmaInit ( MCSPI_DmaHandle  mcspiDmaHandle)

API to open an MCSPI DMA channel.

This API will open a DMA Channel using the appropriate DMA driver callbacks and the registered via Sysconfig

Parameters
mcspiDmaHandle[in] MCSPILLD_Handle returned from MCSPI_open()
Returns
Handle to the MCSPI DMA Config Object

◆ MCSPI_lld_dmaDeInit()

int32_t MCSPI_lld_dmaDeInit ( MCSPILLD_Handle  hMcspi,
const MCSPI_ChConfig *  chCfg,
uint32_t  chCnt 
)

API to close an MCSPI DMA channel.

This API will open a DMA Channel using the appropriate DMA driver callbacks registered via Sysconfig

Parameters
hMcspi[in] MCSPILLD_Handle returned from MCSPI_open()
chCnt[in] Channel number
chCfg[in] Pointer to MCSPI_ChConfig. This parameter can't be NULL
Returns
MCSPI_STATUS_SUCCESS on success, else failure

◆ MCSPI_lld_dmaChInit()

int32_t MCSPI_lld_dmaChInit ( MCSPILLD_Handle  hMcspi,
uint32_t  chCnt 
)

API to init a DMA Channel opened.

This API will open a DMA Channel using the appropriate DMA driver callbacks registered via Sysconfig

Parameters
hMcspi[in] MCSPILLD_Handle returned from MCSPI_open()
chCnt[in] Channel number
Returns
MCSPI_STATUS_SUCCESS on success, else failure

◆ MCSPI_lld_dmaTransfer()

int32_t MCSPI_lld_dmaTransfer ( MCSPILLD_Handle  hMcspi,
MCSPI_ChObject *  chObj,
const MCSPI_Transaction *  transaction 
)

API to do a DMA transfer using a specific DMA driver - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
hMcspi[in] MCSPILLD_Handle returned from MCSPI_open()
chObj[in] Pointer to MCSPI_ChObject. This parameter can't be NULL
transaction[in] Pointer to MCSPI_Transaction. This parameter can't be NULL
Returns
MCSPI_STATUS_SUCCESS on success, else failure

◆ MCSPI_lld_dmaStop()

void MCSPI_lld_dmaStop ( MCSPILLD_Handle  hMcspi,
MCSPI_ChObject *  chObj,
uint32_t  chNum 
)

API to Stop DMA using a specific DMA driver - UDMA, EDMA etc.

Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.

Parameters
hMcspi[in] MCSPILLD_Handle returned from MCSPI_open()
chObj[in] Pointer to MCSPI_ChObject. This parameter can't be NULL
chNum[in] Channel number