AM263x MCU+ SDK  26.00.00

Introduction

TI DP83869 RGMII Ethernet PHY.

Data Structures

struct  Dp83869_Cfg
 DP83869 PHY configuration parameters. More...
 

Functions

void Dp83869_initCfg (Dp83869_Cfg *cfg)
 Initialize DP83869 PHY specific config params. More...
 
void Dp83869_bind (EthPhyDrv_Handle *hPhy, uint8_t phyAddr, Phy_RegAccessCb_t *pRegAccessCb)
 
bool Dp83869_isPhyDevSupported (EthPhyDrv_Handle hPhy, const void *pVersion)
 
bool Dp83869_isMacModeSupported (EthPhyDrv_Handle hPhy, Phy_Mii mii)
 
int32_t Dp83869_config (EthPhyDrv_Handle hPhy, const void *pExtCfg, const uint32_t extCfgSize, Phy_Mii mii, bool loopbackEn)
 
void Dp83869_reset (EthPhyDrv_Handle hPhy)
 
bool Dp83869_isResetComplete (EthPhyDrv_Handle hPhy)
 
void Dp83869_printRegs (EthPhyDrv_Handle hPhy)
 

Enumerations

enum  Dp83869_Gpio0Mode {
  DP83869_GPIO0_CLK_OUT = 0x0U, DP83869_GPIO0_INT = 0x2U, DP83869_GPIO0_LINK_STATUS = 0x3U, DP83869_GPIO0_TX_SFD = 0x5U,
  DP83869_GPIO0_RX_SFD = 0x6U, DP83869_GPIO0_WOL = 0x7U, DP83869_GPIO0_ED = 0x8U, DP83869_GPIO0_PRBS_ERR = 0x9U,
  DP83869_GPIO0_LED_2 = 0xAU, DP83869_GPIO0_LED_GPIO_3 = 0xBU, DP83869_GPIO0_CRS = 0xCU, DP83869_GPIO0_COL = 0xDU,
  DP83869_GPIO0_CONSTANT0 = 0xEU, DP83869_GPIO0_CONSTANT1 = 0xFU
}
 GPIO_0 mux modes. More...
 
enum  Dp83869_Gpio1Mode {
  DP83869_GPIO1_CLK_OUT = 0x0U, DP83869_GPIO1_INT = 0x2U, DP83869_GPIO1_LINK_STATUS = 0x3U, DP83869_GPIO1_TX_SFD = 0x5U,
  DP83869_GPIO1_RX_SFD = 0x6U, DP83869_GPIO1_WOL = 0x7U, DP83869_GPIO1_ED = 0x8U, DP83869_GPIO1_PRBS_ERR = 0x9U,
  DP83869_GPIO1_LED_2 = 0xAU, DP83869_GPIO1_LED_GPIO_3 = 0xBU, DP83869_GPIO1_CRS = 0xCU, DP83869_GPIO1_COL = 0xDU,
  DP83869_GPIO1_CONSTANT0 = 0xEU, DP83869_GPIO1_CONSTANT1 = 0xFU
}
 GPIO_1 mux modes. More...
 
enum  Dp83869_LedMode {
  DP83869_LED_LINKED = 0x0U, DP83869_LED_RXTXACT = 0x1U, DP83869_LED_TXACT = 0x2U, DP83869_LED_RXACT = 0x3U,
  DP83869_LED_COLLDET = 0x4U, DP83869_LED_LINKED_1000BT = 0x5U, DP83869_LED_LINKED_100BTX = 0x6U, DP83869_LED_LINKED_10BT = 0x7U,
  DP83869_LED_LINKED_10100BT = 0x8U, DP83869_LED_LINKED_1001000BT = 0x9U, DP83869_LED_FULLDUPLEX = 0xAU, DP83869_LED_LINKED_BLINKACT = 0xBU,
  DP83869_LED_RXTXERR = 0xDU, DP83869_LED_RXERR = 0xEU
}
 LED modes (sources). More...
 

Macros

#define DP83869_LED_NUM   (4U)
 Number of LEDs available in the PHY. More...
 

Macro Definition Documentation

◆ DP83869_LED_NUM

#define DP83869_LED_NUM   (4U)

Number of LEDs available in the PHY.

Enumeration Type Documentation

◆ Dp83869_Gpio0Mode

GPIO_0 mux modes.

Enumerator
DP83869_GPIO0_CLK_OUT 

Clock Out

DP83869_GPIO0_INT 

Interrupt

DP83869_GPIO0_LINK_STATUS 

Link Status

DP83869_GPIO0_TX_SFD 

Transmit SFD

DP83869_GPIO0_RX_SFD 

Receive SFD

DP83869_GPIO0_WOL 

Wake on LAN

DP83869_GPIO0_ED 
DP83869_GPIO0_PRBS_ERR 

PRBS Errors

DP83869_GPIO0_LED_2 

LED_2

DP83869_GPIO0_LED_GPIO_3 

LED_GPIO (3)

DP83869_GPIO0_CRS 

CRS

DP83869_GPIO0_COL 

COL

DP83869_GPIO0_CONSTANT0 

Constant 0

DP83869_GPIO0_CONSTANT1 

Constant 1

◆ Dp83869_Gpio1Mode

GPIO_1 mux modes.

Enumerator
DP83869_GPIO1_CLK_OUT 

Clock Out

DP83869_GPIO1_INT 

Interrupt

DP83869_GPIO1_LINK_STATUS 

Link Status

DP83869_GPIO1_TX_SFD 

Transmit SFD

DP83869_GPIO1_RX_SFD 

Receive SFD

DP83869_GPIO1_WOL 

Wake on LAN

DP83869_GPIO1_ED 
DP83869_GPIO1_PRBS_ERR 

PRBS Errors

DP83869_GPIO1_LED_2 

LED_2

DP83869_GPIO1_LED_GPIO_3 

LED_GPIO (3)

DP83869_GPIO1_CRS 

CRS

DP83869_GPIO1_COL 

COL

DP83869_GPIO1_CONSTANT0 

Constant 0

DP83869_GPIO1_CONSTANT1 

Constant 1

◆ Dp83869_LedMode

LED modes (sources).

Enumerator
DP83869_LED_LINKED 

Link established

DP83869_LED_RXTXACT 

Receive or transmit activity

DP83869_LED_TXACT 

Transmit activity

DP83869_LED_RXACT 

Receive activity

DP83869_LED_COLLDET 

Collision detected

DP83869_LED_LINKED_1000BT 

1000BT link established

DP83869_LED_LINKED_100BTX 

100 BTX link established

DP83869_LED_LINKED_10BT 

10BT link established

DP83869_LED_LINKED_10100BT 

10/100BT link established

DP83869_LED_LINKED_1001000BT 

100/1000BT link established

DP83869_LED_FULLDUPLEX 

Full duplex

DP83869_LED_LINKED_BLINKACT 

Link established, blink for transmit or receive activity

DP83869_LED_RXTXERR 

Receive error or transmit error

DP83869_LED_RXERR 

Receive error

Function Documentation

◆ Dp83869_initCfg()

void Dp83869_initCfg ( Dp83869_Cfg *  cfg)

Initialize DP83869 PHY specific config params.

Initializes the DP83869 PHY specific configuration parameters.

Parameters
cfgDP83869 PHY config structure pointer

◆ Dp83869_bind()

void Dp83869_bind ( EthPhyDrv_Handle *  hPhy,
uint8_t  phyAddr,
Phy_RegAccessCb_t *  pRegAccessCb 
)

◆ Dp83869_isPhyDevSupported()

bool Dp83869_isPhyDevSupported ( EthPhyDrv_Handle  hPhy,
const void *  pVersion 
)

◆ Dp83869_isMacModeSupported()

bool Dp83869_isMacModeSupported ( EthPhyDrv_Handle  hPhy,
Phy_Mii  mii 
)

◆ Dp83869_config()

int32_t Dp83869_config ( EthPhyDrv_Handle  hPhy,
const void *  pExtCfg,
const uint32_t  extCfgSize,
Phy_Mii  mii,
bool  loopbackEn 
)

◆ Dp83869_reset()

void Dp83869_reset ( EthPhyDrv_Handle  hPhy)

◆ Dp83869_isResetComplete()

bool Dp83869_isResetComplete ( EthPhyDrv_Handle  hPhy)

◆ Dp83869_printRegs()

void Dp83869_printRegs ( EthPhyDrv_Handle  hPhy)