AM263x MCU+ SDK  26.00.00
APIs for SOC Specific Functions

Introduction

For more details and example usage, see SOC

Sub Modules

 APIs for SOC Reset and Clock Functions
 
 APIs for SOC Xbars
 

Functions

static int32_t MCSPI_lld_isBaseAddrValid (uint32_t baseAddr)
 API to validate MCSPI base address. More...
 
static int32_t MMCSD_lld_isBaseAddrValid (uint32_t baseAddr)
 API to validate MMCSD base addresses. More...
 
int32_t SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable)
 Enable clock to specified module. More...
 
int32_t SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate)
 Set module clock to specified frequency. More...
 
const char * SOC_getCoreName (uint16_t coreId)
 Convert a core ID to a user readable name. More...
 
uint64_t SOC_getSelfCpuClk (void)
 Get the clock frequency in Hz of the CPU on which the driver is running. More...
 
void SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition)
 Lock control module partition to prevent writes into control MMRs. More...
 
void SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition)
 Unlock control module partition to allow writes into control MMRs. More...
 
void SOC_setEpwmTbClk (uint32_t epwmInstance, uint32_t enable)
 Enable or disable ePWM time base clock from Control MMR. More...
 
void SOC_setMultipleEpwmTbClk (uint32_t epwmMask, uint32_t enable)
 Enable or disable Multiple ePWM time base clock from Control MMR. More...
 
void SOC_enableAdcReference (uint32_t adcInstance)
 Enable ADC references by writing to Control MMR. More...
 
void SOC_enableAdcInternalReference (uint32_t adcInstance, uint32_t enable)
 Enables the ADC internal reference. More...
 
void SOC_enableAdcReferenceMonitor (uint32_t adcInstance, uint32_t enable)
 Enable ADC reference Monitors by writing to Control MMR. More...
 
uint32_t SOC_getAdcReferenceStatus (uint32_t adcInstance)
 Gets the Reference status. More...
 
void SOC_setEpwmGroup (uint32_t epwmInstance, uint32_t group)
 Configure the ePWM group. More...
 
void SOC_selectSdfm1Clk0Source (uint8_t source)
 Select the SDFM1 CLK0 source. More...
 
void SOC_gateEpwmClock (uint32_t epwmInstance)
 Gate the ePWM clock. More...
 
void SOC_ungateEpwmClock (uint32_t epwmInstance)
 Ungate the ePWM clock. More...
 
void SOC_gateFsitxClock (uint32_t fsitxInstance)
 Gate the FSI-TX clock. More...
 
void SOC_gateFsirxClock (uint32_t fsirxInstance)
 Gate the FSI-RX clock. More...
 
void SOC_gateCmpssaClock (uint32_t cmpssaInstance)
 Gate the CMPSS-A clock. More...
 
void SOC_ungateCmpssaClock (uint32_t cmpssaInstance)
 Ungate the CMPSS-A clock. More...
 
void SOC_gateCmpssbClock (uint32_t cmpssbInstance)
 Gate the CMPSS-B clock. More...
 
void SOC_ungateCmpssbClock (uint32_t cmpssbInstance)
 Ungate the CMPSS-B clock. More...
 
void SOC_gateEcapClock (uint32_t ecapInstance)
 Gate the ECAP clock. More...
 
void SOC_ungateEcapClock (uint32_t ecapInstance)
 Ungate the ECAP clock. More...
 
void SOC_gateEqepClock (uint32_t eqepInstance)
 Gate the EQEP clock. More...
 
void SOC_ungateEqepClock (uint32_t eqepInstance)
 Ungate the EQEP clock. More...
 
void SOC_gateSdfmClock (uint32_t sdfmInstance)
 Gate the SDFM clock. More...
 
void SOC_ungateSdfmClock (uint32_t sdfmInstance)
 Ungate the SDFM clock. More...
 
void SOC_gateDacClock (void)
 Gate the DAC clock. More...
 
void SOC_ungateDacClock (void)
 Ungate the DAC clock. More...
 
void SOC_gateAdcClock (uint32_t adcInstance)
 Gate the ADC clock. More...
 
void SOC_ungateAdcClock (uint32_t adcInstance)
 ungate the ADC clock More...
 
void SOC_gateOttoClock (uint32_t ottoInstance)
 Gate the OTTO clock. More...
 
void SOC_ungateOttoClock (uint32_t ottoInstance)
 Ungate the OTTO clock. More...
 
void SOC_gateSdfmPllClock (uint32_t sdfmInstance)
 Gate the SDFM PLL clock. More...
 
void SOC_ungateSdfmPllClock (uint32_t sdfmInstance)
 Ungate the SDFM PLL clock. More...
 
void SOC_gateFsiPllClock (uint32_t fsiInstance)
 Gate the FSI-TX PLL clock. More...
 
void SOC_generateEpwmReset (uint32_t ePWMInstance)
 Generate ePWM reset. More...
 
void SOC_generateFsiTxReset (uint32_t fsitxInstance)
 Generate FSI-TX reset. More...
 
void SOC_generateFsiRxReset (uint32_t fsirxInstance)
 Generate FSI-RX reset. More...
 
void SOC_generateCmpssaReset (uint32_t cmpssaInstance)
 Generate CMPSS-A reset. More...
 
void SOC_generateCmpssbReset (uint32_t cmpssbInstance)
 Generate CMPSS-B reset. More...
 
void SOC_generateEcapReset (uint32_t ecapInstance)
 Generate ECAP reset. More...
 
void SOC_generateEqepReset (uint32_t eqepInstance)
 Generate EQEP reset. More...
 
void SOC_generateSdfmReset (uint32_t sdfmInstance)
 Generate SDFM reset. More...
 
void SOC_generateDacReset (void)
 Generate DAC reset. More...
 
void SOC_generateAdcReset (uint32_t adcInstance)
 Generate ADC reset. More...
 
void Soc_enableEPWMHalt (uint32_t epwmInstance)
 Halt EPWM with corresponding cPU. More...
 
void Soc_disableEPWMHalt (uint32_t epwmInstance)
 Halt EPWM with corresponding cPU. More...
 
void Soc_enableECAPHalt (uint32_t ecapInstance)
 Halt ECAP with corresponding cPU. More...
 
void Soc_disableECAPHalt (uint32_t ecapInstance)
 Halt ECAP with corresponding cPU. More...
 
void SOC_generateOttoReset (uint32_t ottoInstance)
 Generate OTTO reset. More...
 
void SOC_selectIcssGpiMux (uint8_t pru_instance, uint32_t mask)
 Selection of ICSS GPI MUX. More...
 
void SOC_setResetCPSWBit ()
 Setting CPSW hard reset Bit. More...
 
void SOC_clearResetCPSWBit ()
 Clearing CPSW hard reset bit. More...
 
uint64_t SOC_virtToPhy (void *virtAddr)
 SOC Virtual (CPU) to Physical address translation function. More...
 
void * SOC_phyToVirt (uint64_t phyAddr)
 Physical to Virtual (CPU) address translation function. More...
 
void SOC_configSlewRate (uint32_t baseAddr, uint32_t bankNum, uint32_t groupNum, uint32_t samplePeriod)
 Configure GPIO pin Slew rate. More...
 
static int32_t UART_IsBaseAddrValid (uint32_t baseAddr)
 Macro to validate UART base address. More...
 
uint32_t SOC_getFlashDataBaseAddr (void)
 This function gets the SOC mapped data base address of the flash. More...
 

Macros

#define MSS_CTRL_PARTITION0   (1)
 
#define TOP_CTRL_PARTITION0   (2)
 
#define CONTROLSS_CTRL_PARTITION0   (3)
 
#define MSS_RCM_PARTITION0   (4)
 
#define TOP_RCM_PARTITION0   (5)
 
#define KICK_LOCK_VAL   (0x00000000U)
 
#define KICK0_UNLOCK_VAL   (0x01234567U)
 
#define KICK1_UNLOCK_VAL   (0x0FEDCBA8U)
 
#define IS_I2C_BASE_ADDR_VALID(baseAddr)
 Macro to check if the I2C base address is valid. More...
 
#define IS_QSPI_BASE_ADDR_VALID(baseAddr)   (baseAddr == CSL_QSPI0_U_BASE)
 Macro to check if the QSPI base address is valid. More...
 
#define IS_QSPI_MEMORY_MAP_ADDR_VALID(baseAddr)
 Macro to check if the QSPI Memory Mapped address is valid. More...
 

SOC Domain ID

#define SOC_DOMAIN_ID_MAIN   (0U)
 

Macro Definition Documentation

◆ SOC_DOMAIN_ID_MAIN

#define SOC_DOMAIN_ID_MAIN   (0U)

◆ MSS_CTRL_PARTITION0

#define MSS_CTRL_PARTITION0   (1)

◆ TOP_CTRL_PARTITION0

#define TOP_CTRL_PARTITION0   (2)

◆ CONTROLSS_CTRL_PARTITION0

#define CONTROLSS_CTRL_PARTITION0   (3)

◆ MSS_RCM_PARTITION0

#define MSS_RCM_PARTITION0   (4)

◆ TOP_RCM_PARTITION0

#define TOP_RCM_PARTITION0   (5)

◆ KICK_LOCK_VAL

#define KICK_LOCK_VAL   (0x00000000U)

◆ KICK0_UNLOCK_VAL

#define KICK0_UNLOCK_VAL   (0x01234567U)

◆ KICK1_UNLOCK_VAL

#define KICK1_UNLOCK_VAL   (0x0FEDCBA8U)

◆ IS_I2C_BASE_ADDR_VALID

#define IS_I2C_BASE_ADDR_VALID (   baseAddr)
Value:
((baseAddr == CSL_I2C0_U_BASE) || \
(baseAddr == CSL_I2C1_U_BASE) || \
(baseAddr == CSL_I2C2_U_BASE) || \
(baseAddr == CSL_I2C3_U_BASE))

Macro to check if the I2C base address is valid.

◆ IS_QSPI_BASE_ADDR_VALID

#define IS_QSPI_BASE_ADDR_VALID (   baseAddr)    (baseAddr == CSL_QSPI0_U_BASE)

Macro to check if the QSPI base address is valid.

◆ IS_QSPI_MEMORY_MAP_ADDR_VALID

#define IS_QSPI_MEMORY_MAP_ADDR_VALID (   baseAddr)
Value:
((baseAddr == CSL_EXT_FLASH0_U_BASE) || \
(baseAddr == CSL_EXT_FLASH1_U_BASE))

Macro to check if the QSPI Memory Mapped address is valid.

Function Documentation

◆ MCSPI_lld_isBaseAddrValid()

static int32_t MCSPI_lld_isBaseAddrValid ( uint32_t  baseAddr)
inlinestatic

API to validate MCSPI base address.

◆ MMCSD_lld_isBaseAddrValid()

static int32_t MMCSD_lld_isBaseAddrValid ( uint32_t  baseAddr)
inlinestatic

API to validate MMCSD base addresses.

◆ SOC_moduleClockEnable()

int32_t SOC_moduleClockEnable ( uint32_t  moduleId,
uint32_t  enable 
)

Enable clock to specified module.

Parameters
moduleId[in] see SOC_RcmPeripheralId for list of module ID's
enable[in] 1: enable clock to the module, 0: disable clock to the module
Returns
SystemP_SUCCESS Module clock is enabled
SystemP_FAILURE Module clock could not be enabled

◆ SOC_moduleSetClockFrequency()

int32_t SOC_moduleSetClockFrequency ( uint32_t  moduleId,
uint32_t  clkId,
uint64_t  clkRate 
)

Set module clock to specified frequency.

Parameters
moduleId[in] see SOC_RcmPeripheralId for list of module ID's
clkId[in] see SOC_RcmPeripheralClockSource for list of clocks
clkRate[in] Frequency to set in Hz
Returns
SystemP_SUCCESS Module clock is enabled
SystemP_FAILURE Module clock could not be enabled

◆ SOC_getCoreName()

const char* SOC_getCoreName ( uint16_t  coreId)

Convert a core ID to a user readable name.

Parameters
coreId[in] see CSL_CoreID
Returns
name as a string

◆ SOC_getSelfCpuClk()

uint64_t SOC_getSelfCpuClk ( void  )

Get the clock frequency in Hz of the CPU on which the driver is running.

Returns
Clock frequency in Hz

◆ SOC_controlModuleLockMMR()

void SOC_controlModuleLockMMR ( uint32_t  domainId,
uint32_t  partition 
)

Lock control module partition to prevent writes into control MMRs.

Parameters
domainId[in] See SOC_DomainId_t
partition[in] Partition number to unlock

◆ SOC_controlModuleUnlockMMR()

void SOC_controlModuleUnlockMMR ( uint32_t  domainId,
uint32_t  partition 
)

Unlock control module partition to allow writes into control MMRs.

Parameters
domainId[in] See SOC_DomainId_t
partition[in] Partition number to unlock

◆ SOC_setEpwmTbClk()

void SOC_setEpwmTbClk ( uint32_t  epwmInstance,
uint32_t  enable 
)

Enable or disable ePWM time base clock from Control MMR.

Parameters
epwmInstance[in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]
enable[in] TRUE to enable and FALSE to disable

◆ SOC_setMultipleEpwmTbClk()

void SOC_setMultipleEpwmTbClk ( uint32_t  epwmMask,
uint32_t  enable 
)

Enable or disable Multiple ePWM time base clock from Control MMR.

Parameters
epwmMask[in] ePWM instance Mask [1 - CSL_CONTROLSS_CTRL_EPWM_CLKSYNC_BIT_MAX]
enable[in] TRUE to enable and FALSE to disable

◆ SOC_enableAdcReference()

void SOC_enableAdcReference ( uint32_t  adcInstance)

Enable ADC references by writing to Control MMR.

Parameters
adcInstance[in] ADC instance number [0 - (CSL_ADC_PER_CNT-1)]

◆ SOC_enableAdcInternalReference()

void SOC_enableAdcInternalReference ( uint32_t  adcInstance,
uint32_t  enable 
)

Enables the ADC internal reference.

Parameters
adcInstance[in] ADC instance number [0 - (CSL_ADC_PER_CNT-1)]
enable[in] TRUE to enable internal reference - FALSE to disable.

◆ SOC_enableAdcReferenceMonitor()

void SOC_enableAdcReferenceMonitor ( uint32_t  adcInstance,
uint32_t  enable 
)

Enable ADC reference Monitors by writing to Control MMR.

Parameters
adcInstance[in] ADC instance number [0 - (CSL_ADC_PER_CNT-1)]
enable[in] TRUE to enable internal reference Monitor - FALSE to disable.

◆ SOC_getAdcReferenceStatus()

uint32_t SOC_getAdcReferenceStatus ( uint32_t  adcInstance)

Gets the Reference status.

Parameters
adcInstance[in] ADC instance number [0 - (CSL_ADC_PER_CNT-1)]
Returns
TRUE - reference OK. FALSE - reference NOT OK.

◆ SOC_setEpwmGroup()

void SOC_setEpwmGroup ( uint32_t  epwmInstance,
uint32_t  group 
)

Configure the ePWM group.

Parameters
epwmInstance[in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]
group[in] The group for this ePWM instance [0 - 3]

◆ SOC_selectSdfm1Clk0Source()

void SOC_selectSdfm1Clk0Source ( uint8_t  source)

Select the SDFM1 CLK0 source.

Parameters
source[in] Source of SDFM1 CLK0. 0: source is SDFM1 CK0 from Pinmux. 1: source is SDFM0 CK0 from Pinmux

◆ SOC_gateEpwmClock()

void SOC_gateEpwmClock ( uint32_t  epwmInstance)

Gate the ePWM clock.

Parameters
epwmInstance[in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]

◆ SOC_ungateEpwmClock()

void SOC_ungateEpwmClock ( uint32_t  epwmInstance)

Ungate the ePWM clock.

Parameters
epwmInstance[in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]

◆ SOC_gateFsitxClock()

void SOC_gateFsitxClock ( uint32_t  fsitxInstance)

Gate the FSI-TX clock.

Parameters
fsitxInstance[in] FSITX instance number [0 - 3]

◆ SOC_gateFsirxClock()

void SOC_gateFsirxClock ( uint32_t  fsirxInstance)

Gate the FSI-RX clock.

Parameters
fsirxInstance[in] FSIRX instance number [0 - 3]

◆ SOC_gateCmpssaClock()

void SOC_gateCmpssaClock ( uint32_t  cmpssaInstance)

Gate the CMPSS-A clock.

Parameters
cmpssaInstance[in] CMPSS-A instance number [0 - 9]

◆ SOC_ungateCmpssaClock()

void SOC_ungateCmpssaClock ( uint32_t  cmpssaInstance)

Ungate the CMPSS-A clock.

Parameters
cmpssaInstance[in] CMPSS-A instance number [0 - 9]

◆ SOC_gateCmpssbClock()

void SOC_gateCmpssbClock ( uint32_t  cmpssbInstance)

Gate the CMPSS-B clock.

Parameters
cmpssbInstance[in] CMPSS-B instance number [0 - 9]

◆ SOC_ungateCmpssbClock()

void SOC_ungateCmpssbClock ( uint32_t  cmpssbInstance)

Ungate the CMPSS-B clock.

Parameters
cmpssbInstance[in] CMPSS-B instance number [0 - 9]

◆ SOC_gateEcapClock()

void SOC_gateEcapClock ( uint32_t  ecapInstance)

Gate the ECAP clock.

Parameters
ecapInstance[in] ECAP instance number [0 - 9]

◆ SOC_ungateEcapClock()

void SOC_ungateEcapClock ( uint32_t  ecapInstance)

Ungate the ECAP clock.

Parameters
ecapInstance[in] ECAP instance number [0 - 9]

◆ SOC_gateEqepClock()

void SOC_gateEqepClock ( uint32_t  eqepInstance)

Gate the EQEP clock.

Parameters
eqepInstance[in] EQEP instance number [0 - 2]

◆ SOC_ungateEqepClock()

void SOC_ungateEqepClock ( uint32_t  eqepInstance)

Ungate the EQEP clock.

Parameters
eqepInstance[in] EQEP instance number [0 - 2]

◆ SOC_gateSdfmClock()

void SOC_gateSdfmClock ( uint32_t  sdfmInstance)

Gate the SDFM clock.

Parameters
sdfmInstance[in] SDFM instance number [0 - 1]

◆ SOC_ungateSdfmClock()

void SOC_ungateSdfmClock ( uint32_t  sdfmInstance)

Ungate the SDFM clock.

Parameters
sdfmInstance[in] SDFM instance number [0 - 1]

◆ SOC_gateDacClock()

void SOC_gateDacClock ( void  )

Gate the DAC clock.

◆ SOC_ungateDacClock()

void SOC_ungateDacClock ( void  )

Ungate the DAC clock.

◆ SOC_gateAdcClock()

void SOC_gateAdcClock ( uint32_t  adcInstance)

Gate the ADC clock.

Parameters
adcInstance[in] ADC instance number [0 - 4]

◆ SOC_ungateAdcClock()

void SOC_ungateAdcClock ( uint32_t  adcInstance)

ungate the ADC clock

Parameters
adcInstance[in] ADC instance number [0 - 4]

◆ SOC_gateOttoClock()

void SOC_gateOttoClock ( uint32_t  ottoInstance)

Gate the OTTO clock.

Parameters
ottoInstance[in] OTTO instance number [0 - 3]

◆ SOC_ungateOttoClock()

void SOC_ungateOttoClock ( uint32_t  ottoInstance)

Ungate the OTTO clock.

Parameters
ottoInstance[in] OTTO instance number [0 - 3]

◆ SOC_gateSdfmPllClock()

void SOC_gateSdfmPllClock ( uint32_t  sdfmInstance)

Gate the SDFM PLL clock.

Parameters
sdfmInstance[in] SDFM instance number [0 - 1]

◆ SOC_ungateSdfmPllClock()

void SOC_ungateSdfmPllClock ( uint32_t  sdfmInstance)

Ungate the SDFM PLL clock.

Parameters
sdfmInstance[in] SDFM instance number [0 - 1]

◆ SOC_gateFsiPllClock()

void SOC_gateFsiPllClock ( uint32_t  fsiInstance)

Gate the FSI-TX PLL clock.

Parameters
fsiInstance[in] FSI instance number [0 - 3]

◆ SOC_generateEpwmReset()

void SOC_generateEpwmReset ( uint32_t  ePWMInstance)

Generate ePWM reset.

Parameters
ePWMInstance[in] ePWM instance number [0 - 31]

◆ SOC_generateFsiTxReset()

void SOC_generateFsiTxReset ( uint32_t  fsitxInstance)

Generate FSI-TX reset.

Parameters
fsitxInstance[in] FSI instance number [0 - 3]

◆ SOC_generateFsiRxReset()

void SOC_generateFsiRxReset ( uint32_t  fsirxInstance)

Generate FSI-RX reset.

Parameters
fsirxInstance[in] FSI instance number [0 - 3]

◆ SOC_generateCmpssaReset()

void SOC_generateCmpssaReset ( uint32_t  cmpssaInstance)

Generate CMPSS-A reset.

Parameters
cmpssaInstance[in] CMPSS-A instance number [0 - 9]

◆ SOC_generateCmpssbReset()

void SOC_generateCmpssbReset ( uint32_t  cmpssbInstance)

Generate CMPSS-B reset.

Parameters
cmpssbInstance[in] CMPSS-B instance number [0 - 9]

◆ SOC_generateEcapReset()

void SOC_generateEcapReset ( uint32_t  ecapInstance)

Generate ECAP reset.

Parameters
ecapInstance[in] ECAP instance number [0 - 9]

◆ SOC_generateEqepReset()

void SOC_generateEqepReset ( uint32_t  eqepInstance)

Generate EQEP reset.

Parameters
eqepInstance[in] EQEP instance number [0 - 2]

◆ SOC_generateSdfmReset()

void SOC_generateSdfmReset ( uint32_t  sdfmInstance)

Generate SDFM reset.

Parameters
sdfmInstance[in] SDFM instance number [0 - 1]

◆ SOC_generateDacReset()

void SOC_generateDacReset ( void  )

Generate DAC reset.

◆ SOC_generateAdcReset()

void SOC_generateAdcReset ( uint32_t  adcInstance)

Generate ADC reset.

Parameters
adcInstance[in] ADC instance number [0 - 4]

◆ Soc_enableEPWMHalt()

void Soc_enableEPWMHalt ( uint32_t  epwmInstance)

Halt EPWM with corresponding cPU.

Parameters
epwmInstance[in] EPWM instance number [0 - 31]

◆ Soc_disableEPWMHalt()

void Soc_disableEPWMHalt ( uint32_t  epwmInstance)

Halt EPWM with corresponding cPU.

Parameters
epwmInstance[in] EPWM instance number [0 - 31]

◆ Soc_enableECAPHalt()

void Soc_enableECAPHalt ( uint32_t  ecapInstance)

Halt ECAP with corresponding cPU.

Parameters
ecapInstance[in] ECAP instance number [0 - 10]

◆ Soc_disableECAPHalt()

void Soc_disableECAPHalt ( uint32_t  ecapInstance)

Halt ECAP with corresponding cPU.

Parameters
ecapInstance[in] ECAP instance number [0 - 10]

◆ SOC_generateOttoReset()

void SOC_generateOttoReset ( uint32_t  ottoInstance)

Generate OTTO reset.

Parameters
ottoInstance[in] OTTO instance number [0 - 3]

◆ SOC_selectIcssGpiMux()

void SOC_selectIcssGpiMux ( uint8_t  pru_instance,
uint32_t  mask 
)

Selection of ICSS GPI MUX.

Parameters
pru_instance[in] PRU instance number [0 - 1]
mask[in] Bitwise selection of ICSSM GPI source. GPI or PWMXBar select for ICSSM port 0/1. 0-GPI, 1-PWMXBAR

◆ SOC_setResetCPSWBit()

void SOC_setResetCPSWBit ( )

Setting CPSW hard reset Bit.

◆ SOC_clearResetCPSWBit()

void SOC_clearResetCPSWBit ( )

Clearing CPSW hard reset bit.

◆ SOC_virtToPhy()

uint64_t SOC_virtToPhy ( void *  virtAddr)

SOC Virtual (CPU) to Physical address translation function.

Parameters
virtAddr[IN] Virtual/CPU address
Returns
Corresponding SOC physical address

◆ SOC_phyToVirt()

void* SOC_phyToVirt ( uint64_t  phyAddr)

Physical to Virtual (CPU) address translation function.

Parameters
phyAddr[IN] Physical address
Returns
Corresponding virtual/CPU address

◆ SOC_configSlewRate()

void SOC_configSlewRate ( uint32_t  baseAddr,
uint32_t  bankNum,
uint32_t  groupNum,
uint32_t  samplePeriod 
)

Configure GPIO pin Slew rate.

Parameters
baseAddrBase Address of IOMUX registers (CSL_IOMUX_U_BASE)
bankNumBank number of GPIO Pin
groupNumGroup Number where one group register applies to 8 GPIO's. So, one bank will be in two groups. For lower half, pass group number as 0 and for upper half pass 1.
samplePeriodSampling period in units of clock cycles.
Note
Qualifier selection should be done for Pad config register using Pinmux_config

◆ UART_IsBaseAddrValid()

static int32_t UART_IsBaseAddrValid ( uint32_t  baseAddr)
inlinestatic

Macro to validate UART base address.

API to validate UART base address

◆ SOC_getFlashDataBaseAddr()

uint32_t SOC_getFlashDataBaseAddr ( void  )

This function gets the SOC mapped data base address of the flash.

Returns
Data BaseAddress of the flash