This file contains the declaration of the APIs , Macros, structures and Enums for device abstraction layer file of ECC Bus Safety.
Go to the source code of this file.
Data Structures | |
struct | SDL_ECC_BUS_SAFETY_Base_Addr_Offset_S |
struct | SDL_ECC_BUS_SAFETY_staticRegs |
Functions | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_secExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data) |
This API is used for SEC test on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_dedExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data) |
This API is used for DED test on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_redExecute (uint32_t busSftyNode, SDL_ECC_BUS_SAFETY_busSftyFiType fiType, SDL_ECC_BUS_SAFETY_busSftyFiRedType redType) |
This API is used for RED test on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_secErrorClear (uint32_t busSftyNode) |
This API is used to clear SEC error on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_getSecErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get SEC error Status on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_dedErrorClear (uint32_t busSftyNode) |
This API is used to clear DED error on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_getDedErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get DED error Status on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_redErrorClear (uint32_t busSftyNode) |
This API is used to clear RED error on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_getRedErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get RED error Status on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_readStaticRegs (uint32_t busSftyNode, SDL_ECC_BUS_SAFETY_staticRegs *pStaticRegs) |
This API is used to get DSS static register values. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_secExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data) |
This API is used for SEC test on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_dedExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data) |
This API is used for DED test on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_redExecute (uint32_t busSftyNode, SDL_ECC_BUS_SAFETY_busSftyFiType fiType, SDL_ECC_BUS_SAFETY_busSftyFiRedType redType) |
This API is used for RED test on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_secErrorClear (uint32_t busSftyNode) |
This API is used to clear SEC error on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_getSecErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get SEC error Status on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_dedErrorClear (uint32_t busSftyNode) |
This API is used to clear DED error on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_getDedErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get DED error Status on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_redErrorClear (uint32_t busSftyNode) |
This API is used to clear RED error on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_getRedErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get RED error Status on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_readStaticRegs (uint32_t busSftyNode, SDL_ECC_BUS_SAFETY_staticRegs *pStaticRegs) |
This API is used to get MSS static register values. More... | |
uint32_t | SDL_ECC_BUS_SAFETY_DSS_AWR2944_AWR2943_Detect (void) |
This API is used to detect the device AWR2944/ Awr2943. More... | |