This example application illustrates the configuration and usage of Ether-Ring topology with 4 nodes connected in loop where each node works as central compute, zone left, zone right and zone tail. The example application enables both MAC ports by default and each node is connected to it's neighbouring node in a loop. This application uses Concurrence execution of gPTP IEEE 802.1AS stack and IEEE 802.1 Qbv (EST) configuration and Ether-ring to support Packet Duplication, Ring Termination in Hardware and Duplicate Rejection in Software.
The example application opens two DMA TX channels and two DMA RX channels. The TX0 and RX0 DMA channel will be used by the application to send the Class-A and Class-D stream packets via Ether-Ring Driver. The TX0 and RX0 DMA channel will be used for GPTP.
API for packet transmission.
The Application creates Class-A, Class-D stream RTOS tasks which creates the 802.1Q Ethernet Multicast packet with stream configuration and calls "EtherRing_submitTxPktQ" API from Ether-Ring Driver. "EtherRing_submitTxPktQ" creates a custom Custom header(4 bytes) which consists of CB-like Ethertype(0x88B5), unique sequence ID for each Ethernet packet and adds the custom Header to the packet sent from application without modifying the payload using zero-copy (using Transmit Scatter-Gather feature of HW). The packet is submitted to DMA and CPSW duplicates the multicast packet and sent it to both MAC ports.
When the packets are received RX DMA ISR will be triggered and "EtherRing_retrieveRxPktQ" is called from RTOS Rx application task. "EtherRing_retrieveRxPktQ" calls the DMA Retrieve API to retrieve the packets and Duplicate Packet Rejection is done using {SrcMacAddr, Sequence Number} based Look-up Table. Original stream packets found using look-up table are sent to Application and Duplicate packets received are submitted back to the DMA.
This EST schedule is 1 msec long and is composed of 8 intervals, each with a gate mask that enables transmission of 2,3 are configured for Class A and Class D streams.
The application follows a coordinated startup sequence using GPTP synchronization, EST scheduling, and hardware pulse generation:
All nodes initialize networking stack and wait for GPTP (802.1AS) clock synchronization:
RX Host time stamping is enabled from syscfg to measure the jitter in latency for the Received packets and timestamp value is stored in "rxPktTs" for each received packet(pktInfo). The timestamp values are stored in Ether-Ring driver for Jitter measurement.
The following helper options are also provided in the application's start menu to configure the each node uniquely in Etherring:
Make sure you have setup the EVM with cable connections as shown in below Diagram. In addition, follow the steps in the next section.
==========================
EtherRing App
==========================
0 - Central Compute Node
1 - Zone Left Node
2 - Zone Right Node
3 - Zone Tail Node
Enter the nodeId :
0
start to open driver.
EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:0 From 4 To 2
Init all configs
----------------------------------------------
sitara-cpsw: init config
Open MAC port 1
EnetPhy_bindDriver:1843
Open MAC port 2
EnetPhy_bindDriver:1843
PHY 3 is alive
PHY 12 is alive
sitara-cpsw: Create RX task for regular traffic
initQs() txFreePktInfoQ initialized with 48 pkts
MAC port addr: 70:ff:76:1f:6a:46
sitara-cpsw: default RX flow started
Waiting for GPTP ready!!
Start: uniconf_task
EnetApp_uniconfTask: dbname: NULL
EnetApp_gptpYangConfig:domain=0
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_SINGLE_CLOCK_MODE=1
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_USE_HW_PHASE_ADJUSTMENT=1
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_CLOCK_COMPUTE_INTERVAL_MSEC=100
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_FREQ_OFFSET_IIR_ALPHA_START_VALUE=1
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_FREQ_OFFSET_IIR_ALPHA_STABLE_VALUE=4
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_PHASE_OFFSET_IIR_ALPHA_START_VALUE=1
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_PHASE_OFFSET_IIR_ALPHA_STABLE_VALUE=4
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_MAX_DOMAIN_NUMBER=1
Start: gptp2d_task
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
GPTP ready!!
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
Start: melcoApp_EST
EnetApp_initTsn:TSN app start done!
ClassA stream count:1
ClassD stream count:1
Waiting for GPTP ready!!
GPTP ready!!
Waiting for GPTP ready!!
GPTP ready!!
Logger_task: started
unibase-1.1.4
INF:cbase:tilld0: has mac: 70:FF:76:1F:6A:46
INF:cbase:tilld1: has mac: 00:00:00:00:00:00
INF:cbase:cb_lld_task_create: uniconf_task stack_size=8192
INF:uconf:simpledb_open:no data is imported
INF:uconf:get_next_nameid:a new mod=xl4-data, enum=0
INF:uconf:get_next_nameid:a new mod=xl4-extmod, enum=1
INF:uconf:uc_hwal_open:
INF:cbase:cb_rawsock_open:combase-1.1.3
INF:cbase:cb_rawsock_open:dmaTxChId=-1 numRxChannels=1 dmaRxChId=-1 nTxPkts=0 nRxPkts=0 pktSize=0
INF:uconf:get_next_nameid:a new mod=ietf-interfaces, enum=2
INF:uconf:get_next_nameid:a new mod=ieee1588-ptp-tt, enum=3
INF:uconf:get_next_nameid:a new mod=ieee802-dot1q-bridge, enum=4
INF:uconf:get_next_nameid:a new mod=excelfore-tsn-remote, enum=5
INF:uconf:get_next_nameid:a new mod=excelfore-netconf-server, enum=6
INF:uconf:get_next_nameid:a new mod=ietf-netconf-monitoring, enum=7
INF:uconf:get_next_nameid:a new mod=ietf-yang-library, enum=8
INF:uconf:get_next_nameid:a new mod=ieee802-dot1ab-lldp, enum=9
INF:uconf:get_nWRN:gptp:gptpgcfg_link_check:can't read speed
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
Cpsw_handleLinkUp:1645
MAC Port 1: link up
INF:cbase:cbl_query_response:tilld0: link UP, speed=1000, duplex=1 !!!!
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
WRN:gptp:000013-500229:waiting_for_pdelay_interval_timer_proc:portIndex=1, sourcePortIdentity=34:08:E1:FF:FE:84:DB:CF, thisClock=70:FF:76:FF:FE:1F:6A:46, neighborPropDelay=392
Cpsw_handleLinkUp:1645
MAC Port 2: link up
INF:cbase:cbl_query_response:tilld1: link UP, speed=1000, duplex=1 !!!!
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
WRN:gptp:000014-625027:waiting_for_pdelay_interval_timer_proc:portIndex=2, sourcePortIdentity=34:08:E1:FF:FE:84:DD:31, thisClock=70:FF:76:FF:FE:1F:6A:46, neighborPropDelay=392
portIdx=0 netdev tilld0
syncFlag: 0
Current port-state: 9
EnetApp_enableCBS
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:ydbi_get_item_ifk4vk1:no data
INF:uconf:get_queue_map_params:netdev=tilld0, num_tc=0
The following AdminList param will be configured for EST:
GateMask[7..0]=oCCCoCCC (0x88), start=0 ns, end=19999 ns, dur=20000 ns
GateMask[7..0]=oCCCCoCC (0x84), start=20000 ns, end=124999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=125000 ns, end=144999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=145000 ns, end=249999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=250000 ns, end=269999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=270000 ns, end=374999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=375000 ns, end=394999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=395000 ns, end=499999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=500000 ns, end=519999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=520000 ns, end=624999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=625000 ns, end=644999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=645000 ns, end=749999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=750000 ns, end=769999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=770000 ns, end=874999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=875000 ns, end=894999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=895000 ns, end=999999 ns, dur=105000 ns
Base time=20000000000ns,Cycle time=1000000ns
Set admin control list succesfully
EnetApp_enableCBS
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:ydbi_get_item_ifk4vk1:no data
INF:uconf:get_queue_map_params:netdev=tilld1, num_tc=0
INF:uconf:get_queue_map_params:netdev=tilld0, num_tc=8
INF:cbase:TAS state is set to 2
INF:cbase:TAS operational list status updated:
INF:cbase:TAS state is set to 1
INF:cbase:Successfully configure TAS
The following AdminList param will be configured for EST:
GateMask[7..0]=oCCCoCCC (0x88), start=0 ns, end=19999 ns, dur=20000 ns
GateMask[7..0]=oCCCCoCC (0x84), start=20000 ns, end=124999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=125000 ns, end=144999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=145000 ns, end=249999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=250000 ns, end=269999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=270000 ns, end=374999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=375000 ns, end=394999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=395000 ns, end=499999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=500000 ns, end=519999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=520000 ns, end=624999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=625000 ns, end=644999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=645000 ns, end=749999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=750000 ns, end=769999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=770000 ns, end=874999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=875000 ns, end=894999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=895000 ns, end=999999 ns, dur=105000 ns
Base time=20000000000ns,Cycle time=1000000ns
Set admin control list succesfully
INF:uconf:get_queue_map_params:netdev=tilld1, num_tc=8
INF:cbase:TAS state is set to 2
INF:cbase:TAS operational list status updated:
INF:cbase:TAS state is set to 1
INF:cbase:Successfully configure TAS
WRN:gptp:000018-746101:md_pdelay_resp_sm_recv_req: port=2, expected SeqID=10723, but received=10724
Starting the Stream Traffic
RxTs and CurrentTs values stored
----------ETHERRING DEMONSTRATION COMPLETED----------
[RXTS]: 29954385101
[RXTS]: 29954510117
[RXTS]: 29954635123
[RXTS]: 29954760134
[RXTS]: 29954885145
[RXTS]: 29955010066
[RXTS]: 29955135082
[RXTS]: 29955260083
[RXTS]: 29955385094
[RXTS]: 29955510120
[RXTS]: 29955635121
[RXTS]: 29955760127
[RXTS]: 29955885143
[RXTS]: 29956010069
[RXTS]: 29956135075
[LAT]: 31248385523
[LAT]: 31248509968
[LAT]: 31248635684
[LAT]: 31248760014
[LAT]: 31248885115
[LAT]: 31249010280
[LAT]: 31249185376
[LAT]: 31249260041
[LAT]: 31249385041
[LAT]: 31249510402
[LAT]: 31249675958
[LAT]: 31249759993
[LAT]: 31249885083
[LAT]: 31250010974
[RX] Packet Count of stream0: 30000
[TX] Packet Count of stream0: 30000