This example demonstrates the UART RX and TX operation from both hld and lld driver APIs by looping the Tx & Rx externally in polling mode of operation.
Connect Jumper wires between the following HSEC pins
Connect Jumper wires between the following pins
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Boards | am263x-cc, am263x-lp |
Example folder | examples/drivers/uart/uart_hld_lld_external_loopback |
Shown below is a sample output when the application is run, Please note that application prints in CCS console.
CCS Console: