This example demonstrates the UART RX and TX operation in blocking, DMA mode of operation from LLD driver. This example receives 8 characters and echos back the same. The application ends when the user types 8 characters.
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 freertos |
r5fss0-0 nortos | |
Toolchain | ti-arm-clang |
Boards | am263x-cc, am263x-lp |
Example folder | examples/drivers/uart/uart_echo_dma_lld |
Shown below is a sample output when the application is run, Please note that application prints in both CCS and UART console. In UART console you need to enter 8 characters.
CCS Console:
UART Console: