AM263x MCU+ SDK  26.00.00
SBL QSPI

Introduction

This bootloader does SOC initializations and attempts to boot a multicore mcelf image present at 0x80000 location in the QSPI Flash. To flash a multicore mcelf at this location, follow the steps mentioned in Basic steps to flash files.

If a multicore application image is found at the location, the SBL parses it. Each core is then initialized, application image is loaded, entry points are set and the core is released from reset. For more on bootflow/bootloaders, please refer Understanding the bootflow and bootloaders

SBL QSPI Multicore ELF

For AM263x device, use the Multicore ELF project for SBL QSPI

To flash an mcelf file, use the project examples/drivers/boot/sbl_qspi_multicore_elf

When an mcelf image is found, the SBL parses it, loads each segment to its specified address location. Then the core is released from reset.

SBL QSPI FASTBOOT

This SBL is optimized for performance. It utilizes caching and disables logs which are present in other SBLs. Only MCELF application image format is supported with this SBL.

To flash an mcelf file, use the project examples/drivers/boot/sbl_qspi_fastboot.

In addition to the SBL and application, the HSM runtime firmware should also be flashed at an address known to the this SBL. This flash address can be configured via sysconfig and must match the one present in flash writer tool.

When an mcelf image is found, the SBL parses it, loads each segment to its specified address location. Then the core is released from reset.

The steps to run the example is same irrespective of the image format. Please follow the steps mentioned in Achieving Fast Secure Boot and Boot time calculator.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263x-cc, am263x-lp
Example folder examples/drivers/boot/sbl_qspi_multicore_elf

Steps to Run the Example

Since this is a bootloader, the example will be run every time you boot an application using this example. It is run from a QSPI boot media unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Refer to the page Basic steps to flash files to flash this bootloader along with the application to boot.

See Also

BOOTLOADER

Sample Output

Starting QSPI Bootloader ...
[BOOTLOADER PROFILE] System_init : 196us
[BOOTLOADER PROFILE] Drivers_open : 28us
[BOOTLOADER PROFILE] Board_driversOpen : 235us
[BOOTLOADER PROFILE] CPU load : 126043us
[BOOTLOADER_PROFILE] SBL Total Time Taken : 126509us
Image loading done, switching to application ...