AM263x MCU+ SDK  11.00.00
LIN External Commander Transmit

Introduction

This example is a application which demonstrates the LIN message communication to external PC via PLIN-USB (from PEAK Systems -> IPEH-004052) Instance LIN1 is set as a Commander in Transmit Mode.

The LIN1 instance initiates the transmission by sending LINID followed by message. The size of the message is also increased with increasing id.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263x-cc
Example folder examples/drivers/lin/lin_external
Note
This Example is only functional on am263x-cc E2 board. This is not supported on am263x-cc E1 or am263x-lp. For support on these boards, please reach out to your TI representative. This example is only functional on Windows setup due to limited availibility of PLIN-View Pro.

Steps to Run the Example

  • Board Configuration, change the SW9 to ON mode, and change the SW10 to 1-2.
    LIN SW9 set to ON

LIN SW10 connected in 1-2
  • Hardware Conectivity, connect the PLIN-USB module to PC from USB and Serial Port to be connected as mentioned in the image below.
    LIN Hardware Connectivity with PLIN USB - J32 Header
  • Software Setup, Download and Install the PLIN-View Pro from https://www.peak-system.com/PLIN-USB.485.0.html?&L=1
  • Click on LIN in the menu bar and connect to PLIN-USB. Make sure the LINMode for PLIN is Responder with Baud Rate of 19200.
    LIN Hardware Connectivity with PLIN USB.
  • After successful connection with PLIN-USB, the status of connection is shown as the bottom of the screen.
    PLIN Connectivity status.
  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run

Overridding the default configurations

  • To override the default configurations or initializations, uncheck the box of Default Configuration and rebuild the example. The same example will work without any other changes.

Bypassing Default Configuration.

See Also

LIN

Sample Output

Shown below is a sample output when the application is run,

[LIN] LIN mode external, application started ...
[I2C] LIN Volatage Level Shifter started ...
[LIN] : New Data Sent = 12
[LIN] : New Data Sent = 34
[LIN] : New Data Sent = 56
[LIN] : New Data Sent = 78
[LIN] : New Data Sent = 9a
[LIN] : New Data Sent = ab
[LIN] : New Data Sent = cd
[LIN] : New Data Sent = ef
All tests have passed!!

Shown below is a sample output on PLIN-View Pro

Output on PLIN-View Pro