AM263x MCU+ SDK  09.02.00
ECAP Capture Pwm

Introduction

This example uses the ECAP in capture mode to capture PWM.

The example does the below

  • Configures ECAP in Capture mode and captures the epwm output.
  • It captures the time between the rising and falling edge of epwm output.
___________________ _____________ __________________
| | | | | |
| EPWM |---GPIO---| I/P XBAR |---I/P MUX---| ECAP |---INT XBAR
|_________________| |___________| |________________|

External Connections

AM263X-CC

No external connection is required.

AM263X-LP

No external connection is required.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263x-cc, am263x-lp
Example folder examples/drivers/ecap/ecap_capture_pwm/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run

See Also

ECAP

Sample Output

Shown below is a sample output when the application is run,

ECAP Capture Pwm Test Started ...
Interrupt No.: 10 and Pass Count: 10
ECAP Capture Pwm Passed!!
All tests have passed!!