Introduction
This example sets up ePWM0 to periodically trigger a burst mode conversions of burst size 3 on ADC1 for conversion of inputs on ADC_AIN0, ADC_AIN1, ADC_AIN2, ADC_AIN3 and burst mode conversion on ADC_AIN3. This demonstrates a batch of conversion on ADC0 (inputs on ADC_AIN0 and ADC_AIN1) and burst mode conversion on ADC0 (input ADC_AIN3). ADC0 Interrupt ISR is used to read results of ADC0 (i.e. digital representations of inputs ADC_AIN0, ADC_AIN1 and average of oversampled ADC_AIN3)
Example Block diagram
Example Description
The example demonstrates Burst mode of ADC periodically triggered by trigger from EPWM0.
SOC Configurations
- SOC0 - SOC6 are configured High priority
- SOC7 - SOC15 are configured for Burst mode, with Burst size of 3 i.e., SOC(7,8,9), SOC(10,11,12), SOC(13,14,15) act as bursts and
- EPWM0SOCA is selected as trigger for Burst mode.
- SOC(7,10,13, 14) sample on ADC 1 Channel 0
- SOC(8,11) sample on ADC 1 Channel 1
- SOC(9,12) sample on ADC 1 Channel 2
- SOC(15) sample on ADC 1 Channel 3
Interrupt Configurations
- ADC1 INT 1 is generated at the EOC/SOC9
- ADC1 INT 2 is generated at the EOC/SOC12
- ADC1 INT 3 is generated at the EOC/SOC15
ISR
- ADC INT 1,2,3 are configured to same ISR, App_adcISR.
- reads which EOC generated Interrupt and reads the respective result registers.
Watch Variables
- gAdc1Result0[] : Digital representation of the voltage, averaged on burst sample on pin ADC0_AIN0
- gAdc1Result1[] : Digital representation of the voltage, averaged on burst sample on pin ADC0_AIN1
- gAdc1Result2[] : Digital representation of the voltage sampled on pin ADC0_AIN2
- gAdc1result3[] : Digital representation of the voltage sampled on pin ADC0_AIN3
External Connections :
AM263Px-CC E2 or AM263x-CC E2
Feed analog voltages on
- ADC1_AIN0, i.e., HSEC PIN 12
- ADC1_AIN1, i.e., HSEC PIN 14
- ADC1_AIN2, i.e., HSEC PIN 18
- ADC1_AIN3, i.e., HSEC PIN 20
AM263x-CC E1
Feed analog voltages on
- ADC1_AIN0, i.e., HSEC PIN 18
- ADC1_AIN1, i.e., HSEC PIN 20
- ADC1_AIN2, i.e., HSEC PIN 21
- ADC1_AIN3, i.e., HSEC PIN 23
AM263Px-LP or AM263x-LP
Feed analog voltages on
- ADC1_AIN0, i.e., J1/3 PIN 24
- ADC1_AIN1, i.e., J1/3 PIN 29
- ADC1_AIN2, i.e., J5/7 PIN 67
- ADC1_AIN3, i.e., J1/3 PIN 6
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am263x-cc, am263x-lp |
Example folder | examples/drivers/adc/adc_burst_mode_epwm/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section.
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Using the watch variables, view the ADC conversion results.
- View the ADC conversion results in UART console logs
See Also
ADC
Sample Output
Shown below is a sample output when the application is run,
ADC Burst Mode EPWM Test Started ...
ADC1Digital Converted Values
Channel0 : Channel1 : Channel2 : Channel3
766 : 769 : 1533 : 766
775 : 777 : 1550 : 777
771 : 773 : 1546 : 769
775 : 775 : 1546 : 772
781 : 783 : 1556 : 780
776 : 777 : 1545 : 770
785 : 784 : 1569 : 781
780 : 777 : 1554 : 778
782 : 781 : 1564 : 781
789 : 789 : 1576 : 787
781 : 784 : 1561 : 785
ADC Burst Mode EPWM Test Passed
All tests have passed!!