AM263x MCU+ SDK  26.00.00
DAP Default

Introduction

This example demonstrates the Device Agent Protocol (DAP) communication layer used for integration with Edge AI Studio. DAP provides a standardized UART-based protocol for streaming sensor data, receiving commands, and transmitting inference results between the microcontroller and Edge AI Studio.

This example serves as a reference implementation for:

  • Establishing DAP communication with Edge AI Studio
  • Implementing sensor data streaming
  • Handling pipeline configuration commands
  • Transmitting inference results

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263x-lp
Example folder examples/ai/dap_default/

DAP Protocol Overview

The Device Agent Protocol (DAP) provides:

  • Frame-based communication: CRC-validated frames for reliable data transfer
  • Multiple data channels: Support for sensor signals, inference signals, results, values, and logs
  • Command handling: Pipeline configuration and control commands from Edge AI Studio
  • Multi-sensor streaming: Support for streaming data from multiple sensors simultaneously

Key DAP Functions

Function Description
Dap_Init() Initialize DAP instance
Dap_Process() Main processing loop
Dap_SendSensorData() Stream sensor data
Dap_StartSensorStream() Start sensor streaming
Dap_StopSensorStream() Stop sensor streaming

Dependencies

  • Edge AI Studio for communication
  • UART interface for DAP protocol

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • Connect Edge AI Studio to the device via UART

See Also

AI Examples

Sample Output

[DAP] Example started...
[DAP] Initialized successfully. Waiting for commands...