AM263x MCU+ SDK  26.00.00
Blower Imbalance Detection

Introduction

Blower Imbalance detection is a classification problem to understand the correct working of fan blowers. The problem is to identify whether the fans of a running motor have any imbalance in rotation or not. This becomes important in real-world scenarios such as dust accumulation on fan blades, cooling systems, elevators, and anywhere there is a running motor. This example uses current readings instead of additional sensors to do the classification.

This project demonstrates implementation of an AI-based blower imbalance detection system on AM26x microcontrollers, helping prevent hazards through early detection of faults.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263x-lp
Example folder examples/ai/blower_imbalance/

Dataset and Model Details

Dataset

TI has created a specialized blower imbalance dataset containing AC current measurements (3-phase).

Parameter Value
Sensor Current Meter
Channels 3 (AC Current - 3 phases)
Sampling Rates 20 Hz, 30 Hz, 50 Hz, 60 Hz (variable)
Samples per File Variable: 36,000 - 90,000 samples
Total Files 123 files (69 normal, 54 fault)

Output Classes:

  • Class 0: Normal Operation
  • Class 1: Blower Imbalance

Model Architecture

This lightweight classification model CLS_1k_NPU contains approximately 1,000 parameters and follows a streamlined architecture consisting of four convolutional layers (each enhanced with BatchNorm and ReLU activation functions) followed by a single linear layer.

Input Features

The model takes 4D input (N,C,H,W):

  • N (1): batch size which is restricted to 1
  • C (3): channels which is 3 for 3-phase AC current
  • H (128): samples of timeseries AC current which is 128 in this example
  • W (1): width of samples is restricted to 1 for timeseries applications

Output

This model produces a 1D output representing the two possible classes - normal operation or blower imbalance condition.

Feature Extraction Configuration

The feature extraction pipeline uses FFT-based frequency analysis:

  • FE_FFT: Performs Fast Fourier Transform (256-point)
  • FE_DC_REM: Removes DC component
  • FE_BIN: Groups frequencies into 16 bins (bin size 8)
  • FE_BIN_NORMALIZE: Normalizes bin values
  • FE_LOG: Applies logarithmic scaling
  • FE_CONCAT: Combines 8 frames for temporal context

The pipeline processes 256-sample frames per channel, producing 16 features per frame, concatenated across 8 frames for 128 total features per channel.

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • The application will classify current readings as normal or imbalanced

See Also

AI Examples

Sample Output

Blower Imbalance Detection Example Started ...
Feature extraction mismatches 0
All tests have passed!!
Golden vectors matched: 2 not matched: 0