This module contains APIs to program and use the Flash module on the board like XSPI NOR Flash. See Flash for more details.
Data Structures | |
struct | Flash_DevConfig |
Flash device config. This will be part of the flash config, so has to be filled by sysconfig or otherwise before invoking Flash_open. More... | |
struct | Flash_Params |
Parameters passed during Flash_open() More... | |
struct | Flash_Fxns |
Driver implementation callbacks. More... | |
struct | Flash_Attrs |
Flash device attributes, these are filled by SysCfg based on the flash device that is selected. More... | |
struct | Flash_Config |
Flash driver configuration, these are filled by SysCfg based on the flash device that is selected. More... | |
Functions | |
void | Flash_Params_init (Flash_Params *params) |
Set default parameters in the Flash_Params structure. More... | |
Flash_Handle | Flash_open (uint32_t instanceId, Flash_Params *params) |
Open flash driver. More... | |
void | Flash_close (Flash_Handle handle) |
Close flash driver. More... | |
Flash_Handle | Flash_getHandle (uint32_t instanceId) |
Get handle to flash driver. More... | |
int32_t | Flash_read (Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len) |
Read data from flash. More... | |
int32_t | Flash_write (Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len) |
Write to flash. More... | |
int32_t | Flash_blkPageToOffset (Flash_Handle handle, uint32_t *offset, uint32_t block, uint32_t page) |
Utility API to convert (Block Num, Page Num) to offset in bytes. More... | |
int32_t | Flash_offsetToBlkPage (Flash_Handle handle, uint32_t offset, uint32_t *block, uint32_t *page) |
Utility API to convert offset in bytes to (Block Num, Page Num) More... | |
int32_t | Flash_SectorPageToOffset (Flash_Handle handle, uint32_t *offset, uint32_t sector, uint32_t page) |
Utility API to convert (Sector Num, Page Num) to offset in bytes. More... | |
int32_t | Flash_offsetToSectorPage (Flash_Handle handle, uint32_t offset, uint32_t *sector, uint32_t *page) |
Utility API to convert offset in bytes to (Sector Num, Page Num) More... | |
int32_t | Flash_eraseBlk (Flash_Handle handle, uint32_t blockNum) |
Erase a block from flash. More... | |
int32_t | Flash_eraseSector (Flash_Handle handle, uint32_t sectorNum) |
Erase a sector from flash. More... | |
int32_t | Flash_reset (Flash_Handle handle) |
Do a soft reset of the flash. More... | |
uint32_t | Flash_getPhyTuningOffset (Flash_Handle handle) |
Return flash offset to write PHY tuning data. More... | |
Flash_Attrs * | Flash_getAttrs (uint32_t instanceId) |
Return flash attributes. More... | |
Typedefs | |
typedef void * | Flash_Handle |
Handle to the FLash driver returned by Flash_opem() More... | |
typedef struct Flash_Config_s | Flash_Config |
Forward declaration of Flash_Config. More... | |
typedef struct Flash_Params_s | Flash_Params |
Forward declaration of Flash_Params. More... | |
Flash driver implementation callbacks | |
typedef int32_t(* | Flash_OpenFxn) (Flash_Config *config, Flash_Params *params) |
Driver implementation to open a specific flash driver. More... | |
typedef void(* | Flash_CloseFxn) (Flash_Config *config) |
Driver implementation to close a specific flash driver. More... | |
typedef int32_t(* | Flash_ReadFxn) (Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len) |
Driver implementation to read from flash using a specific flash driver. More... | |
typedef int32_t(* | Flash_WriteFxn) (Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len) |
Driver implementation to write to flash using specific flash driver. More... | |
typedef int32_t(* | Flash_EraseFxn) (Flash_Config *config, uint32_t blockNum) |
Driver implementation to erase a block using a specific flash driver. More... | |
typedef int32_t(* | Flash_EraseSectorFxn) (Flash_Config *config, uint32_t sectorNum) |
Driver implementation to erase a sector using a specific flash driver. More... | |
typedef int32_t(* | Flash_ResetFxn) (Flash_Config *config) |
Driver implementation to soft reset the flash. More... | |
typedef int32_t(* | Flash_quirksFxn) (Flash_Config *config) |
User implementation of a custom function to handle vendor specific quirks. More... | |
typedef int32_t(* | Flash_custProtocolFxn) (Flash_Config *config) |
User implementation of a custom function to configure flash to operate in a specific protocol. More... | |
typedef void* Flash_Handle |
Handle to the FLash driver returned by Flash_opem()
typedef struct Flash_Config_s Flash_Config |
Forward declaration of Flash_Config.
typedef struct Flash_Params_s Flash_Params |
Forward declaration of Flash_Params.
typedef int32_t(* Flash_OpenFxn) (Flash_Config *config, Flash_Params *params) |
Driver implementation to open a specific flash driver.
Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.
config | [in] Flash configuration for the specific flash device |
params | [in] User controllable parameters when opening the flash device |
typedef void(* Flash_CloseFxn) (Flash_Config *config) |
Driver implementation to close a specific flash driver.
Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.
config | [in] Flash configuration for the specific flash device |
typedef int32_t(* Flash_ReadFxn) (Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len) |
Driver implementation to read from flash using a specific flash driver.
Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.
config | [in] Flash configuration for the specific flash device |
offset | [in] Offset in the flash from where to start the read |
buf | [in] Buffer into which to read the data into |
len | [in] Length of the data to read, in bytes |
typedef int32_t(* Flash_WriteFxn) (Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len) |
Driver implementation to write to flash using specific flash driver.
Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.
config | [in] Flash configuration for the specific flash device |
offset | [in] Offset in the flash from where to start the write. |
buf | [in] Buffer which has the data to write. |
len | [in] Length of the data to write, in bytes |
typedef int32_t(* Flash_EraseFxn) (Flash_Config *config, uint32_t blockNum) |
Driver implementation to erase a block using a specific flash driver.
Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.
config | [in] Flash configuration for the specific flash device |
blockNum | [in] Block number to erase. |
typedef int32_t(* Flash_EraseSectorFxn) (Flash_Config *config, uint32_t sectorNum) |
Driver implementation to erase a sector using a specific flash driver.
Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.
config | [in] Flash configuration for the specific flash device |
sectorNum | [in] Sector number to erase. |
typedef int32_t(* Flash_ResetFxn) (Flash_Config *config) |
Driver implementation to soft reset the flash.
Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.
config | [in] Flash configuration for the specific flash device |
sectorNum | [in] Sector number to erase. |
typedef int32_t(* Flash_quirksFxn) (Flash_Config *config) |
User implementation of a custom function to handle vendor specific quirks.
Typically this callback is hidden from the end application and is implemented when a new type of flash device needs to be implemented.
config | [in] Flash configuration for the specific flash device |
typedef int32_t(* Flash_custProtocolFxn) (Flash_Config *config) |
User implementation of a custom function to configure flash to operate in a specific protocol.
config | [in] Flash configuration for the specific flash device |
void Flash_Params_init | ( | Flash_Params * | params | ) |
Set default parameters in the Flash_Params structure.
Call this API to set defaults and then override the fields as needed before calling Flash_open.
params | [out] Initialized parameters |
Flash_Handle Flash_open | ( | uint32_t | instanceId, |
Flash_Params * | params | ||
) |
Open flash driver.
Make sure the SOC peripheral driver is opened before calling this API. Drivers_open function generated by SysCfg opens the underlying SOC peripheral driver, e.g OSPI.
Internally this API also reads the device and manufacture ID and checks if it matches the expected value for the flash device, if there is mismatch then NULL
is returned.
Global variables Flash_Config gFlashConfig[]
and uint32_t gFlashConfigNum
is instantiated by SysCfg to describe the flash configuration based on user selection in SysCfg.
instanceId | [in] Index within Flash_Config gFlashConfig[] denoting the flash driver to open |
params | [in] Open parameters |
void Flash_close | ( | Flash_Handle | handle | ) |
Close flash driver.
handle | [in] Flash driver handle from Flash_open |
Flash_Handle Flash_getHandle | ( | uint32_t | instanceId | ) |
Get handle to flash driver.
instanceId | [in] Index within Flash_Config gFlashConfig[] |
int32_t Flash_read | ( | Flash_Handle | handle, |
uint32_t | offset, | ||
uint8_t * | buf, | ||
uint32_t | len | ||
) |
Read data from flash.
Internally it will use DMA and do the needed cache sync operations as needed.
handle | [in] Flash driver handle from Flash_open |
offset | [in] Offset in the flash from where to start the read |
buf | [in] Buffer into which to read the data into |
len | [in] Length of the data to read, in bytes |
int32_t Flash_write | ( | Flash_Handle | handle, |
uint32_t | offset, | ||
uint8_t * | buf, | ||
uint32_t | len | ||
) |
Write to flash.
Make sure the block is erased before writing
handle | [in] Flash driver handle from Flash_open |
offset | [in] Offset in the flash from where to start the write. |
buf | [in] Buffer which has the data to write. |
len | [in] Length of the data to write, in bytes |
int32_t Flash_blkPageToOffset | ( | Flash_Handle | handle, |
uint32_t * | offset, | ||
uint32_t | block, | ||
uint32_t | page | ||
) |
Utility API to convert (Block Num, Page Num) to offset in bytes.
handle | [in] Flash driver handle from Flash_open |
offset | [out] Offset in the flash, in bytes. |
block | [in] Block number to convert |
page | [in] Page number within the block |
int32_t Flash_offsetToBlkPage | ( | Flash_Handle | handle, |
uint32_t | offset, | ||
uint32_t * | block, | ||
uint32_t * | page | ||
) |
Utility API to convert offset in bytes to (Block Num, Page Num)
handle | [in] Flash driver handle from Flash_open |
offset | [in] Offset in the flash, in bytes. MUST be page size aligned. |
block | [out] Converted Block number |
page | [out] Converted Page number within the block |
int32_t Flash_SectorPageToOffset | ( | Flash_Handle | handle, |
uint32_t * | offset, | ||
uint32_t | sector, | ||
uint32_t | page | ||
) |
Utility API to convert (Sector Num, Page Num) to offset in bytes.
handle | [in] Flash driver handle from Flash_open |
offset | [out] Offset in the flash, in bytes. |
sector | [in] Sector number to convert |
page | [in] Page number within the block |
int32_t Flash_offsetToSectorPage | ( | Flash_Handle | handle, |
uint32_t | offset, | ||
uint32_t * | sector, | ||
uint32_t * | page | ||
) |
Utility API to convert offset in bytes to (Sector Num, Page Num)
handle | [in] Flash driver handle from Flash_open |
offset | [in] Offset in the flash, in bytes. MUST be page size aligned. |
sector | [out] Converted sector number |
page | [out] Converted Page number within the block |
int32_t Flash_eraseBlk | ( | Flash_Handle | handle, |
uint32_t | blockNum | ||
) |
Erase a block from flash.
Use the utility API Flash_offsetToBlkPage to convert a offset to block number
handle | [in] Flash driver handle from Flash_open |
blockNum | [in] Block number to erase. |
int32_t Flash_eraseSector | ( | Flash_Handle | handle, |
uint32_t | sectorNum | ||
) |
Erase a sector from flash.
Use the utility API Flash_offsetToSectorPage to convert a offset to block number
handle | [in] Flash driver handle from Flash_open |
sectorNum | [in] Sector number to erase. |
int32_t Flash_reset | ( | Flash_Handle | handle | ) |
Do a soft reset of the flash.
handle | [in] Flash driver handle from Flash_open |
uint32_t Flash_getPhyTuningOffset | ( | Flash_Handle | handle | ) |
Return flash offset to write PHY tuning data.
handle | [in] Flash driver handle from Flash_open |
Flash_Attrs* Flash_getAttrs | ( | uint32_t | instanceId | ) |
Return flash attributes.
instanceId | [in] Flash instance ID |