AM263x MCU+ SDK  08.05.00

Detailed Description

Global Param struct for the Rx channel open.

The parameter structure for the Rx channel open, containing a global channel config structure for all rx channels.

Data Fields

uint8_t dmaPriority
 
uint32_t rxBufferOffset
 

Field Documentation

◆ dmaPriority

uint8_t EnetCpdma_RxChInitPrms::dmaPriority

This field selects which scheduling bin the channel will be placed in for bandwidth allocation of the Rx DMA units.

◆ rxBufferOffset

uint32_t EnetCpdma_RxChInitPrms::rxBufferOffset

Receive buffer offset