Go to the source code of this file.
Macros | |
#define | MSS_CTRL_PARTITION0 (1) |
#define | TOP_CTRL_PARTITION0 (2) |
#define | CONTROLSS_CTRL_PARTITION0 (3) |
#define | MSS_RCM_PARTITION0 (4) |
#define | TOP_RCM_PARTITION0 (5) |
#define | KICK_LOCK_VAL (0x00000000U) |
#define | KICK0_UNLOCK_VAL (0x01234567U) |
#define | KICK1_UNLOCK_VAL (0x0FEDCBA8U) |
SOC Domain ID | |
#define | SOC_DOMAIN_ID_MAIN (0U) |
Functions | |
int32_t | SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable) |
Enable clock to specified module. More... | |
int32_t | SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate) |
Set module clock to specified frequency. More... | |
const char * | SOC_getCoreName (uint16_t coreId) |
Convert a core ID to a user readable name. More... | |
uint64_t | SOC_getSelfCpuClk (void) |
Get the clock frequency in Hz of the CPU on which the driver is running. More... | |
void | SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition) |
Lock control module partition to prevent writes into control MMRs. More... | |
void | SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition) |
Unlock control module partition to allow writes into control MMRs. More... | |
void | SOC_setEpwmTbClk (uint32_t epwmInstance, uint32_t enable) |
Enable or disable ePWM time base clock from Control MMR. More... | |
void | SOC_enableAdcReference (uint32_t adcInstance) |
Enable ADC references by writing to Control MMR. More... | |
void | SOC_setEpwmGroup (uint32_t epwmInstance, uint32_t group) |
Configure the ePWM group. More... | |
void | SOC_selectSdfm1Clk0Source (uint8_t source) |
Select the SDFM1 CLK0 source. More... | |
void | SOC_gateEpwmClock (uint32_t epwmInstance) |
Gate the ePWM clock. More... | |
void | SOC_gateFsitxClock (uint32_t fsitxInstance) |
Gate the FSI-TX clock. More... | |
void | SOC_gateFsirxClock (uint32_t fsirxInstance) |
Gate the FSI-RX clock. More... | |
void | SOC_gateCmpssaClock (uint32_t cmpssaInstance) |
Gate the CMPSS-A clock. More... | |
void | SOC_gateCmpssbClock (uint32_t cmpssbInstance) |
Gate the CMPSS-B clock. More... | |
void | SOC_gateEcapClock (uint32_t ecapInstance) |
Gate the ECAP clock. More... | |
void | SOC_gateEqepClock (uint32_t eqepInstance) |
Gate the EQEP clock. More... | |
void | SOC_gateSdfmClock (uint32_t sdfmInstance) |
Gate the SDFM clock. More... | |
void | SOC_gateDacClock (void) |
Gate the DAC clock. More... | |
void | SOC_gateAdcClock (uint32_t adcInstance) |
Gate the ADC clock. More... | |
void | SOC_gateOttoClock (uint32_t ottoInstance) |
Gate the OTTO clock. More... | |
void | SOC_gateSdfmPllClock (uint32_t sdfmInstance) |
Gate the SDFM PLL clock. More... | |
void | SOC_gateFsiPllClock (uint32_t fsiInstance) |
Gate the FSI-TX PLL clock. More... | |
void | SOC_generateEpwmReset (uint32_t ePWMInstance) |
Generate ePWM reset. More... | |
void | SOC_generateFsiTxReset (uint32_t fsitxInstance) |
Generate FSI-TX reset. More... | |
void | SOC_generateFsiRxReset (uint32_t fsirxInstance) |
Generate FSI-RX reset. More... | |
void | SOC_generateCmpssaReset (uint32_t cmpssaInstance) |
Generate CMPSS-A reset. More... | |
void | SOC_generateCmpssbReset (uint32_t cmpssbInstance) |
Generate CMPSS-B reset. More... | |
void | SOC_generateEcapReset (uint32_t ecapInstance) |
Generate ECAP reset. More... | |
void | SOC_generateEqepReset (uint32_t eqepInstance) |
Generate EQEP reset. More... | |
void | SOC_generateSdfmReset (uint32_t sdfmInstance) |
Generate SDFM reset. More... | |
void | SOC_generateDacReset (void) |
Generate DAC reset. More... | |
void | SOC_generateAdcReset (uint32_t adcInstance) |
Generate ADC reset. More... | |
void | SOC_generateOttoReset (uint32_t ottoInstance) |
Generate OTTO reset. More... | |
void | SOC_selectIcssGpiMux (uint8_t pru_instance, uint32_t mask) |
Selection of ICSS GPI MUX. More... | |
uint64_t | SOC_virtToPhy (void *virtAddr) |
SOC Virtual (CPU) to Physical address translation function. More... | |
void * | SOC_phyToVirt (uint64_t phyAddr) |
Physical to Virtual (CPU) address translation function. More... | |