Functions | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_secExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data) |
This API is used for SEC test on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_dedExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data) |
This API is used for DED test on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_redExecute (uint32_t busSftyNode, SDL_ECC_BUS_SAFETY_busSftyFiType fiType, SDL_ECC_BUS_SAFETY_busSftyFiRedType redType) |
This API is used for RED test on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_secErrorClear (uint32_t busSftyNode) |
This API is used to clear SEC error on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_getSecErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get SEC error Status on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_dedErrorClear (uint32_t busSftyNode) |
This API is used to clear DED error on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_getDedErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get DED error Status on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_redErrorClear (uint32_t busSftyNode) |
This API is used to clear RED error on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_DSS_getRedErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get RED error Status on DSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_secExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data) |
int32_t | SDL_ECC_BUS_SAFETY_MSS_dedExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data) |
This API is used for DED test on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_redExecute (uint32_t busSftyNode, SDL_ECC_BUS_SAFETY_busSftyFiType fiType, SDL_ECC_BUS_SAFETY_busSftyFiRedType redType) |
This API is used for RED test on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_secErrorClear (uint32_t busSftyNode) |
This API is used to clear SEC error on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_getSecErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get SEC error Status on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_dedErrorClear (uint32_t busSftyNode) |
This API is used to clear DED error on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_getDedErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get DED error Status on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_redErrorClear (uint32_t busSftyNode) |
This API is used to clear RED error on MSS. More... | |
int32_t | SDL_ECC_BUS_SAFETY_MSS_getRedErrorStatus (uint32_t busSftyNode, uint32_t *status) |
This API is used to get RED error Status on MSS. More... | |
int32_t SDL_ECC_BUS_SAFETY_DSS_secExecute | ( | uint32_t | busSftyNode, |
uint32_t | addr, | ||
uint32_t | wr_data | ||
) |
This API is used for SEC test on DSS.
busSftyNode | Node identifier |
addr | address to which data to be written |
wr_data | data to be be written on the address |
int32_t SDL_ECC_BUS_SAFETY_DSS_dedExecute | ( | uint32_t | busSftyNode, |
uint32_t | addr, | ||
uint32_t | wr_data | ||
) |
This API is used for DED test on DSS.
busSftyNode | Node identifier |
addr | address to which data to be written |
wr_data | data to be be written on the address |
int32_t SDL_ECC_BUS_SAFETY_DSS_redExecute | ( | uint32_t | busSftyNode, |
SDL_ECC_BUS_SAFETY_busSftyFiType | fiType, | ||
SDL_ECC_BUS_SAFETY_busSftyFiRedType | redType | ||
) |
This API is used for RED test on DSS.
busSftyNode | Node identifier |
fiType | indicates the Fi type |
redType | indicates interface type |
int32_t SDL_ECC_BUS_SAFETY_DSS_secErrorClear | ( | uint32_t | busSftyNode | ) |
This API is used to clear SEC error on DSS.
busSftyNode | Node identifier |
int32_t SDL_ECC_BUS_SAFETY_DSS_getSecErrorStatus | ( | uint32_t | busSftyNode, |
uint32_t * | status | ||
) |
This API is used to get SEC error Status on DSS.
busSftyNode | Node identifier |
status | pointer to which status to be updated |
int32_t SDL_ECC_BUS_SAFETY_DSS_dedErrorClear | ( | uint32_t | busSftyNode | ) |
This API is used to clear DED error on DSS.
busSftyNode | Node identifier |
int32_t SDL_ECC_BUS_SAFETY_DSS_getDedErrorStatus | ( | uint32_t | busSftyNode, |
uint32_t * | status | ||
) |
This API is used to get DED error Status on DSS.
busSftyNode | Node identifier |
status | pointer to which status to be updated |
int32_t SDL_ECC_BUS_SAFETY_DSS_redErrorClear | ( | uint32_t | busSftyNode | ) |
This API is used to clear RED error on DSS.
busSftyNode | Node identifier |
int32_t SDL_ECC_BUS_SAFETY_DSS_getRedErrorStatus | ( | uint32_t | busSftyNode, |
uint32_t * | status | ||
) |
This API is used to get RED error Status on DSS.
busSftyNode | Node identifier |
status | pointer to which status to be updated |
int32_t SDL_ECC_BUS_SAFETY_MSS_secExecute | ( | uint32_t | busSftyNode, |
uint32_t | addr, | ||
uint32_t | wr_data | ||
) |
int32_t SDL_ECC_BUS_SAFETY_MSS_dedExecute | ( | uint32_t | busSftyNode, |
uint32_t | addr, | ||
uint32_t | wr_data | ||
) |
This API is used for DED test on MSS.
busSftyNode | Node identifier |
addr | address to which data to be written |
wr_data | data to be be written on the address |
int32_t SDL_ECC_BUS_SAFETY_MSS_redExecute | ( | uint32_t | busSftyNode, |
SDL_ECC_BUS_SAFETY_busSftyFiType | fiType, | ||
SDL_ECC_BUS_SAFETY_busSftyFiRedType | redType | ||
) |
This API is used for RED test on MSS.
busSftyNode | Node identifier |
fiType | indicates the Fi type |
redType | indicates interface type |
int32_t SDL_ECC_BUS_SAFETY_MSS_secErrorClear | ( | uint32_t | busSftyNode | ) |
This API is used to clear SEC error on MSS.
busSftyNode | Node identifier |
int32_t SDL_ECC_BUS_SAFETY_MSS_getSecErrorStatus | ( | uint32_t | busSftyNode, |
uint32_t * | status | ||
) |
This API is used to get SEC error Status on MSS.
busSftyNode | Node identifier |
status | pointer to which status to be updated |
int32_t SDL_ECC_BUS_SAFETY_MSS_dedErrorClear | ( | uint32_t | busSftyNode | ) |
This API is used to clear DED error on MSS.
busSftyNode | Node identifier |
int32_t SDL_ECC_BUS_SAFETY_MSS_getDedErrorStatus | ( | uint32_t | busSftyNode, |
uint32_t * | status | ||
) |
This API is used to get DED error Status on MSS.
busSftyNode | Node identifier |
status | pointer to which status to be updated |
int32_t SDL_ECC_BUS_SAFETY_MSS_redErrorClear | ( | uint32_t | busSftyNode | ) |
This API is used to clear RED error on MSS.
busSftyNode | Node identifier |
int32_t SDL_ECC_BUS_SAFETY_MSS_getRedErrorStatus | ( | uint32_t | busSftyNode, |
uint32_t * | status | ||
) |
This API is used to get RED error Status on MSS.
busSftyNode | Node identifier |
status | pointer to which status to be updated |