This module contains APIs for using configuring the DPL function pointers to be used by SDL, and also defines the DPL APIs used by SDL for services such as interrupt registration.
|
file | sdl_dpl.h |
| This file contains the SDL DPL API's.
|
|
|
struct | SDL_DPL_HwipParams |
| This structure contains the parameters for interrupt registration through the SDL DPL interface. More...
|
|
struct | SDL_DPL_Interface |
| This structure contains the pointers for the DPL interfaces provided by the application to SDL_DPL_init. More...
|
|
◆ pSDL_DPL_InterruptCallbackFunction
typedef void(* pSDL_DPL_InterruptCallbackFunction) (void *arg) |
Prototype for the interrupt callback function.
◆ pSDL_DPL_HwipHandle
◆ pSDL_DPL_InterruptFunction
typedef int32_t(* pSDL_DPL_InterruptFunction) (int32_t intNum) |
Prototype for the interrupt enable/disable functions.
◆ pSDL_DPL_RegisterFunction
Prototype for the interrupt registration function.
◆ pSDL_DPL_DeregisterFunction
Prototype for the interrupt de-register function.
◆ pSDL_DPL_DelayFunction
typedef int32_t(* pSDL_DPL_DelayFunction) (int32_t ndelay) |
Prototype for the delay function.
◆ pSDL_DPL_AddrTranslateFunction
typedef void*(* pSDL_DPL_AddrTranslateFunction) (uint64_t addr, uint32_t size) |
Prototype for address translation function.
◆ SDL_DPL_init()
DPL init.
This function initializes the DPL interface structure with the functions provided by the application. These functions are application dependent, so it is required to be passed by the user.
- Parameters
-
dplInterface | [IN] DPL interface structure. |
- Returns
- The SDL error code for the API. If dplInterface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS
◆ SDL_DPL_enableInterrupt()
int32_t SDL_DPL_enableInterrupt |
( |
int32_t |
intNum | ) |
|
DPL enable interrupt.
This function will enable the specific interrupt number passed.
- Parameters
-
intNum | [IN] Interrupt Number |
- Returns
- The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS
◆ SDL_DPL_disableInterrupt()
int32_t SDL_DPL_disableInterrupt |
( |
int32_t |
intNum | ) |
|
DPL disable interrupt.
This function will disable the specific interrupt number passed.
- Parameters
-
intNum | [IN] Interrupt Number |
- Returns
- The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS
◆ SDL_DPL_registerInterrupt()
DPL register interrupt.
This function will register the specific interrupt number passed.
- Parameters
-
pParams | [IN] Parameters for interrupt registration |
handle | [OUT] Handle for this registered interrupt |
- Returns
- The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS
◆ SDL_DPL_deregisterInterrupt()
DPL deregister interrupt.
This function will deregister the specific interrupt number passed.
- Parameters
-
handle | [IN] Handle for the registered interrupt |
- Returns
- The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS
◆ SDL_DPL_delay()
int32_t SDL_DPL_delay |
( |
int32_t |
ndelay | ) |
|
DPL delay.
This function is used assign delay in the function
- Parameters
-
ndelay | [IN] delay in microseconds |
- Returns
- The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS
◆ SDL_DPL_addrTranslate()
void* SDL_DPL_addrTranslate |
( |
uint64_t |
addr, |
|
|
uint32_t |
size |
|
) |
| |
DPL Address translation function.
This function is used by the SDL to get a translation for a 64-bit address to local address space. It is expected that the requested adddress will remain available at the returned address and not be removed.
- Parameters
-
addr | [IN] Memory address to be translated |
size | [IN] Size of the memory |
- Returns
- The translated address or (-1) for failure.